Internet of Things
  • Technologies
  • More
Internet of Things
Forum New IoT developer device in the making
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 526 subscribers
  • Views 1322 views
  • Users 0 members are here
  • iot_platform
  • internet_of_things
  • stand-alone
  • mobile_connectivity
  • 2g
  • water_resistance
  • developer_device
Related

New IoT developer device in the making

e14 Contributor
e14 Contributor over 11 years ago

Hi guys!

 

We've been developing this new IoT developer device with built-in sensors and mobile connectivity that can be used for tracking and monitoring different things. To try and make the thing as good as we can for IoT developers, we're trying to reach out to people with specific knowledge in the field to find out what (if anything) they would want to do with a device like this. Would it be ok to do that here? We could really use all the help and opinions we can possibly get. Cheers!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz +1
    Hey shabaz, thanks for your comment! You're right, the description was a bit vague. Our idea is that we'll provide the HW so that SW developers (and also non-developers) wouldn't have to worry about it…
  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor +1
    Kaisa T You are quite right that it suits a particular application and market. The connectivity and battery life are very good, and its waterproof and can easily be mounted, which are also very good ideas…
Parents
  • engswee
    0 engswee over 11 years ago

    Dear Kaisa,

     

    The idea is good and the device look nice.

    Web IDE will be the best option for public user but it will be difficult for advance user with limited function.

     

    My suggestion is to create a GUI for SPI, I²C, ADC and other interface. So that user can modifier according to their need. It difficult but I think lot people will love it.

    Basically user don't need to do the programing code. They just set the parameter in GUI and the device is ready to go with plug and play sensor. image

    If still the programing code then you will face a lot of competitor. I just give some example ( https://www.spark.io/ ) (https://electricimp.com/) (https://cubesensors.com/).

    If you feel you have room to fit in. Go ahead.

     

    cheer

    ES

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to engswee

    Hi ES!

     

    Thanks so much for your comment.  Unfortunately GUI support for the serial interfaces is not in on the roadmap. However, you’ll have an option to make that a priority later on: We'll be setting up a feature request site where everybody can influence our roadmap by voting on submitted feature requests. We'll see where that takes us image

     

    Kaisa

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to engswee

    Hi ES!

     

    Thanks so much for your comment.  Unfortunately GUI support for the serial interfaces is not in on the roadmap. However, you’ll have an option to make that a priority later on: We'll be setting up a feature request site where everybody can influence our roadmap by voting on submitted feature requests. We'll see where that takes us image

     

    Kaisa