Internet of Things
  • Technologies
  • More
Internet of Things
Forum Resistor rating for IR LED for WiFi IoT remote
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 518 subscribers
  • Views 8872 views
  • Users 0 members are here
  • current
  • led
  • ir
  • iot
  • resistor
  • remote
Related

Resistor rating for IR LED for WiFi IoT remote

ntewinkel
ntewinkel over 4 years ago

Hello!

I was pondering this, and searching into the webs and on the lines, and then realized I have this awesome community of smart people here that probably already know the answers!

Short version:
Are 1/4 watt resistors enough to pulse an LED at 1 amp for an IR remote?
The LED is rated for 100mA continuous, 1.5 amp peak, and 1.6v forward voltage max.
I used an online calculator to figure out that with a 5v supply, a 6.8 ohm resistor will give it a 500mA current, and 3.4 ohms gives a 1amp current.

I'm not sure how to calculate the current on that LED - is it 1.6 volts x 1 amp? or 5 volts x 1 amp?

Either way though - even just the 1.6 watts is 6 times the current rating of the resistors I have. Is that ok for pulsed use for remote control like that?

Should I be using a set of parallel resistors instead (knowing I'll have to up the resistor values to compensate) ?

Project details:
My heat pump is kinda noisy, so at night we set it to "night mode" which is the quietest fan setting it has. We can't keep it at that setting because it won't heat the house well enough, so in the morning we turn the temperature up a few degrees and set the fan to "automatic".

I've been trying to automate this process, because the heat pump remote is kind of annoying in that you have to step through all 5 fan speeds to get back to Automatic.

I bought a little WiFi IR remote off Amazon a few years ago, which is ok for turning the heat up in the morning, but it only supports 3 basic fan speeds, so it doesn't properly turn the fan down at night. I recently bought another similar newer unit, hoping that after a few years my Daikin heat pump would now be fully supported, but it's still the same. Frowning2

But there's hope! I found a Github repository that actually fully supports my Daikin heat pump codes! And for my favourite IoT micro-controller even - the Wemos D1 Mini.

Using a basic IR LED I had scavenged from something in the past, I was able to get it to work, but the IR LED range was just -barely- able to reach the heat pump when aimed just right (I realize now that I was using far to big a resistor value).

So I got a few new "high power" IR LEDs (the clear QED234 ones) from element14's shop, which I hope will give me the range I need. Then I did the aforementioned calculations to find the ideal resistor values to get some good oompf out of the LED to reach further.

I was just about to start soldering things up when I realized that 1amp of current is higher than the 1/4 watt rating of the resistors I have.

I'm hoping you'll have some good advice for this software-biased hobbyist Laughing

Also - I'm guessing a resistor failure would generally not cause a short? (ie, losing a resistor is ok, I have plenty more - losing an IR LED is tougher as I only have a few!)

Thanks!
-Nico

  • Sign in to reply
  • Cancel

Top Replies

  • ntewinkel
    ntewinkel over 4 years ago +6
    Hi All, It works! It seems I was overthinking things, as usual :D I just tested a 2-LED circuit using 22 ohm resistors, which runs the LEDs at about 150mA, and it seems to be plenty to reach the…
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago +5
    Hello Nico, some comments: 1) Remotes usually send a modulated signal (38 kHz is a very common frequency, but anything between 34 and 56 kHz could be possible). This is good for your use case, as it…
  • fmilburn
    fmilburn over 4 years ago +3
    Hi Nico, It is easiest to look at the 1A case. There will be a 1A x 3.4R = 3.4v drop across the resistor and 1.6V drop across the LED. Since power = I*I*R the resistor sees spikes of 3.4W and the LED…
Parents
  • fmilburn
    0 fmilburn over 4 years ago

    Hi Nico,

    It is easiest to look at the 1A case.  There will be a 1A x 3.4R = 3.4v drop across the resistor and 1.6V drop across the LED.  Since power = I*I*R the resistor sees spikes of 3.4W and the LED sees 1.6W.  That doesn’t sound good. Are you using a transistor to control on/off?  Have you considered a constant current source without a resistor.  I’m curious what people more knowledgeable than me think. 

    Frank

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 4 years ago in reply to fmilburn

    Thanks Frank! I knew I was missing something big but didn’t know what! - I missed the math on the voltage drop on the resistor being vcc-(led voltage drop).

    And yes, early on I found that I had to use a transistor to get any results at all.
    I haven’t checked the ratings on it, I think it’s a pn2222a - in the most basic circuit where the I/O pin drives the transistor, connected through a resistor of course.

    I’m not familiar with constant current sources, I’m just using a phone charger cube rated at 1amp/5v

    I’m aiming for just a basic “works ok”, so if I can reduce the amperage to something within easier limits, I’ll do that. It only really needs to be in one spot aimed at the heat pump and send a packet twice a day, so I might be able to get away with some bursts of over current.

    I have a few more days away but will try some hands on testing later.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 4 years ago in reply to fmilburn

    Thanks Frank! I knew I was missing something big but didn’t know what! - I missed the math on the voltage drop on the resistor being vcc-(led voltage drop).

    And yes, early on I found that I had to use a transistor to get any results at all.
    I haven’t checked the ratings on it, I think it’s a pn2222a - in the most basic circuit where the I/O pin drives the transistor, connected through a resistor of course.

    I’m not familiar with constant current sources, I’m just using a phone charger cube rated at 1amp/5v

    I’m aiming for just a basic “works ok”, so if I can reduce the amperage to something within easier limits, I’ll do that. It only really needs to be in one spot aimed at the heat pump and send a packet twice a day, so I might be able to get away with some bursts of over current.

    I have a few more days away but will try some hands on testing later.