Internet of Things
  • Technologies
  • More
Internet of Things
Forum Resistor rating for IR LED for WiFi IoT remote
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 518 subscribers
  • Views 8886 views
  • Users 0 members are here
  • current
  • led
  • ir
  • iot
  • resistor
  • remote
Related

Resistor rating for IR LED for WiFi IoT remote

ntewinkel
ntewinkel over 4 years ago

Hello!

I was pondering this, and searching into the webs and on the lines, and then realized I have this awesome community of smart people here that probably already know the answers!

Short version:
Are 1/4 watt resistors enough to pulse an LED at 1 amp for an IR remote?
The LED is rated for 100mA continuous, 1.5 amp peak, and 1.6v forward voltage max.
I used an online calculator to figure out that with a 5v supply, a 6.8 ohm resistor will give it a 500mA current, and 3.4 ohms gives a 1amp current.

I'm not sure how to calculate the current on that LED - is it 1.6 volts x 1 amp? or 5 volts x 1 amp?

Either way though - even just the 1.6 watts is 6 times the current rating of the resistors I have. Is that ok for pulsed use for remote control like that?

Should I be using a set of parallel resistors instead (knowing I'll have to up the resistor values to compensate) ?

Project details:
My heat pump is kinda noisy, so at night we set it to "night mode" which is the quietest fan setting it has. We can't keep it at that setting because it won't heat the house well enough, so in the morning we turn the temperature up a few degrees and set the fan to "automatic".

I've been trying to automate this process, because the heat pump remote is kind of annoying in that you have to step through all 5 fan speeds to get back to Automatic.

I bought a little WiFi IR remote off Amazon a few years ago, which is ok for turning the heat up in the morning, but it only supports 3 basic fan speeds, so it doesn't properly turn the fan down at night. I recently bought another similar newer unit, hoping that after a few years my Daikin heat pump would now be fully supported, but it's still the same. Frowning2

But there's hope! I found a Github repository that actually fully supports my Daikin heat pump codes! And for my favourite IoT micro-controller even - the Wemos D1 Mini.

Using a basic IR LED I had scavenged from something in the past, I was able to get it to work, but the IR LED range was just -barely- able to reach the heat pump when aimed just right (I realize now that I was using far to big a resistor value).

So I got a few new "high power" IR LEDs (the clear QED234 ones) from element14's shop, which I hope will give me the range I need. Then I did the aforementioned calculations to find the ideal resistor values to get some good oompf out of the LED to reach further.

I was just about to start soldering things up when I realized that 1amp of current is higher than the 1/4 watt rating of the resistors I have.

I'm hoping you'll have some good advice for this software-biased hobbyist Laughing

Also - I'm guessing a resistor failure would generally not cause a short? (ie, losing a resistor is ok, I have plenty more - losing an IR LED is tougher as I only have a few!)

Thanks!
-Nico

  • Sign in to reply
  • Cancel

Top Replies

  • ntewinkel
    ntewinkel over 4 years ago +6
    Hi All, It works! It seems I was overthinking things, as usual :D I just tested a 2-LED circuit using 22 ohm resistors, which runs the LEDs at about 150mA, and it seems to be plenty to reach the…
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago +5
    Hello Nico, some comments: 1) Remotes usually send a modulated signal (38 kHz is a very common frequency, but anything between 34 and 56 kHz could be possible). This is good for your use case, as it…
  • fmilburn
    fmilburn over 4 years ago +3
    Hi Nico, It is easiest to look at the 1A case. There will be a 1A x 3.4R = 3.4v drop across the resistor and 1.6V drop across the LED. Since power = I*I*R the resistor sees spikes of 3.4W and the LED…
Parents
  • ntewinkel
    0 ntewinkel over 4 years ago

    Hi all,

    I just found some additional information on Adafruit that I think will clear up my resistor current worries.

    They are using a Raspberry Pi Zero with a QT-Py-Hat as a WiFi controlled IR remote control, which is exactly what I'm aiming for too, so I have hope it will also work in my setup.
    This is the Adafruit page with all the details: https://learn.adafruit.com/iot-ir-remote-using-raspberry-pi-zero-w-and-qtpy-hat/parts-required

    They recommend using 2 LEDs, where one is a wide angle LED and the other one a narrow angle LED. Each LED gets a transistor, which are both switched with a 3rd transistor that is controlled by the micro controller.

    The recommended IR LEDs are rated to 100mA with 1amp max, and 1.6v forward voltage. My LEDs have the same spec, with higher peak amps, so I assume they will behave in a similar way.

    For the resistors, they use ("optional") 33 ohm resistors, which if the online calculators are correct, comes out to the basic 100mA rating of the LED. Their explanation says these are optional and indicate they are only there to limit current if the LEDs draw so much power that they crash the main board. They are just using basic 1/4w resistors in that case too.

    They also have this IR-only project, using the same kind of circuit.
    https://learn.adafruit.com/building-an-infrared-transmitter-and-receiver-board
    The schematics for that are open source too: https://github.com/cyborg5/IRIO3 

    "The first option is to add a 33 ohm current limiting resistor in line with each of the LEDs. Without them, this circuit will drive the IR LEDs beyond their rated continuous current capacity. However because IR signals are intermittent and modulated it is safe to do this."

    This is a close-up of the schematic of the QT-Py-Hat on the Adafruit website, which has an IR transmitter on it. It's open source. (I've erased the bits that don't apply to my case).

    IR transmitter remote control circuit

    So, I'm guessing if they are leaving out the resistors altogether and aren't worried about burning the LEDs, then I probably don't need to worry about the resistor rating too much either, especially if I keep it within a reasonable range.

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 4 years ago

    Hi all,

    I just found some additional information on Adafruit that I think will clear up my resistor current worries.

    They are using a Raspberry Pi Zero with a QT-Py-Hat as a WiFi controlled IR remote control, which is exactly what I'm aiming for too, so I have hope it will also work in my setup.
    This is the Adafruit page with all the details: https://learn.adafruit.com/iot-ir-remote-using-raspberry-pi-zero-w-and-qtpy-hat/parts-required

    They recommend using 2 LEDs, where one is a wide angle LED and the other one a narrow angle LED. Each LED gets a transistor, which are both switched with a 3rd transistor that is controlled by the micro controller.

    The recommended IR LEDs are rated to 100mA with 1amp max, and 1.6v forward voltage. My LEDs have the same spec, with higher peak amps, so I assume they will behave in a similar way.

    For the resistors, they use ("optional") 33 ohm resistors, which if the online calculators are correct, comes out to the basic 100mA rating of the LED. Their explanation says these are optional and indicate they are only there to limit current if the LEDs draw so much power that they crash the main board. They are just using basic 1/4w resistors in that case too.

    They also have this IR-only project, using the same kind of circuit.
    https://learn.adafruit.com/building-an-infrared-transmitter-and-receiver-board
    The schematics for that are open source too: https://github.com/cyborg5/IRIO3 

    "The first option is to add a 33 ohm current limiting resistor in line with each of the LEDs. Without them, this circuit will drive the IR LEDs beyond their rated continuous current capacity. However because IR signals are intermittent and modulated it is safe to do this."

    This is a close-up of the schematic of the QT-Py-Hat on the Adafruit website, which has an IR transmitter on it. It's open source. (I've erased the bits that don't apply to my case).

    IR transmitter remote control circuit

    So, I'm guessing if they are leaving out the resistors altogether and aren't worried about burning the LEDs, then I probably don't need to worry about the resistor rating too much either, especially if I keep it within a reasonable range.

    -Nico