Internet of Things
  • Technologies
  • More
Internet of Things
Forum Why does the Bluetooth version need to be constantly updated?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 516 subscribers
  • Views 3283 views
  • Users 0 members are here
  • bluetooth
Related

Why does the Bluetooth version need to be constantly updated?

deryunpony
deryunpony over 3 years ago

With the passage of time, Bluetooth technology has been developed for 23 years, and the version has also been upgraded from 1.0 to 5.3. In theory, the more advanced the Bluetooth chip, the higher the cost. Why does the Bluetooth version need to be constantly updated?

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +6
    Bluetooth went through several different iterations - early upgrades (Classic, EDR) focused more on improving data rates, while later upgrades address complexity and low-power requirements (Smart, BLE…
  • baldengineer
    baldengineer over 3 years ago +5
    deryunpony said: Why does the Bluetooth version need to be constantly updated? Why does any technology need to be updated? New features enable new applications and use. As we explore those new capabilities…
  • misaz
    misaz over 3 years ago +4
    There is demand for new technologies and us cases. If Bluetooth would not be developed than proprietary standards supporting these new technologies and use cases would arrise. It is better to have one…
  • misaz
    0 misaz over 3 years ago

    There is demand for new technologies and us cases. If Bluetooth would not be developed than proprietary standards supporting these new technologies and use cases would arrise. It is better to have one standard rather multiple vendor specific proprietary standards.

    I dont think the price grow always. Bluetooth is good that it is backward compatible and many new features can be implemented using older chips with just chaning firmware (software). Note that many chip BT/BLE vendors do this and for example Noric regularly increments supported Bluetooth version on older chips.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 3 years ago

    Bluetooth went through several different iterations - early upgrades (Classic, EDR) focused more on improving data rates, while later upgrades address complexity and low-power requirements (Smart, BLE) while adding special capabilities (e.g. larger packets, AoA, ToA measurements for ranging) and also improving range (Coded PHY) or data rate (2M PHY).

    The technology progresses because there is an application for it - costs actually reduced for BLE versus Classic because of the reduced complexity. The needs of consumers have changed too - expectations on size, battery life has placed pressure on better wireless connectivity.

    - Gough

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 3 years ago
    deryunpony said:
    In theory, the more advanced the Bluetooth chip, the higher the cost.

    That's not quite the case. For example, when PSoC4 BLE modules (BLE 4.0 / 4.1 / 4.2) were released approx. 10 years ago they were one of the most competitively priced (they combined ARM M0+ MCU with BLE stack). I seem to recall the price point being around $10. Now you can get BLE modules from same manufacturer from $6 upwards.

    Then OEM's like Espressif came along and they've introduced BLE 5 modules at even lower prices at sub $5.

    In my experience often the higher priced modules have more memory and faster processors and have nothing really to do with the Bluetooth wireless stack etc.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • baldengineer
    0 baldengineer over 3 years ago
    deryunpony said:
    Why does the Bluetooth version need to be constantly updated?

    Why does any technology need to be updated? New features enable new applications and use. As we explore those new capabilities we envision even newer ones!

    The ubiquity of a nearly seamless, and for the most part secure, wireless protocol opens up a world of possibilities. In the 2000s, Bluetooth was viewed as a wireless-serial connection between PC, laptops, and mobile phones. That is where the focus for higher data rates came from with versions 2 and 3. However, with the popularity of a wireless handset for use with mobile phones, in cars, and even some desk phones came a need for better audio quality. How do you get higher quality? Faster data rates! Now you can stream audio data fast enough to get quality comparable to wires!

    Then as Bluetooth 3 got to impressive speeds the new focus became power management, so Bluetooth 4 gets a little speed bump and introduces the Low-Energy protocol. (And wow, as a terrible firmware developer, I love BLE! It is so easy to develop for compared to the full stack.)

    And now that practically everything that requires a WiFi connection also has a BLE radio for that initial setup, there are an unthinkable number of Bluetooth devices in the field. Wouldn't it be nice if they could mesh with each other? Kind of like how AirTags and Tiles do? Now you have Bluetooth 5....

    So why does it update? Because the industry and its customers continue to see new ways to use this ubiquitous protocol.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 3 years ago

    Bluetooth was developed to fill a low-power short range wireless communications gap. It has evolved with upgrades to have lower power, higher bandwidth, longer range, lower latency etc.

    These upgrades fill needs and demands in the industry for better performance. It would be possible to accommodate new technologies by creating completely new standards and call Bluetooth Low Energy something else since it is significantly different from Bluetooth. But the Bluetooth SIG decided to keep it all under the same umbrella and just keep upgrading/expanding the scope of Bluetooth.

    Most commonly used protocols are constantly evolving, USB is changing, Wi-Fi is changing, cell phone radios are changing, etc. Standards that are not used much any more like RS232 are pretty static.

    New technologies cost money to develop and those costs need to be recovered when selling products, but eventually the costs come down as the technology matures. You can still buy legacy Bluetooth devices which may be lower cost - which I do whenever those features are adequate for my application. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago

    I confess the upgrades at times add to my frustration. Didn't I already learn that...oh it is a new version and it is different than the other versions. Argh!

    When I step back and examine the features that are added through change it makes sense. The changes are meeting needs. I command line much of my Linux knowledge. This stuff is so new much of that knowledge is not available. DIdn't that use to work...oh yeah it is a new version.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 3 years ago

    deryunpony I use Debian 11, as I only use Bluetooth for my headphones, I really don't care about the upgrades, unless it breaks my distro. like Firefox does (continuously crashes and restarts. or how about my trusty VLC (video streamer, now when it crashes it takes the whole system down!! :( 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to phoenixcomm

    Go Windows!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 3 years ago in reply to Jan Cumps

    jancumps You are out of your mind.... Fools Love Micro$oft. Laughing