Internet of Things
  • Technologies
  • More
Internet of Things
Forum Why does the Bluetooth version need to be constantly updated?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 516 subscribers
  • Views 3284 views
  • Users 0 members are here
  • bluetooth
Related

Why does the Bluetooth version need to be constantly updated?

deryunpony
deryunpony over 3 years ago

With the passage of time, Bluetooth technology has been developed for 23 years, and the version has also been upgraded from 1.0 to 5.3. In theory, the more advanced the Bluetooth chip, the higher the cost. Why does the Bluetooth version need to be constantly updated?

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +6
    Bluetooth went through several different iterations - early upgrades (Classic, EDR) focused more on improving data rates, while later upgrades address complexity and low-power requirements (Smart, BLE…
  • baldengineer
    baldengineer over 3 years ago +5
    deryunpony said: Why does the Bluetooth version need to be constantly updated? Why does any technology need to be updated? New features enable new applications and use. As we explore those new capabilities…
  • misaz
    misaz over 3 years ago +4
    There is demand for new technologies and us cases. If Bluetooth would not be developed than proprietary standards supporting these new technologies and use cases would arrise. It is better to have one…
Parents
  • dougw
    0 dougw over 3 years ago

    Bluetooth was developed to fill a low-power short range wireless communications gap. It has evolved with upgrades to have lower power, higher bandwidth, longer range, lower latency etc.

    These upgrades fill needs and demands in the industry for better performance. It would be possible to accommodate new technologies by creating completely new standards and call Bluetooth Low Energy something else since it is significantly different from Bluetooth. But the Bluetooth SIG decided to keep it all under the same umbrella and just keep upgrading/expanding the scope of Bluetooth.

    Most commonly used protocols are constantly evolving, USB is changing, Wi-Fi is changing, cell phone radios are changing, etc. Standards that are not used much any more like RS232 are pretty static.

    New technologies cost money to develop and those costs need to be recovered when selling products, but eventually the costs come down as the technology matures. You can still buy legacy Bluetooth devices which may be lower cost - which I do whenever those features are adequate for my application. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 3 years ago

    Bluetooth was developed to fill a low-power short range wireless communications gap. It has evolved with upgrades to have lower power, higher bandwidth, longer range, lower latency etc.

    These upgrades fill needs and demands in the industry for better performance. It would be possible to accommodate new technologies by creating completely new standards and call Bluetooth Low Energy something else since it is significantly different from Bluetooth. But the Bluetooth SIG decided to keep it all under the same umbrella and just keep upgrading/expanding the scope of Bluetooth.

    Most commonly used protocols are constantly evolving, USB is changing, Wi-Fi is changing, cell phone radios are changing, etc. Standards that are not used much any more like RS232 are pretty static.

    New technologies cost money to develop and those costs need to be recovered when selling products, but eventually the costs come down as the technology matures. You can still buy legacy Bluetooth devices which may be lower cost - which I do whenever those features are adequate for my application. 

    • Cancel
    • Vote Up +3 Vote Down