Internet of Things
  • Technologies
  • More
Internet of Things
Forum Searching for wire-to-board connector, 34 mm round board, needs battery, haptic motor, speaker wires
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 520 subscribers
  • Views 2170 views
  • Users 0 members are here
  • connector
  • wire to board
  • arduino
Related

Searching for wire-to-board connector, 34 mm round board, needs battery, haptic motor, speaker wires

frankcohen
frankcohen over 3 years ago

Hi 14-ers, I am designing a mobile entertainment IoT device. It is a 34 mm round board with components on both sides. It's an ESP32-S3 Arduino-compatible board with a bunch of sensors. One application will be as a wrist watch. It will have a round battery with + and - leads (30 gauge, ~0.0509mm2), speaker, and haptic motor. I plan to manufacture 500 to 1000 wrist watches. I need an inexpensive and small footprint (less than 10 mm x 5 mm) connector to attach the battery, speaker, haptic motor. What do you recommend?

Reflection's design is free and open-source at https://github.com/frankcohen/ReflectionsOS.

-Frank

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +3
    Hi, I suggest that the mating connectors to whatever is already on the speaker and motor are used, regardless of cost. Otherwise what you save in any other choice of connector, will just get absorbed…
  • Gough Lui
    Gough Lui over 3 years ago +2
    Not sure what your Z-height requirements and mounting orientation will be, but JST SH 1mm connectors seem rather popular for smaller applications without being too esoteric. Otherwise it may just be…
  • charlieo21
    charlieo21 over 3 years ago +1
    Molex has this connector series with 1.2mm height. Pico-EZmate
Parents
  • Gough Lui
    0 Gough Lui over 3 years ago

    Not sure what your Z-height requirements and mounting orientation will be, but JST SH 1mm connectors seem rather popular for smaller applications without being too esoteric.

    Otherwise it may just be better to try and fabricate a flexible flat ribbon PCB to connect those items where you could potentially even go down to 0.5mm pitch.

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • frankcohen
    0 frankcohen over 3 years ago in reply to Gough Lui

    Thanks! The JST connectors look good and I'm going to investigate them more. It's a wrist watch project so the Z heigh needs to be 2 mm or less. The flex solution seems good and perhaps overkill. I can buy batteries with any connector, for example. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • frankcohen
    0 frankcohen over 3 years ago in reply to Gough Lui

    Thanks! The JST connectors look good and I'm going to investigate them more. It's a wrist watch project so the Z heigh needs to be 2 mm or less. The flex solution seems good and perhaps overkill. I can buy batteries with any connector, for example.