Internet of Things
  • Technologies
  • More
Internet of Things
Forum Shelly 1 interference with garage door remote
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 28 replies
  • Subscribers 514 subscribers
  • Views 6572 views
  • Users 0 members are here
  • shelly
  • shelly interference
  • garage door
Related

Shelly 1 interference with garage door remote

feiticeir0
feiticeir0 over 2 years ago

Hi all.

I'm having a problem with a shelly 1 and my garage door remote.

Recently I've connected my two garage door motors with shellys 1 .

One of them is working perfectly fine with the shelly safe inside the motor housing.

The other one, before the shelly, I was able to open the door with the remote from 10m-15m away (32 ft to 49 ft more or less). With the shelly connected, I'm only able to open the door with the remote, just from 5m (16ft) away.

The motor board is not the same - one is TE120 (working fine) and the other one is ATH10 (the situation described above).

image

image

One thing I did noticed was (the one where the distance was reduced), when I was testing, I had the shelly on a 10m (32ft) wire, rolled around an aluminum ladder on the wall and it was working fine. When I reduced the wire (to leave everything nice and tidy on the wall), this started to happen.

I use the same remote for both (different buttons) . I've switched the shellys - could it be a faulty one - but the problem remained.

Could a ferrite filter solve the problem ? Or at least attenuate some interference ?

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • feiticeir0
    feiticeir0 over 2 years ago +3
    UPDATE: I new that shelly could be powered by 24v DC, so I've procured a 24v output - the green PINS bottom left of the pictures - and after searching why I wasn't able to power the shelly with 24v (it…
  • Jan Cumps
    Jan Cumps over 2 years ago +3
    glad that it's OK now. When I had little children, the family on the other side of the street could not open their garage door when we had the baby-phone on. It took a while to make that connection…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to beacon_dave +3
    The high speed trains between Amsterdam and Antwerp would randomly fail after crossing the Dutch-Belgian border. Software would lock up. Took a while to solve that too ...
Parents
  • obones
    0 obones over 2 years ago

    Wouldn't adding a metallic shell around the ATH10 board be appropriate in this case?
    I mean, it seems it's the one doing the interference, so maybe it radiates too much and a grounded shield would sufficiently attenuate the interference

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • feiticeir0
    0 feiticeir0 over 2 years ago in reply to obones

    What do you mean ? The board is screwed to the casing. can I try with a aluminium foil and see ? Smiley

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • feiticeir0
    0 feiticeir0 over 2 years ago in reply to obones

    What do you mean ? The board is screwed to the casing. can I try with a aluminium foil and see ? Smiley

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • obones
    0 obones over 2 years ago in reply to feiticeir0

    I mean, creating a crude Farday cage around the board suspected of interfering with the proper functioning of the entire device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago in reply to obones

    the problem is that both of them are supposed to have radio transmission capability (gate motor to receive signal from remote and shelly to allow for control from the Internet) as I understand - but maybe modules can be shielded, with only antennas on the external side...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • feiticeir0
    0 feiticeir0 over 2 years ago in reply to JWx

    I've already tried to place the antenna outside the casing, but it didn't work... Disappointed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago in reply to feiticeir0

    so maybe if external antenna on remote working frequency can be found, it can be connected using shielded (coax) cable, moved some distance from the motor control unit and then shelly and control unit separated by some metal foil/sheet or even temporary metal box around shelly (maybe this tells us if interference is going through the air or by cables - but if it is working when shelly is connected using long cables I would suspect that interference is through the air)?