Internet of Things
  • Technologies
  • More
Internet of Things
Forum Shelly 1 interference with garage door remote
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 28 replies
  • Subscribers 514 subscribers
  • Views 6561 views
  • Users 0 members are here
  • shelly
  • shelly interference
  • garage door
Related

Shelly 1 interference with garage door remote

feiticeir0
feiticeir0 over 2 years ago

Hi all.

I'm having a problem with a shelly 1 and my garage door remote.

Recently I've connected my two garage door motors with shellys 1 .

One of them is working perfectly fine with the shelly safe inside the motor housing.

The other one, before the shelly, I was able to open the door with the remote from 10m-15m away (32 ft to 49 ft more or less). With the shelly connected, I'm only able to open the door with the remote, just from 5m (16ft) away.

The motor board is not the same - one is TE120 (working fine) and the other one is ATH10 (the situation described above).

image

image

One thing I did noticed was (the one where the distance was reduced), when I was testing, I had the shelly on a 10m (32ft) wire, rolled around an aluminum ladder on the wall and it was working fine. When I reduced the wire (to leave everything nice and tidy on the wall), this started to happen.

I use the same remote for both (different buttons) . I've switched the shellys - could it be a faulty one - but the problem remained.

Could a ferrite filter solve the problem ? Or at least attenuate some interference ?

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • feiticeir0
    feiticeir0 over 2 years ago +3
    UPDATE: I new that shelly could be powered by 24v DC, so I've procured a 24v output - the green PINS bottom left of the pictures - and after searching why I wasn't able to power the shelly with 24v (it…
  • Jan Cumps
    Jan Cumps over 2 years ago +3
    glad that it's OK now. When I had little children, the family on the other side of the street could not open their garage door when we had the baby-phone on. It took a while to make that connection…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to beacon_dave +3
    The high speed trains between Amsterdam and Antwerp would randomly fail after crossing the Dutch-Belgian border. Software would lock up. Took a while to solve that too ...
Parents
  • kmikemoo
    0 kmikemoo over 2 years ago

    feiticeir0 I did not find your Shelly board on the internet, however... if the wire closest the oscillator is your antenna, the lower picture appears to have a shorter one than the upper picture.  It's definitely a smaller gauge, but that shouldn't be of much impact.  Length does matter.  I would duplicate the length for the one that is operating correctly and try it on the other one.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • feiticeir0
    0 feiticeir0 over 2 years ago in reply to kmikemoo

    It's Shelly 1.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • feiticeir0
    0 feiticeir0 over 2 years ago in reply to feiticeir0

    You are correct. Those wires are the antenna.

    And the shorter one is the one working perfectly fine ! Smiley

    I can try to shorter the other one and see ! Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • feiticeir0
    0 feiticeir0 over 2 years ago in reply to feiticeir0

    You are correct. Those wires are the antenna.

    And the shorter one is the one working perfectly fine ! Smiley

    I can try to shorter the other one and see ! Slight smile