Internet of Things
  • Technologies
  • More
Internet of Things
Forum RE: Power Connection problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 518 subscribers
  • Views 495 views
  • Users 0 members are here
  • pico
  • raspberry_pi_3
Related

RE: Power Connection problem

GeoForeman
GeoForeman 3 months ago

Hi Everyone, I have a project  that needs to connect rp2040, rapsberry pi pico 0 to modules : HW‑357, 3.7v 4000mA battery, usb for charging, now for other sensors

Ky-008 ,HC-SR501 , NEO-M8, 3V-5V DC vibration motors ,microSD card breakout board / microSD card Adapter, please include the breadboard..

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 3 months ago in reply to dang74 +4
    If you must have 3.3V you will have a hard choice. To get the most out of a nominal 3.7V Lithium Ion battery you would like to run it down to 3V or even 2.7V. Fully charged it will deliver 4V. For…
  • dougw
    dougw 3 months ago +1
    The battery could have a max voltage higher than its nominal 3.7V , maybe as high as 4.2 V. Pico has a regulator that outputs 3.3V and expects interface signals to be 3.3V compatible. Do you have a specific…
  • dougw
    dougw 3 months ago in reply to dang74 +1
    Systems that require multiple supply voltages are very common and it is much simpler now to use efficient switching converters to meet these requirements than it used to be. It is very common to generate…
Parents
  • dougw
    dougw 3 months ago

    The battery could have a max voltage higher than its nominal 3.7V , maybe as high as 4.2 V. Pico has a regulator that outputs 3.3V and expects interface signals to be 3.3V compatible. Do you have a specific question about the peripherals you mentioned? Are you looking for a schematic?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 3 months ago in reply to dougw

    In the future I was considering starting a project that will use a chargeable battery.  I was thinking of having a SEPIC converter between the battery and my downstream 3.3V devices.  The thought process being that it could handle the higher than expected voltages like the 4.2V that you cite and also keep ticking as the battery voltage gets depleted.  Do you know if this is a common approach?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw 3 months ago in reply to dang74

    Systems that require multiple supply voltages are very common and it is much simpler now to use efficient switching converters to meet these requirements than it used to be. It is very common to generate high voltages with step-up converters. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw 3 months ago in reply to dang74

    Systems that require multiple supply voltages are very common and it is much simpler now to use efficient switching converters to meet these requirements than it used to be. It is very common to generate high voltages with step-up converters. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dang74
    dang74 3 months ago in reply to dougw

    Thanks dougw