Internet of Things
  • Technologies
  • More
Internet of Things
Forum Which sensor to use for detection of Humans Climbing Poles
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 524 subscribers
  • Views 2257 views
  • Users 0 members are here
  • frontpage
  • proximity sensors
  • aurdino
  • ras pi 3
Related

Which sensor to use for detection of Humans Climbing Poles

davetechnosis
davetechnosis over 9 years ago

My Use Case

 

Our client is in Power Generation business. There have more than 3000 poles to transfer power from production to power grid. The distance between each pole is 400 meters. Most of the wires are having active current, but the ones at the low level are used for earthing and dont have any power supply.

 

The line passes through remotest areas of India and consequently, the locals cut the Earthing wire (no active current) and sell them in market. Motion detection camera is one of the option but that creates false alarms. I am looking for a sensor where in any human is trying to climb the pole, the camera gets active and takes snap of the user trying to climb.

 

What kind of sensor can be used for this use case? We need to detect it from the proximity of 5 meters.

 

The image of the pole is here: https://blogs-images.forbes.com/stevensalzberg/files/2014/08/670px-power_lines.jpg

  • Sign in to reply
  • Cancel

Top Replies

  • michaelwylie
    michaelwylie over 9 years ago +3
    This is already done in industry. The presence of the electric fields means the best solution will be fiber optic sensing. Fiber is immune to EMI. If you are serious about it, you can message me on here…
  • kas.lewis
    kas.lewis over 9 years ago +2
    The motion scene camera connected to image recognition to look for a person. That may be one solution. Also if you cap sense where you are looking for a signature of a human body, this would take some…
  • davetechnosis
    davetechnosis over 9 years ago in reply to dougw +2
    Ya, I wish, but the issue with IR is that it makes false alarms as even birds are routine visitors.
Parents
  • DAB
    DAB over 9 years ago

    It might be easy to establish a capacitive sensing system, but I am not sure they could detect at the 5 m range.

     

    It might be possible to set up a ground grid capacitive sensor, but I am not sure it would be cost effective.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • davetechnosis
    davetechnosis over 9 years ago in reply to DAB

    Sounds like a good idea. Shall try and do the pilot. Lets see.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • davetechnosis
    davetechnosis over 9 years ago in reply to DAB

    Sounds like a good idea. Shall try and do the pilot. Lets see.