Medical
  • Technologies
  • More
Medical
Blog ECG signal amplication
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Medical to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 11 May 2014 12:29 AM Date Created
  • Views 2717 views
  • Likes 2 likes
  • Comments 7 comments
Related
Recommended

ECG signal amplication

e14 Contributor
e14 Contributor
11 May 2014

Good morning.

I just received my Raspberry Pi. I am a very very beginner, with some knowledge in programming, trying to learn JAVA but a dummy in electronics.

Could someone tell me how to amplify an ECG signal so that it can be "seen" by the GPIO? Between 1 and 5 mV.

Thank you very much.

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 12 years ago in reply to dougw +1
    Be very careful using devices like RPI as ECGs. There are strict standards for medical equipment connected to the mains, even via PCs, USB or power supply bricks and it is unlikely that the typical cheapo…
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +1
    I don't want to be a total PITA but you are replying to a 7 month old post with a link to a paper which can only be accessed by paying money. What am I missing here ? MK
Parents
  • sunnyiut
    sunnyiut over 12 years ago

    Hello,

    between 1 and 5mV !!! or 0 and 3.3V? I think the GPIO has input voltage 0v and 3.3v

    however, diagnostic systems use 12 LEAD ECG, but for monitoring purpose u just need 3 LEADs [limb leads]. Frequencies between 0.05Hz to 150Hz would be good enough. For just monitoring a single Lead the following block diagram can meet the purpose. While you may need to vary the 2nd stage gain [Gain-25] according to your voltage range. A level shifter will be necessary if you use dual power supply.

    image

    Say for LEAD1 you need to connect the LA at the non-inverting input of INA [instrumentation amplifier] and the RA at the inverting input. You will need another electrode which will be connected at the RL as reference [GND]. You can go for RLD [right leg drive] to reduce the line power noise. where the signal is inverted and driven back into the patient through the right leg by an amplifier. you can get the signals without RLD, but it will be a little bit noisy. as you are using Pi, you can implement a 50/60Hz notch filter in your firmware which will improve the signal a lot.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sunnyiut
    sunnyiut over 12 years ago

    Hello,

    between 1 and 5mV !!! or 0 and 3.3V? I think the GPIO has input voltage 0v and 3.3v

    however, diagnostic systems use 12 LEAD ECG, but for monitoring purpose u just need 3 LEADs [limb leads]. Frequencies between 0.05Hz to 150Hz would be good enough. For just monitoring a single Lead the following block diagram can meet the purpose. While you may need to vary the 2nd stage gain [Gain-25] according to your voltage range. A level shifter will be necessary if you use dual power supply.

    image

    Say for LEAD1 you need to connect the LA at the non-inverting input of INA [instrumentation amplifier] and the RA at the inverting input. You will need another electrode which will be connected at the RL as reference [GND]. You can go for RLD [right leg drive] to reduce the line power noise. where the signal is inverted and driven back into the patient through the right leg by an amplifier. you can get the signals without RLD, but it will be a little bit noisy. as you are using Pi, you can implement a 50/60Hz notch filter in your firmware which will improve the signal a lot.