Medical
  • Technologies
  • More
Medical
Blog Surgeon uses Kinect imaging system to repair aneurism in aorta
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Medical to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 18 May 2012 5:52 PM Date Created
  • Views 1107 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • test
  • microsoft
  • industry
  • hmi
  • medtronic
  • embedded
  • cabeatwell
  • prototyping
  • measurement
  • surgery
  • mro
  • medical
  • automation
  • kinect
  • sensor
  • innovation
Related
Recommended

Surgeon uses Kinect imaging system to repair aneurism in aorta

Catwell
Catwell
18 May 2012

image

Image that was controlled via Kinect during operation. (via Microsoft)

 

The Kinect imaging sensor has been used in some technically innovative projects such as Queen’s University’s 3D video conferencing system to Microsoft’s own augmented reality MirageTable. It’s even found its way into the medical field with a recent successful operation involving the repair of an aneurism at Guy’s and St Thomas’ hospital in London.

 

Surgeons involved in complex operations occasionally need to refer to reference material to help them through certain procedures. This is typically done by using an assistant to bring up the materials on a laptop so the doctor can remain at the operating table without having to waste time re-scrubbing because of contamination. This is where a new 3D imaging system that was developed by Microsoft Research Cambridge with Guy’s and St Thomas’ hospital can be invaluable as it was used for the first time by assistant surgeon Tom Carrell to perform heart surgery.

 

image

Promotional image of the Kinect during surgery. (via Microsoft & St. Thomas' Hospital)

 

The system was used to compare a 3D model of an aorta with a live-feed 2D image of the patient's by using a fluoroscopic x-ray camera to help Carrell navigate through the delicate procedure. The 3D model could also be manipulated through a series of minimal gestures that include the ability to rotate the image using the palm of your hand and placing a marker simply by pointing and using a voice command. These simple gestures can be performed using only one hand leaving the other to continue the surgery while others, such as panning, rotating or zooming in/out need the use of both hands. Not only can the system be used in confined spaces commonly found in operating theaters, it also saves valuable time in eliminating the need to take a break to consult reference material.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    Very impressive, but I think we are just seeing the tip of the revolution in medical device enhancements.

     

    Face it, the better the doctor feels about operating on things they cannot readily see, the safer medical care will get.

     

    good post.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    Very impressive, but I think we are just seeing the tip of the revolution in medical device enhancements.

     

    Face it, the better the doctor feels about operating on things they cannot readily see, the safer medical care will get.

     

    good post.

    DAB