Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum need help with a stepper driver
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 3 answers
  • Subscribers 77 subscribers
  • Views 4827 views
  • Users 0 members are here
  • help
  • stepper_motor
  • manual
  • motor_driveboard
  • instruction_manual
  • stepper_driver
  • motor_control_drive
  • instruction
  • help_required
  • division_setting_table
  • motor
  • arduino
  • motor_circuits
  • stepper_drive
Related

need help with a stepper driver

e14 Contributor
e14 Contributor over 13 years ago

imageimageimageimageimageimage

this is a 2-phase stepper motor drive by a chinese company called SCKJMOTOR with the model number SC2680MH

it can be found here in this link http://sckjmotor.com/prodetail.asp?cid=3&scid=6&id=67

i am not much experienced with electronics so i cant figure out how to use it with out an instruction manual and sadly the manual is in chinese image

so i thought maybe i can find some help here on element 14

 

you can see in the pictures  the driver has lots off ports on it they go like  + , PU, + , DR, + , MF, + ,  TM, +V, -V, +A, -A, +B, -B

 

here i think the " + " ports might be a 5V input so i guess i must give 5V in them, but why are there so many???? why do i need to give the driver 5V at 4 different ports ???   image

 

the port " PU " might be pules, i am just guessing, it might be to control the speed of the motor  

 

the port " DR " maybe direction like forward-reverse, another guess 

 

the port " MF " i have no idea, cant even guess this one   image

 

the ports " +V " and " -V" the driver says on the side " DC24-80V "  so i guess i might have to give it some thing between 24V to 80V

 

the posts  +A, -A, +B, -B  are clear i guess, i just have to find the right coil pairs of the stepper motor and connect it to these ports  image 

 

there is also some thing called a division setting table and it gives me values  1, 2, 4, 8, 16, 32, 64 and 128 , i think this must be some thing related to the step divisions of the stepper motor, need some help with that as well

 

please try to help me out with this, i am just starting to take interset in electronice and dont have any experience in this at all, just have some basic electronic knowledge since i am doing engineering and its my 1st year

 

thank you

  • Sign in to reply
  • Cancel
Parents
  • bodgy
    0 bodgy over 13 years ago

    There are some Cantonese speaking people at work, but I'm on day off today, so it would be tomorrow before I could see if they would translate the datasheet for you.

     

    Looking at the wiring diagram from the link you posted.

     

    It does indeed look as though there are three + connections to 5v (perhaps there are 3 internal modules, I don't know). I thought MF might be the 'motor frame' connection, or to you and me, the ground/-v connection, on the other hand there is a timing diagram of a low to high pulse requiring 1uS rise time, so I'm not entirely sure. The wiring diagram has bracketed text underneath that wire, which normally means used or not used under certain conditions.

     

    As there is a timing diagram attached to the PU and DR, as you surmise the PU might well be the PWM drive pulse active on the high to low edge, my first thought was the same as you for DR, possible direction, but by the looks of the timing diagram it does something by going high to low 2.5uS whilst PU is high and before the PU pulses start, MF needs to be low to high before DR goes low.

     

    D4,5,6 switches are indeed the pulse step setting. D2 appears to change the way PU and DR relate to each other. D1 looks as though it might either change the PWM frequency or perhaps provides always on, always off and PWM modes of driving a motor. D3 haven't the faintest idea image .

     

    *******************************EDIT**************************************

     

    PU = PWM = motor speed.

     

     

    DR: Depends on setting of D2 , if D2 is ON it looks as though DR is the direction control by voltage, if D2 is OFF then it appears to require a pulse of some kind, without an actual translation that is just a guess.

     

    D3 is not used by this module currently.

     

    Colin

     

    Message was edited by: Colin Barnard   : Just looked at your images properly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bodgy

    thank you very much for your help, appreciate it alot image

    please dont mind but i did not understand you completely because i have very less knowledge and experience, even my university professors are not very helpful with outside syllabus topics  image

     

    ok so what i understand from you is

     

    ill just give 5V in all the " + " ports 

     

    the PU ill just connect the microcontroller and make it give no off signals with 1uS delay depending on the speed i want 

     

    D1   says its for self test  when ON, i guess its just used to check if the motor is running and the connections are right 

     

    D2  says if  OFF = PU + DR    i still need little more detail info on DR  if its not direction then what is it exactly 

                  if  ON   = CW/CCW    i have no idea  image  whats CW whats CCW ???

     

    MF  , what is  motor frame ???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 13 years ago in reply to e14 Contributor

    I would input 5V to PU/DR+ and then connect the other connections as described (or how you understand them to be connected) and then just try diffrent things. I might suggest if you can get an O-scope or use one at the university that would give you better info then connecting to a motor at this point.

     

    And you do NOT need to connect MF to anything for now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kas.lewis
    0 kas.lewis over 13 years ago in reply to e14 Contributor

    I would input 5V to PU/DR+ and then connect the other connections as described (or how you understand them to be connected) and then just try diffrent things. I might suggest if you can get an O-scope or use one at the university that would give you better info then connecting to a motor at this point.

     

    And you do NOT need to connect MF to anything for now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to kas.lewis

    there are four + ports so ill give 5V to all

     

    but PU and DR shouldnt they be connected to a mircocontroller ????? or any other controller

     

    ill ignore MF 

     

    and what about TM whats zero point, little more detail please is it some thing like reset or start position

     

    and the +V and -V  do i put like 24 V  there  its say DC24-80V    

     

    just trying to be safe, i hope i dont burn it 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 13 years ago in reply to e14 Contributor

    I understand what you are saying about PU/DR, but from the schematic it looks like the pos are cennected  5V and neg to the controller (the controller could be used a s a pull down instead of a pull up, I am assuming). If you do this be sure the uC pins are rated at 5V.

    TM we could not fully understand but we understoof something about zero point, what that means we are unsure.

     

    +V and -V does look like it is connected to 24V

     

    Hope someone else can help explain teh setup, these are my assumtions from what I understood, maybe someone else can give some input as well.