Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Bridgetek EVE Series - Touch Enabled Graphical User Interfaces
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: BRT-Marketing
  • Date Created: 26 Jan 2024 6:40 AM Date Created
  • Views 2504 views
  • Likes 4 likes
  • Comments 11 comments
  • graphical interface
  • bridgetek
  • eve
Related
Recommended

Bridgetek EVE Series - Touch Enabled Graphical User Interfaces

BRT-Marketing
BRT-Marketing
26 Jan 2024

Bridgetek’s products include the EVE family of display controllers which make it easy to add attractive and fully featured touch-enabled graphical user interfaces to existing and new product designs.

To improve the user experience and functionality, EVE devices can be used to upgrade the user interface of a wide range of devices including industrial machines (industrial controllers, machine tools, elevators) and household appliances, and in consumer electronics devices and many more applications.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The flexibility of EVE series is that it can be driven by any low-cost MCU over SPI. This allows existing equipment / products to be easily upgraded by adding colour graphics and touch with minimal impact to the existing design.

Another advantage of the EVE series is the EVE Toolchain programming tools, which significantly facilitate and speed up the process of designing with displays, especially in the field of extensive graphical user interfaces.

Our family of MCUs are optimized for high-speed interface bridging tasks to a wide range of protocols including USB Host, USB Device, SD Host, Ethernet, SPI, I2C, DAC, ADC, PWM, CAN and Camera Interface, these are available on the Bridgetek.

We have a downloadable Free Toolchain with a wide range of examples and easy prototyping by using development modules.

  • Sign in to reply
Parents
  • balajivan1995
    balajivan1995 over 2 years ago

    Do you offer any round display with touch screen ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balajivan1995
    balajivan1995 over 2 years ago

    Do you offer any round display with touch screen ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • BRT-Marketing
    BRT-Marketing over 2 years ago in reply to balajivan1995

    Hello, thanks for your question, yes you can use a wide range of displays including circular ones of different sizes with our EVE display controllers. We have a demo which uses a circular screen, which has capacitive touch, with our BT881 EVE device. You can see the demo here: Bridgetek Inclinometer Video (youtube.com). We don't manufacture the circular display itself but you can use EVE to drive them. Let us know if you have any questions about using EVE with the display.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to balajivan1995

    BuyDisplay (nice name - straight to the point!) have round displays. I've not purchased round displays from BuyDisplay, but have purchased rectangular LCD screens (with and without touch) from them in the past. They seem reliable, and some of their displays are available for a long term.

    There's lots of source code around for many of the controllers they use (e.g. RA8875 chip is easy to drive), so there's tons of community support around (and nowadays sometimes community support is better than what firms offer themselves).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 2 years ago in reply to balajivan1995

    They do not provide displays. You can use any display you want as long as it has compatible interface: parallel RGB. Some other interfaces are possible with converters. For example their eval boards frequently have onboard converter for LVDS. Touch controllers have usualy I2C interface. Their chips contains blob for handling communication with some chips which highly simplify their usage. If you select display with unsupported touch controller you can try find patch on their forum, then you will upload blob of binary code and then you can get touches using the same simple interface. If you do not find patch enywhere, you need to handle communication with chip yourself.

    I wrote review of their eval board and chip few years ago: /products/roadtest/rv/roadtest_reviews/1498/bridgetek_embedded_v_2. SInce that time they extended offer by automotive variants of chips and added new chips with some new capabilities as well as cheaper chips with some reductions for reducing cost.