Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Bridgetek EVE Series - Touch Enabled Graphical User Interfaces
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: BRT-Marketing
  • Date Created: 26 Jan 2024 6:40 AM Date Created
  • Views 2214 views
  • Likes 4 likes
  • Comments 11 comments
  • graphical interface
  • bridgetek
  • eve
Related
Recommended

Bridgetek EVE Series - Touch Enabled Graphical User Interfaces

BRT-Marketing
BRT-Marketing
26 Jan 2024

Bridgetek’s products include the EVE family of display controllers which make it easy to add attractive and fully featured touch-enabled graphical user interfaces to existing and new product designs.

To improve the user experience and functionality, EVE devices can be used to upgrade the user interface of a wide range of devices including industrial machines (industrial controllers, machine tools, elevators) and household appliances, and in consumer electronics devices and many more applications.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The flexibility of EVE series is that it can be driven by any low-cost MCU over SPI. This allows existing equipment / products to be easily upgraded by adding colour graphics and touch with minimal impact to the existing design.

Another advantage of the EVE series is the EVE Toolchain programming tools, which significantly facilitate and speed up the process of designing with displays, especially in the field of extensive graphical user interfaces.

Our family of MCUs are optimized for high-speed interface bridging tasks to a wide range of protocols including USB Host, USB Device, SD Host, Ethernet, SPI, I2C, DAC, ADC, PWM, CAN and Camera Interface, these are available on the Bridgetek.

We have a downloadable Free Toolchain with a wide range of examples and easy prototyping by using development modules.

  • Sign in to reply
  • balajivan1995
    balajivan1995 over 2 years ago in reply to shabaz

    I checked the specs. It is also a GC9A01 based display. I think the Tom & Jerry image on display is probably edited and not rendered. I feel like I can't escape from GC9A01. Joy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BRT-Marketing
    BRT-Marketing over 2 years ago in reply to balajivan1995

    Hello, thanks for your question, yes you can use a wide range of displays including circular ones of different sizes with our EVE display controllers. We have a demo which uses a circular screen, which has capacitive touch, with our BT881 EVE device. You can see the demo here: Bridgetek Inclinometer Video (youtube.com). We don't manufacture the circular display itself but you can use EVE to drive them. Let us know if you have any questions about using EVE with the display.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balajivan1995
    balajivan1995 over 2 years ago in reply to shabaz

    We have placed an order for m5dial. Which is also based on GCxxxx but with a touch controller as well.

    I'll ask my manager to approve the purchase of buydisplay version.We already have a similar 8051 based development board that we acquired from a Chinese vendor. Hopefully customs won't be a pain in the butt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to balajivan1995

    Great!

    That display controller by the way is the same one that is used in the Hackaday VectorScope project  Building a Hackaday “Vectorscope” Badge: DIY Guy Fawkes Edition (which I still need to complete; I'm quite keen to develop a simple circular GUI, and a few circular charting methods). They used a version without touch-screen however. You could check their GitHub site for the source code to drive the display (they used a Pi Pico, but the code should be transferrable. In any case, I'm sure there are plenty of ESP32 examples for that controller too. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balajivan1995
    balajivan1995 over 2 years ago in reply to shabaz

    Thank you very much! The 1.28" display looks nice and crisp. We prefer capacitive touch displays, preferably driven by ESP32. I think I'll give it a try. Alternative option is buying the STM32 dk board with touch display that was in roadtest few months ago. ESP32 makes it easier to update the entire UI design remotely using Wifi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>