Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Copper Clad Prototyping Tools
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 30 Aug 2021 3:17 PM Date Created
  • Views 6285 views
  • Likes 15 likes
  • Comments 19 comments
  • pcb making
  • engraver
  • copper islands
Related
Recommended

Copper Clad Prototyping Tools

shabaz
shabaz
30 Aug 2021

Following on from a Project14 discussion DIY 100kHz VCO - Build & Test  on copper-clad board techniques for prototyping, I was curious to know how I could improve my current method of using a craft knife to cut channels for creating isolated pads and islands on the boards. navadeepganeshu  suggested using a Perspex cutter, which I have yet to try. I also attempted to use a scriber with a ground-out channel.

 

I posed the question on a DIY group channel I'm part of with a few old school friends. They suggested I try an electric engraver, or a 'scorper' or 'graver' tool (these tools are used by jewellers for cutting lines and channels in metal).

So, I gave it a shot, using the tools below.

image

I was really surprised at the quality of the engraver - it was under $20, and seems well made. I don't know if it will last, my main concern was that the grub screws that hold the shaft of the cutter are quite small and I didn't want to over-tighten them in case the screw thread gets torn. Maybe I'm over-worrying, but I will try to find slightly longer grub screws. Aside from that, it all seems like a very neat tool.

 

However I think I may end up using the second tool, the scorper, a lot more, simply because it won't generate dust as the engraver will.

 

The 4-minute video below shows the tools in use.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Any other suggestions or ways to improve these techniques would be great to hear!

  • Sign in to reply
Parents
  • rsjawale24
    rsjawale24 over 5 years ago

    The easiest solution I found out was to use 0.8mm thick FR-4 instead of 1.6mm.

    Unless you have proper tools, you don't get a good edge finish with 1.6mm. So I switched to 0.8mm FR-4. It's easy to cut with large scissors or a sheet metal cutter and the surface edge finish is also good.

    The only drawback is 0.8mm FR-4 is slightly expensive than 1.6mm board.

     

    P.S: I often fabricate antennas and the alignment is necessary between the ground plane (which often is defected ground) and the radiator, hence I need good surface finish as I use the surface edge as a alignment guide for the masks.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rsjawale24
    rsjawale24 over 5 years ago

    The easiest solution I found out was to use 0.8mm thick FR-4 instead of 1.6mm.

    Unless you have proper tools, you don't get a good edge finish with 1.6mm. So I switched to 0.8mm FR-4. It's easy to cut with large scissors or a sheet metal cutter and the surface edge finish is also good.

    The only drawback is 0.8mm FR-4 is slightly expensive than 1.6mm board.

     

    P.S: I often fabricate antennas and the alignment is necessary between the ground plane (which often is defected ground) and the radiator, hence I need good surface finish as I use the surface edge as a alignment guide for the masks.

    • Cancel
    • Vote Up +4 Vote Down