• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Discrete difference amplifier - AC analysis: gain and bandwidth
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 14 Jul 2026 6:26 PM Date Created
  • Views 421 views
  • Likes 7 likes
  • Comments 13 comments
  • simple_dcr
Related
Recommended

Discrete difference amplifier - AC analysis: gain and bandwidth

Jan Cumps
Jan Cumps
14 Jul 2026

This is the AC gain and BW analysis of the difference amplifier module that shabaz designed for a Direct Conversion Receiver.

image

I'm searching for these points:

  • gain at 1 kHz (approx. mid of bandwidth)
  • -3 dB frequencies

I use Vrms values in the post - common for audio circuits. When measuring one of the differential channels, I tie the other to ground.

image

Specs:

  • Gain: ~10 dB
  • Bandwidth (-3 dB): ~30 Hz to 40 kHz (approximate)

Measurements:

image

IN1: gain (1 kHz): 9.2 dB, bw (-3 dB): 30 Hz - 80 kHz

IN2: gain (1 kHz): 9.3 dB, bw (-3 dB): 30 Hz - 80 kHz

image

 shabaz published the KiCad project on GitHub, including simulation. You could load it into KiCad and check if the small signal simulation and my measurements match ...

For all blog posts in this series, click here

spreadsheet: differenceamp.zip

  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps 2 months ago

     shabaz , the current source in the tail of the differential amp (orange area below):

    image

    what was your inspiration to design that sub-circuit that way?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 2 months ago in reply to Jan Cumps

    From memory I originally didn't have any of that, and used a resistor, but needed beyond a certain value to then be able to have lower gain and low distortion (since this stage wasn't intended to have high gain; I would have been happy with just 6 dB or so) but couldn't find a combination that would also give me a good signal input range (I needed at least several hundred mV to suit the circuitry preceeding it).

    Eventually I gave up and tried the BJT current sink, there may well be more optimal biasing that could have eliminated the need for the BJT sink at all, I just couldn't find it through trial-and-error (I'm not an analog designer otherwise I may have known a better technique). (By trial-and-error I mean using the KiCad simulator).

    Once I went down that road although I took some time on it, I believe better results could be achieved. I likely just started with one transistor and then for some reason switched to the darlington pair, but there are better current sink topologies. For the combination of relatively large input (few hundred mV p-p), what seemed like good common signal rejection, low desired gain and low distortion in the speech bandwidth, the tweaks had reached a point where the simulator results suggested there was no need to improve further.

    I was finding it took ages to find something optimal since there are two inputs and I'd have to keep changing the signals to check it was still working fine across these requirements.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz 2 months ago in reply to Jan Cumps

    From memory I originally didn't have any of that, and used a resistor, but needed beyond a certain value to then be able to have lower gain and low distortion (since this stage wasn't intended to have high gain; I would have been happy with just 6 dB or so) but couldn't find a combination that would also give me a good signal input range (I needed at least several hundred mV to suit the circuitry preceeding it).

    Eventually I gave up and tried the BJT current sink, there may well be more optimal biasing that could have eliminated the need for the BJT sink at all, I just couldn't find it through trial-and-error (I'm not an analog designer otherwise I may have known a better technique). (By trial-and-error I mean using the KiCad simulator).

    Once I went down that road although I took some time on it, I believe better results could be achieved. I likely just started with one transistor and then for some reason switched to the darlington pair, but there are better current sink topologies. For the combination of relatively large input (few hundred mV p-p), what seemed like good common signal rejection, low desired gain and low distortion in the speech bandwidth, the tweaks had reached a point where the simulator results suggested there was no need to improve further.

    I was finding it took ages to find something optimal since there are two inputs and I'd have to keep changing the signals to check it was still working fine across these requirements.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jc2048
    jc2048 2 months ago in reply to shabaz

    "...since there are two inputs and I'd have to keep changing the signals..."

    Something that's handy for these kind of situations are the controlled sources in spice. Here I've got a voltage-controlled voltage source on the second input controlled by the generator on the first. If I set the controlled source gain to -1, then the second input is simply the inverse of whatever the generator is set to, and if I set the gain to 1, both inputs are the same and the second tracks the generator.