• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Discrete difference amplifier - AC analysis: gain and bandwidth
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 14 Jul 2026 6:26 PM Date Created
  • Views 428 views
  • Likes 7 likes
  • Comments 13 comments
  • simple_dcr
Related
Recommended

Discrete difference amplifier - AC analysis: gain and bandwidth

Jan Cumps
Jan Cumps
14 Jul 2026

This is the AC gain and BW analysis of the difference amplifier module that shabaz designed for a Direct Conversion Receiver.

image

I'm searching for these points:

  • gain at 1 kHz (approx. mid of bandwidth)
  • -3 dB frequencies

I use Vrms values in the post - common for audio circuits. When measuring one of the differential channels, I tie the other to ground.

image

Specs:

  • Gain: ~10 dB
  • Bandwidth (-3 dB): ~30 Hz to 40 kHz (approximate)

Measurements:

image

IN1: gain (1 kHz): 9.2 dB, bw (-3 dB): 30 Hz - 80 kHz

IN2: gain (1 kHz): 9.3 dB, bw (-3 dB): 30 Hz - 80 kHz

image

 shabaz published the KiCad project on GitHub, including simulation. You could load it into KiCad and check if the small signal simulation and my measurements match ...

For all blog posts in this series, click here

spreadsheet: differenceamp.zip

  • Sign in to reply
Parents
  • shabaz
    shabaz 2 months ago

    Hi Jan,

    Very useful information! I had not got the stripboard prototype working too well (I probably made a soldering or component error somewhere) so it is great to see these real measurements with the PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz 2 months ago

    Hi Jan,

    Very useful information! I had not got the stripboard prototype working too well (I probably made a soldering or component error somewhere) so it is great to see these real measurements with the PCB.