Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Easy Xmas Gift: Simple LED Name Signs or Night-Lights
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 8 Dec 2025 12:53 PM Date Created
  • Views 1397 views
  • Likes 14 likes
  • Comments 10 comments
  • xmas
  • led
  • gift
  • christmas
Related
Recommended

Easy Xmas Gift: Simple LED Name Signs or Night-Lights

shabaz
shabaz
8 Dec 2025

I had a small request from a friend to produce a night-light that spelled out his kids' names.

This turned out to be a very easy project.

image

I obtained quarter-circle wood dowel with a 45-degree cut on the inside, instead of a sharp 90 degree corner. This is a standard thing from DIY stores.

Good quality double-sided tape was applied to an inside edge, and then I stuck on 30mm-high LED characters obtained from AliExpress. They are soldered in series, using thin bare wire, and then a length of two-core wire can be attached to the two remaining ends.

After that, more double-sided tape was applied on top, and then the second dowel piece was pushed against it, to form a semi-circle. Everything was then secured with epoxy glue. Some black adhesive tape (maybe fabric or felt) can be put on the underside afterwards, to hide wires.

image

Here's the end view:

image

I don't know the specifications of the LED characters, so I just drove them with constant current. Each character has a forward voltage of about 3V.

I used a ready-made DC-DC converter board that accepts 5V from a USB phone charger and outputs about 23V. That's the blue board in the photo below.

The green board in the photo is a constant current driver that accepts 6-24V input, and outputs an adjustable current value (there is a tiny trimmer potentiometer). 

image

As well as the trimmer potentiometer, there is also a small resistor that sets the maximum current. I desoldered that resistor and swapped it with a 2.7 ohm part, which should limit the maximum current to a few tens of milliamps (I didn't measure). The brightness seems fine with the trimmer resistor just set to the middle position.

image(Image source: AliExpress)

An enclosure could be 3D-printed, but I crudely milled out a piece of wood. I will fill one end with black PolyDoh, and then close it up with a thin piece of wood.

Of course, this project could be improved a lot, it would be great to hear your thoughts.

Thanks for reading!

  • Sign in to reply
Parents
  • genebren
    genebren 10 months ago

    Very nice!  My granddaughter has asked for some LED lighting creation for her room.  We are going to do some planning over the weekend.  I will have to share this as a possible part of her design. Well done!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 10 months ago in reply to genebren

    Bright blue LEDs aimed at her pillow Grin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps 10 months ago in reply to genebren

    Bright blue LEDs aimed at her pillow Grin