Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Easy Xmas Gift: Simple LED Name Signs or Night-Lights
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 8 Dec 2025 12:53 PM Date Created
  • Views 1465 views
  • Likes 14 likes
  • Comments 10 comments
  • xmas
  • led
  • gift
  • christmas
Related
Recommended

Easy Xmas Gift: Simple LED Name Signs or Night-Lights

shabaz
shabaz
8 Dec 2025

I had a small request from a friend to produce a night-light that spelled out his kids' names.

This turned out to be a very easy project.

image

I obtained quarter-circle wood dowel with a 45-degree cut on the inside, instead of a sharp 90 degree corner. This is a standard thing from DIY stores.

Good quality double-sided tape was applied to an inside edge, and then I stuck on 30mm-high LED characters obtained from AliExpress. They are soldered in series, using thin bare wire, and then a length of two-core wire can be attached to the two remaining ends.

After that, more double-sided tape was applied on top, and then the second dowel piece was pushed against it, to form a semi-circle. Everything was then secured with epoxy glue. Some black adhesive tape (maybe fabric or felt) can be put on the underside afterwards, to hide wires.

image

Here's the end view:

image

I don't know the specifications of the LED characters, so I just drove them with constant current. Each character has a forward voltage of about 3V.

I used a ready-made DC-DC converter board that accepts 5V from a USB phone charger and outputs about 23V. That's the blue board in the photo below.

The green board in the photo is a constant current driver that accepts 6-24V input, and outputs an adjustable current value (there is a tiny trimmer potentiometer). 

image

As well as the trimmer potentiometer, there is also a small resistor that sets the maximum current. I desoldered that resistor and swapped it with a 2.7 ohm part, which should limit the maximum current to a few tens of milliamps (I didn't measure). The brightness seems fine with the trimmer resistor just set to the middle position.

image(Image source: AliExpress)

An enclosure could be 3D-printed, but I crudely milled out a piece of wood. I will fill one end with black PolyDoh, and then close it up with a thin piece of wood.

Of course, this project could be improved a lot, it would be great to hear your thoughts.

Thanks for reading!

  • Sign in to reply
Parents
  • colporteur
    colporteur 10 months ago

    What did it take you for time?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 10 months ago in reply to colporteur

    Hi! Sorry for the delayed response. I batched up several together, and managed to do three of them in a day while doing other things while glue was drying etc.

    Here are some more photos showing detail:

    The DC-DC converter board is adjusted to 23V first, before soldering it to the Constant Current Board (which has a 24V max limit). There is a resistor which is replaced with 2.7 ohm, to reduce the current output.

    image

    Next, I got the stick of wood dowel, applied a layer of double-sided tape and stuck on the characters:

    image

    Then just solder the LED characters in series, and attach the ends to the cable: 

    image

    I applied a layer of double-sided tape on top, and then optionally dremel some notches on the second piece of dowel, if you want it to fit a bit better, but it's not necessary.

    image

    This is what the underside now looked like, with the two pieces of wood pressed together: 

    image

    To make it more permanent, I applied some epoxy glue at the ends of the groove, and put some temporary tape on top until the glue dried (and then remove the tape).

    image

    Finally I applied some black tape to make it look nicer. Job done.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz 10 months ago in reply to colporteur

    Hi! Sorry for the delayed response. I batched up several together, and managed to do three of them in a day while doing other things while glue was drying etc.

    Here are some more photos showing detail:

    The DC-DC converter board is adjusted to 23V first, before soldering it to the Constant Current Board (which has a 24V max limit). There is a resistor which is replaced with 2.7 ohm, to reduce the current output.

    image

    Next, I got the stick of wood dowel, applied a layer of double-sided tape and stuck on the characters:

    image

    Then just solder the LED characters in series, and attach the ends to the cable: 

    image

    I applied a layer of double-sided tape on top, and then optionally dremel some notches on the second piece of dowel, if you want it to fit a bit better, but it's not necessary.

    image

    This is what the underside now looked like, with the two pieces of wood pressed together: 

    image

    To make it more permanent, I applied some epoxy glue at the ends of the groove, and put some temporary tape on top until the glue dried (and then remove the tape).

    image

    Finally I applied some black tape to make it look nicer. Job done.