Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Kelvin (4-Wire) Milliohm Meter:  Version 1.3
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 24 Jan 2019 7:51 AM Date Created
  • Views 5640 views
  • Likes 13 likes
  • Comments 19 comments
  • kelvin measurement
  • op amp
  • 4 wire measurement
  • instrument op amp
  • milliohm measurement
  • milliohm
  • milliohm meter
Related
Recommended

Kelvin (4-Wire) Milliohm Meter:  Version 1.3

fmilburn
fmilburn
24 Jan 2019

This post documents Version 1.3 of an inexpensive but reasonably accurate meter for measuring resistance in the milliohm range. The development to date is documented in the links at the bottom of this post.  Version 1.3 contains numerous upgrades and suggestions from Shabaz, Gene Breniman, John Wiltrout, and Jon Clift to which I am indebted.  I intend to send off for new PCBs tomorrow evening and any comments in the meantime are greatly appreciated!  NOTE: This post was revised on 24 Jan 2019 to update the schematic and PCB screenshots per upgrades and comments from Shabaz.

 

Summary of Changes

  • Added biasing for VREF of the instrument op amp which improves reading of resistances around 1 milliohm
  • Added ability to add capacitance and / or diodes in front of instrument op amp
  • Moved trim pots to trim gain of operational amplifier - current sources are not trimmed
  • Modified arrangement of range switch
  • Changed PCB footprint to fit enclosure used by Shabaz
  • Added through hole 5V alternate input
  • Relocated on / off switch
  • Numerous other small improvements

 

Development is a bit behind as I have been struggling to remove the one known bug - intermittent instability when measuring resistances below 20 milliohms.  I have been making modifications to the Version 1 PCB with flying leads to a breadboard.  This seems to introduce unwanted capacitance and perhaps other problems.  To address this and allow quick changing of components I have determined that I can bend the pins on duPont female sockets and solder them to an 0805 footprint.  Then insert passives as desired.  The black 2 pin socket is a bit hard to see but the concept is demonstrated in the mockup using the Version 1 PCB below.

image

 

The new schematic and PCBs are shown below.

 

Schematic

The original schematic posted here was in error and has been replaced with the corrected version.

image

PCB

The original PCB screenshots posted here were replaced with a version that include an upgraded layout based on comments posted by Shabaz below.

image

image

image

 

As always, comments and suggestions are greatly appreciated!

 

Related Links

Building Frank's Milliohm Meter

Testing Current Sources for a Kelvin (4-Wire) Milliohm Meter

More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

Even More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

Working Prototype of a Kelvin (4-Wire) Milliohm Meter

PCB for a Kelvin (4-Wire) Milliohm Meter

  • Sign in to reply
  • shabaz
    shabaz over 7 years ago in reply to fmilburn

    Hi Frank,

     

    Oh, no problem, I didn't realise it was submitted. These suggestions were minor anyway! The current layout looks great already.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    I already submitted :-(   If you find anything major I will make a run at OshPark. Othrwise I will start a new improvements log and make these changes so they are ready for the next PCB.  I think the next PCB will need to be a bit larger to incorporate upgrades anyway.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to fmilburn

    Hi Frank,

     

    Good idea to remove the old screenshots, to keep clutter down! It's great that you managed to incorporate the changes yet keep it looking tidy.

    I'll go through it today, but I only had these few comments meanwhile.

    1. Very minor, the JP1 jumper is labelled CAL on the PCB, but no current adjust can be done to calibrate since there are no current-trimmers any more, so maybe it can be renamed to (say) Test (and could be completely removed in a Rev 3).

    2. For the comparator, the bypass caps can be closer, something like this:

    image

    3. (Super minor): Maybe label the trimmers HI/LO or something, to indicate which trimmer corresponds to the high range, and which to the low range. Similarly maybe the DPDT switch positions could be labelled, although maybe that's not possible due to space.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago

    I made the order this evening since Chinese New Year is approaching and I wanted to get the boards fabricated and shipped before things shut down.  Changes were minimal compared to what is shown above with no changes to the schematic.  The layout was tidied up a bit and the mask clearance modified so that hopefully there will be solder mask in between the smaller SMD parts which has been a problem in the past from the Chinese board house.  HASL lead free was used instead of ENIG to save a little money.  Should get the ten boards in 2 to 3 weeks.

     

    Hopefully we can hunt down that pesky intermittent instability with the new pads on this board.  If not, it should be useable but it is sometimes necessary to reclip the probes with resistances below 20 milliohms.

     

    The board was revised up to Version 1.3 instead of 2.0 since it has no new active components over the original prototype or Version 1.0.  A major upgrade to Version 2.0 would include auto-ranging and possibly a microcontroller with SCPI.  This started out as a very modest project using an op amp on a bread board to control current and has morphed into this.  Fun!  I have learned a lot.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to shabaz

    Hi shabaz

     

    The correct schematic has now been posted in the original post.  The differences in the old one are the error you pointed out plus the voltage divider biasing VREF also is the negative output to the panel meter.

     

    To keep the clutter down I also removed the old PCB screen shots and posted the revised version in the original post which includes your layout around the instrument op amp.  Bad form I know to erase evidence of my errors :-).  I did not place components quite as tight as you did in your layout but generally followed it. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>