Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Low Battery Warning Indicator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 22 Sep 2020 3:10 AM Date Created
  • Views 41926 views
  • Likes 18 likes
  • Comments 17 comments
  • low voltage
  • tl431
  • low voltage alert
  • battery warning
Related
Recommended

Low Battery Warning Indicator

shabaz
shabaz
22 Sep 2020

Introduction

I like building battery-powered circuits, but always in the back of my mind is the thought that I really ought to provide a ‘low-battery’ indication! Since it isn’t usually a core feature of the project, it often gets forgotten. This ultra-short blog post describes my attempt at a generic low-battery indicator that could (hopefully) be reused for many projects.

 

What does it do?

This circuit alerts the user when the battery needs changing or charging. I have chosen the simplest way of determining that the battery capacity is low, and that’s using the battery terminal voltage.

 

A couple of circuits are described here. One of them lights up a warning LED whenever the voltage drops below a certain value. The other circuit can be used to replace the typical power-on LED. The behavior, in that case, is to use the LED as a normal power-on indicator, but begin to flash when the battery voltage is low. In other words, the LED should permanently light up when the circuit is powered on and the battery is good. When the battery is bad, the LED should flash.

 

The design here avoids using a microcontroller, but if a microcontroller exists in the project then using that could be the most economical and effective way, especially if a comparator or other analog input peripheral is built-in to the microcontroller chip. The circuits in this blog post are more useful for a purely analog design, especially low-noise projects.

 

Basic Circuit

There are many ways to implement a low-battery indicator circuit. This circuit is very low-cost, it uses the TL431 integrated circuit, which costs as little as $0.10 in quantities of a few hundred. The TL431 is a component with dozens of example use-cases, it's extremely versatile, and comes in more than half a dozen different packages, from through-hole varieties to surface-mount SOT-23.

image

The programmed voltage is achieved using the potential divider circuit created by R1 and R2. The entire circuit is fairly accurate while still being low-cost, based on the premise that modern resistors are low-cost and accurate too, and that combined with the TL431 internal reference voltage (2.5V) should work for providing a low voltage indicator that is ‘good enough’.

 

The formula for calculating the resistor value is:

image

where Vref is 2.5V and Vcutoff is the desired threshold voltage for the alert indication. There is an Excel file attached to this blog post below, which can be used to quickly calculate the right resistance values.

 

Flashing LED Circuit

The circuit here keeps the low-cost theme going, by using a jellybean op-amp to implement a flashing LED.

image

 

Reading from right-to-left, op-amp U2B is unused (you could use a single op-amp chip if desired, but the LM2904 dual op-amp is cheap!). Next, op-amp U2B implements an oscillator circuit and the LED blinking rate can be varied by adjusting C2 or R7. The values in the diagram will implement a slow 1 Hz blink rate.

 

The circuit on the left is identical to the earlier simpler circuit, except that a PNP transistor is used to gate the oscillator. When the voltage is higher than the programmed threshold, transistor Q1 conducts and the oscillator does not run and the LED stays lit. When the voltage is lower than the threshold, the capacitor C2 can charge/discharge and the LED will blink. I like this circuit because it saves having to drill two holes for a power-on LED and a low-battery LED!

 

Circuit Adjustments

The circuit can function from 3V up to 26V or even higher (depending on the chosen op-amp). Here’s the detail on the adjustments that should be done to suit any particular needs.

 

Firstly, size the LED resistor (R5 or R8, depending on if you're using the simple or the flashing LED circuit) appropriately. The value in the diagram (1k) will probably work across the entire 3-26V range, but the LED may be extremely brightly lit at very high voltages, and dimly lit at very low voltages. 1k ohm is a good starting point. High-efficiency red LEDs are a good choice too.

 

Next, change the value of resistor R1, to suit the desired low-voltage indication threshold, using the formula mentioned earlier. There is a downloadable Excel file attached to this blog post, to make the calculation easier.

 

To change the blink rate, R7 can be modified. A lower value will result in a faster blink rate. A smaller capacitance value for C2 will also result in a faster blink rate.

 

Summary

These were a fairly trivial couple of circuits, but it solves what is perhaps a common problem, and it will hopefully enable battery-powered projects to be a bit more complete!

Attachments:
low-volt-tl431-calculator.xlsxlow-volt-tl431-calculator.xlsx
  • Sign in to reply
  • BigG
    BigG over 5 years ago

    Hi Shabaz

     

    Your blog looks very interesting.

     

    I'm looking to create a wearable device with something like an ARM Cortex M0 device, which is powered directly with a 3V coin cell battery (CR2032). One feature I want to add is low battery voltage indication.

     

    So, I was wondering if this circuit is suitable for such a design. For example, is the quiescent current of this circuit suitable and what about the current when the LED is actually on or flashing due to low voltage (surely it will drain battery even faster etc.)

     

    Also what alternatives or tweaks are there (I know there is the standard voltage divider option using 100k resistors etc. to keep quiescent current low as possible and ensure ADC sample speed decent).

     

    For example I came across this document using a CMOS comparator - but then thought that this is probably only valid if using an LDO.

    https://www.maximintegrated.com/en/design/technical-documents/app-notes/1/1872.html

     

    Any insight / pearls of wisdom greatly appreciated. Want to keep it simple as possible with minimal MCU processing.

     

    Thanks

     

    Colin

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago

    Very nice circuit.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to genebren

    Hi Gene,

     

    Thanks! I forget to use it often too, but it's a really convenient part when I remember about it!

    This was a ultra-low-cost charger (5mA so not particularly fast, but that was ok for the use-case) with the TLV431 for a NiMH batteryNiMH battery, that's a nice IC too, identical to the TL431 except the TLV431 has a 1.24V reference (it's often a bit more expensive than TL431).

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 6 years ago

    Very cool designs!  I have used the TL431 as a reference, but never as a control element.  This was a great opportunity to learn something new and refresh my existing transistor and op-amp knowledge.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago

    It's too easy to just use a microcontroller these days. It's nice to see a well designed circuit using analog electronics.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>