Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Making Fancy Cables Part 2: Soft Headphone and Composite Cables
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 8 Dec 2018 6:56 AM Date Created
  • Views 3264 views
  • Likes 8 likes
  • Comments 4 comments
  • composite_cable
  • fancy_cables
  • braid
  • headphone_cable
Related
Recommended

Making Fancy Cables Part 2: Soft Headphone and Composite Cables

shabaz
shabaz
8 Dec 2018

Part 1, Making Fancy Cables: Network Cables!  examined how coloured and patterned nylon braids could be used for cable assembles: ) Those cables are intended for demos/presentations and so on.

Nylon braid is very easy to use because it can expand a lot, and is slippery against the wire so it slides on well too. However, although it looks visually nice, it is not soft. For home use, maybe a softer braiding is preferred.

 

For a long time I have wondered how to create composite cables without using metal or nylon braid. Composite cables are those where there could be a mix of different conductors for different signals. A good example is an audio and video (A/V) cable. It can contain wires for the left and right channels, but also some coax for the video signal. A/V cables are not used much nowadays, but sometimes I do want to transport low-power DC alongside a coax cable. There are not many off-the-shelf composite cables that contain all that. Another example was a handheld pick-and-place project discussion while back, where it was desired to have a air (pneumatic) tube, but also a couple of electric wires for illumination, all in a single cord.

 

I explored what cotton braid was available intended for such purposes, and came to the conclusion that it was really hard to find!

In the end it was noticed that some cotton rope is actually made of two or more concentric braids : ) Problem solved!

image

 

The procedure is really easy, just tug on the inner braid layer to pull out an inch of it (the photo shows below the cable a fragment of blue rope with the inner braid partially pulled out), and use sticky tape to attach it to the bundle of wires you wish to use. Then at the other end of the cotton rope, tug on the inner braid layer as well, and keep pushing the outer braid down until it starts covering the wires, and keep going.

 

It is really easy, except that cotton braid cannot be easily expanded, so it only works for a limited thickness of wires. If the wires are thicker, then the cotton braid won’t expand over it.

The diameter of braid that I used was impossible to fit over a cat-5 network cable for instance. But, there was no problem fitting it over RG316 coax (3mm diameter) plus a couple of 10/0.1 wires for power, as shown in the photos. I think it would also work really well for headphone wires, since it is soft.

Here’s a zoomed-in photo:

image

 

The cotton braid does look a bit faded, it is not as neat-looking as nylon braid. However, maybe there are sources for obtaining better braid. I'm still searching.

If the ends of the cotton braid need terminating properly, then adhesive-lined heatshrink sleeving can be used. It is great for finishing off connectors especially where there is no existing strain-relief.

Something like the 4:1 shrink ratio sleeving such as TE ATUMTE ATUM is useful, because it can fit around the housing of the connector, but also shrink down to the cable diameter, and glue itself around the cotton braid so it doesn't fray. Another (easier) method to terminate the braid could be to get some typical household glue (e.g. UHU impact adhesive) and let some soak in to the end where it will pass inside the connector shell. The glue should keep the cotton together, and attached to the inner cables.

 

Thanks for reading!

  • Sign in to reply
Parents
  • three-phase
    three-phase over 7 years ago

    Bespoke made multicore cables can be very handy for some projects. Have you thought about using silicone tubing as an alternative to the cotton braid?

     

    I imagine it won't expand, so will have to be sized accordingly, but the right stiff should be soft and flexible.

     

    A quick scan of eBay shows a couple of offerings;

     

    Silicone tubing

     

    Rubber tubing

     

    Plenty more out there though of differing sizes of diameter and wall thickness.

     

    Kind regards

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to three-phase

    Hi Donald,

     

    I had not thought of that, but it's an excellent idea : ) Since it's translucent, you could even run electro-luminescent wire down it. I'm sure the in-car entertainment enthusiasts would pay for illuminated interconnects : )

    I made use of the cotton rope today incidentally. I had some Hirschmann banana-to-jumper cables that are always getting tangled, and will break someday. So I used the cotton, to keep them super-soft and flexible, and they feel really useful now! I think this should be a product : )

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago in reply to shabaz

    Nice, that heat shrink has sealed up well around both the braid and the cables cores, real neat professional finish. Would also be interesting to see what Y- or T- shaped heat shrink would be available to pull out cores at different points along the braid.

     

    Kind regards.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 7 years ago in reply to shabaz

    Nice, that heat shrink has sealed up well around both the braid and the cables cores, real neat professional finish. Would also be interesting to see what Y- or T- shaped heat shrink would be available to pull out cores at different points along the braid.

     

    Kind regards.