Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog ODROID-GO Handheld Gaming Kit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 27 Jun 2018 8:52 PM Date Created
  • Views 6304 views
  • Likes 12 likes
  • Comments 29 comments
  • educational
  • retro gaming
  • odroid
  • gaming
  • educational kit
  • retro gaming console
  • odroid-go
Related
Recommended

ODROID-GO Handheld Gaming Kit

shabaz
shabaz
27 Jun 2018

Introduction

Thanks to Problemchild he advised me about a simple gaming kit called ODROID-GO, and it was fairly low cost (£38 including delivery to the UK) for such a device, so I was tempted to purchase it. (Note: that there will be duty of approx. £7 to pay, plus £12 handling charge by FedEx, so that makes it less attractive : (

 

The ODROID-GO is a very compact (approx 120x75x13mm) device that internally features an ESP32 (ESP32 PDF datasheet) based module (this contains a microcontroller and 2.4GHz WLAN and Bluetooth Classic and Bluetooth LE capabilities), and rechargeable battery built-in too. There is also a microSD socket and what is especially awesome is a 0.1 inch SIL header socket at the top end of the case, for custom hardware expansion : )

 

image

(image source: ODROID website)

 

It comes with a microUSB cable for charging and USB UART for connecting into the ESP32 module. All that is additionally required is a microSD card, and a small Philips screwdriver to assemble it!

The device comes from ODROID, who manufacture some really nice single board computers and accessories.

 

It arrived today, and although I'd initially thought it was a kit to be soldered, it actually is pre-soldered. I think a child could easily assemble it with just a little supervision. It looks really great, and I'm tempted to purchase another, so both my nephews can have one.

 

This short blog post is a quick introduction to the ODROID-GO, I have not explored it much yet.

 

What's in the Box

This is everything you get in the box (the micro USB cable is also supplied but not shown in the photo):

image

 

What Can it be Used For?

The project is open source, and there is an ODROID-GO github repository with the schematic and source code.

However no programming knowledge is needed to use it just for gaming. For gaming some files are downloadable from the ODROID website that need to be transferred to a microSD card, along with games ROMs. It can play ROMs for various historical consoles like Nintendo GameBoy, and Sega GameGear and so on. I've not explored (nor assembled!) it yet. ODROID-GO assembly steps are online.

 

More interestingly, since it is open source, the possibility exists to create your own games or applications, and connect your own hardware. The expansion port appears to have SPI and a few general purpose input/output connections and 3.3V available. Perhaps it could become a debug tool : )

 

Some More Pics..

The enclosure looks to be of reasonable quality, injection-moulded, perhaps 1mm thick. It could crack perhaps if mishandled; it looks like the same plastic that CD case covers were made of. It is custom-designed and has the ODROID legend on the front. The lower half of the shell has a slot for inserting the microSD card, but I didn't like that such a delicate card is exposed. It would have been better to have a plastic cover for it. Other than that, I didn't have any complaints, but I still need to assemble it to explore further. There are four black rubber buttons (the enclosure has them labelled as Menu, Volume, Select and Start), and also a directional pad and a couple of buttons labelled A and B, suitable for games. There is a slide switch on the right of the ODROID-GO, for power on/off. The hard LCD cover is adhesive, so once the LCD is fitted, it may be awkward to remove. Anyway, the LCD it is unlikely to go faulty. The PCB can still be removed by disconnecting the LCD.

image

The pre-assembled circuit board looks nicely made, it is a 1.6mm fiberglass board so it is fairly rugged.

image

 

Everything looks easy to maintain and debug, there are lots of test points on the circuit board. The holes where the screws should go are marked; three screws secure the PCB to the inside of the front shell of the enclosure, and then six screws will secure the rear half of the enclosure.

image

 

That's it for this short blog post. To be continued..

  • Sign in to reply
Parents
  • Problemchild
    Problemchild over 8 years ago

    O dear Shabaz you made it sound so attractive I bought one as well. Also got another XU4 so I can make a mobile with my Lime /Lime Mini SDR!!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to Problemchild

    FedEx today sent me a demand for £19: ( I'd thought it was below the limit for duty, but I'd mistaken it with the limit for gifts.

    For non-gifts, the limit is £15.

    So basically there is an additional cost of £7 plus £12 handling charge by FedEx, total £19 : (

    Still, if you've got other gear like the XU4 at the same time, then that £12 handling charge is absorbed a bit better.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to shabaz

    there is an additional cost of £7 plus £12 handling charge by FedEx, total £19 : (

    I also dislike the freight company that has already been paid to deliver an item, adding a handling charge to collect a fee.

     

    Here in NZ we have the NZ Customs adding a large amount when they want to collect Tax (usually GST) and the freight company then gets in on the act with various other charges.

     

     

    Apparently the NZ Government is pushing legislation that means the overseas companies need to collect the GST.

    Unsurprisingly many have decided to refuse to take orders ...

     

    Amazon has done one better, and redirects Australian customers to the Australian site, which often doesn't have the item, and the price is far more than the conversion plus tax.

     

    Both governments would have been better getting Paypal, or the Credut card companies to do their collecting at purchase time.

    The transaction from the vendor could have an extra field to show it was not a transaction, and therefore the GST is not applicable.

     

     

    Odroid have a list of distributors

    https://www.hardkernel.com/main/distributor.php .

     

     

    This american site has listed them in their products

    https://ameridroid.com/products?keywords=go

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 8 years ago in reply to mcb1

    yeah we complain here about taxes but when you get redirected to a local site which charges more because they have to make a proffit and also put up with the pedantic nature of importing in certain countries then we are in fact quite lucky here. Most EBAY items arent stoped unlike say Germany where that as now become a "thing" apparently and similar suff else where. It's just anoying to order a single small item only to find all  the greedy little noses getting in the trough and costing you more than the device. That said we are ordering from Korea here and getting delivery inside 4-7 days ...Isnt the world fantastic!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to Problemchild

    I was thinking about the £500,000+ Vega+ portable console Indiegogo campaign today.. the console that couldn't be achieved in two years, yet Clive Sinclair managed just fine creating the original all those years ago.

     

    ODROID-GO to some extent could replace that! Just needs someone to port it across. And for more performance there is always the Pi and compact LCDs and RetroPie.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago in reply to Problemchild

    I was thinking about the £500,000+ Vega+ portable console Indiegogo campaign today.. the console that couldn't be achieved in two years, yet Clive Sinclair managed just fine creating the original all those years ago.

     

    ODROID-GO to some extent could replace that! Just needs someone to port it across. And for more performance there is always the Pi and compact LCDs and RetroPie.