Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Vintage Curvy PCB Traces with KiCad 7
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 3 Jul 2023 11:43 PM Date Created
  • Views 10140 views
  • Likes 10 likes
  • Comments 32 comments
  • kicad 7
  • kicad 6
  • kicad
Related
Recommended

Vintage Curvy PCB Traces with KiCad 7

shabaz
shabaz
3 Jul 2023
Vintage Curvy PCB Traces with KiCad 7

Table of Contents

  • Introduction
  • What’s Required?
  • Running the Plugin
  • Fixing Issues
  • Summary

Introduction

Old-school printed circuit boards (PCBs) often had wavy copper traces! They were done manually by rolling out UV-light-blocking crepe sticky-backed tape onto clear film.

image

The photo above shows a layout I did as a teenager (I wasn't very good at it). It's for a lighting control unit.

I have meant to experiment with a particular rounded-track feature for KiCad 7 for ages. It ought to produce a reasonable likeness to those old vintage circuit boards! I gave it a shot today. It can transform machine-generated PCB tracks to look more like hand-taped PCB layouts.

What’s Required?

The only prerequisite is to complete your board design (you can still edit it later) and install a special plugin. To install the plugin, on the KiCad startup screen, click on the icon for the Plugin and Content Manager:

image

Search for the Round Tracks plugin, click on it, and install it:

image


Now open up the PCB Editor for the project you’re working on. In my case, it was an amplifier board:

image

As you can see in the screenshot above, the board is already routed, but using sharp corners on the PCB tracks everywhere.

Running the Plugin

In the PCB Editor, click Tools->External Plugins->Round Tracks. A small settings window will appear. The screenshot below shows what settings I used; there’s not a lot there to configure!

image

Click on Run, and it shouldn’t take too long to execute:

image

Click on OK, and then the new board layout will appear!

Fixing Issues

When you run the Design Rule Check (DRC), some new errors may be revealed. For instance, I had four errors with this board. The first one is highlighted here:

image

This was easy to fix by closing the newly generated board and editing the original board layout:

image

The plugin was re-run, and as seen in the screenshot below, the problem was sorted!

image

All four errors were similar and fixed using the same method.

image


Generally, I think it did a fantastic job, although a few cosmetic artifacts could be tweaked. For instance, a kind of delta shape is visible at the top-right in the screenshot above that could be cleaned up simply by deleting any redundant traces in the generated output.

The new PCB layout will be in a file with a new name (with a -rounded suffix) if the Create a new file option was checked in earlier settings.

Here’s the final error-free result, with most of the redundant traces removed:

image

I think it's not bad, although to keep it 1970s style, it shouldn't have copper fill (or at least, not so tidy copper fill) around the traces!


Summary

Curved vintage-style PCB traces is quite a niche thing to want to do, but it could be interesting, especially for restoring or recreating old electronic products or perhaps retrofitting new functions or interfaces. With KiCad, it was straightforward to do, using a Round Tracks plugin and executing it against a normally-completed PCB design.

The plugin generated a new PCB file, so it is possible to edit the original PCB layout and re-run the plugin as desired, to improve it and resolve any clearance issues caused by rounding tracks too close to other PCB elements.

With KiCad 7, some extra things could be done to improve the look further. For instance, the silkscreen font can be changed to any arbitrary old font (although silkscreen was less common on early boards).

Thanks for reading!

  • Sign in to reply
  • shabaz
    shabaz over 2 years ago in reply to shabaz

    Early 2011 was the final time Germanium diodes were in stock at Farnell, they cost £1.11 each:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to jc2048

    Hi Jon,

    This is extremely useful! I'd had a hunch that germanium diodes would conduct sooner, but hadn't tried it. I'm down to just three Ge diodes in the junk parts box, they are OA47, bought when Farnell was down to single-digits stock of them : (

    image

    I'm going to save them for a crystal radio one day. I tried with a Schottky diode, but failed, and suspect it was partially because of that.

    Your work encouraged me to measure the OA47 just now. This is the result I'm seeing (I only measured one of them, so I don't know about variability).

    image

    In the reverse direction, I see 2uA leakage at -200mV, and 3uA leakage at -1.5V. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 2 years ago in reply to shabaz

    image

    Here's a direct comparison. It does look like the Ge diode starts earlier than the Schottky. But the curves cross at 2mA/0.3V, so it doesn't maintain the advantage at higher currents.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to jc2048

    I love the clean traces from the ADALM1000. It's great as a curve tracer. It is interesting comparing the chart to the one with the Schottky diode from your ADALM100 bloig post:

    image

    I think the Germanium diode started conducting just a little earlier than the Schottky diode, since the trace looks a fraction higher at 0.2V!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 2 years ago in reply to Jan Cumps

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>