Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum ARMP Archaeology Resistivity Meter Project - base data
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 3 answers
  • Subscribers 327 subscribers
  • Views 2265 views
  • Users 0 members are here
  • armp
Related

ARMP Archaeology Resistivity Meter Project - base data

davemartin
davemartin over 6 years ago

Re the Archaeology Resistivity Meter Project (armp ), and further to the discussions on the injection aspect, and the linearity (or otherwise) of the ‘device under test’, I’ve run some tests. Main plots are included in-line below; fuller set available if needed. This first note is already rather long, so the next section with control plots and alternative stimuli etc. will follow in part 2.

 

ARMP – field plots, part 1


Purpose

Share data on characteristics of a typical archaeological earth resistance measurement path to assist with design of the Archaeological Resistance Meter Project (ARMP).


Test setup / conditions

Injection:  +/5v from Wavetek 275; into HP 6826A bipolar amplifier (max +/- 50v, with constant-voltage and constant-current mode); injected current monitored via 100R 0.1% in series with amplifier output. Stimulation principally 137Hz square wave, plus selected other waveforms.

Monitoring:  Fluke PM3394A (4 ch), waveforms captured single-sweep to capture peaks and also using in-scope averaging (32 sweeps) to give crude filtering.

Soil Probes:   fixed (P1C1) and mobile (P2C2) probes, P1-C1 and P2-C2 0.5m separation, P1C1 and P2C2 up to 50m apart, leads (unscreened) in ‘twin-probe’ configuration as typically used in archaeological resistivity survey.

Target:  marked 50m length of favourable but mixed ground (note a, b).

 

At each station along the test traverse, inject test 137Hz square-wave at 10 mA (note c), record injection waveforms C1C2 (voltage V1 and current I) and potential P1P2 (voltage V2). Main results in table 1.1 below.

Also - described in part 2 - record control plots (dummy load) and at selected stations P1P2 potential V2 with no injection to capture background electrical noise with, and without, 50Hz main electricity on in nearby property. At selected stations, in addition to 137Hz, also record with 32Hz and 80Hz square-wave stimulus, and with other non-square-wave stimuli (sine wave, triangle/sawtooth, trapezoid). Analysis of various stimuli to follow further in part 3.

 

Results

Injection

At intervals along the 50m traverse, the injection voltage (V1) necessary to inject the target current (I) was captured, below is a plot of V1 against distance (X) for each target current. Target I was nominal 10 mA, which required V1 in range +/- 30 to 45v; note that at 30 metre point where the test traverse encounters more stony terrain, the test struggled to inject more than 5 mA at +/- 55v.

 

image

Fig 1.1 – Absolute injected current (I) and necessary voltage (V1) vs distance (X) along test traverse

 

The injection waveform was also captured (V1 and I vs time T), below (figs 1.2, 1.3) are typical plots for target 10 mA at 15 metres. Injection waveform plots for each station, and reference plots, are available (note d)


image

Fig 1.2 – Injected current (I) and necessary voltage (V1) waveform at X=15m – single sweep

 

image

Fig 1.3 – Injected current (I) and necessary voltage (V1) waveform at X=15m – averaged in-scope

 

The upper (green) trace in figs 1.2 & 1.3 is the injection voltage V1. The lower (purple) trace is the current injected I. In this example (at X = 15m), V1 is +/- 35.1v and I is +/- 9.5 mA (measured as +/- 0.95v across 100R).

 

P1P2 voltage

The differential voltage V2 between  P1P2 was also recorded (no differential probe to hand so acquired by using one scope channel for P1 and one for P2, and subtracting ch2 from ch1). Figure1.6 below shows differential V2 at each station along the traverse, along with the injection parameters.

 

image

Fig 1.4 – Absolute injected current (I) and voltage (V1), and differential P1P2 (V2)
vs distance (X) along test traverse

 

 


Fig 1.5 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=15m – single sweep
Upper (green) trace is the injection voltage V1; central (purple) trace is the current injected I;
lower (blue) trace is  differential P1P2 (V2)

imageimage

Fig 1.6 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=15m – averaged in-scope


The effects of the injection waveform will discussed more in part 2.

 

Resistance

At each test station, waveform was captured with potential P1P2 (V2) and injected current C1C2 (I) against time, and resultant apparent resistance (R2) derived. Sample below at 15m station.

 

image

Fig 1.7 – Injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=15m

 

Values for R2 at each test station against distance X are:


Fig 1.8 – Soil resistance R2 (V2/I) vs distance (X) along test traverse
image

 

And, just for reference, the same plot but including with values for R1, the resistance encountered by the injection circuit, which shows the effect of contact resistance:

image

Fig 1.9 – Soil resistance R2 (V2/I) and injection resistance R1 (V1/I) vs distance (X) along test traverse

 

Key data


Table 1.1 – Key measurements obtained with 137Hz square-wave excitation
V1/I/R1 injection C1C2; V2/R2 soil sample based on P1P2 potential and injected I
image
P1C1 static at 0 metres; P2C2 moved to each station in turn
(voltages and current are +/- value shown)

 

Comments

  1. The ‘inrush’ when injection is applied can be seen in the injection (V1, I) vs time plots (figs 1.2, 1.3), the differential potential plots (figs 1.,5, 1.6) and the derived resistance plot (fig 1.7).
  2. Even in relatively conductive soil conditions, when a small stony patch was encountered, +/- 50v injection was unable to inject 10 mA (fig 1.1, note e)
  3. Spikes or ringing in V2 (P1P2) occur at the leading edge of each reversal, significantly in excess of the proportions exhibited by the injection waveform (see part 2).

 

Notes

(a)    Test location – 50m traverse, no edge effects, damp soil. Slight 50 Hz mains, plus electric fencing energiser effect, plus other stray / telluric current; background noise plots taken P1P2 at selected locations with no injection with, and without, mains on in nearby property (see part 2).

(b)   Earth path distance - in the main ARMP use case (twin-probe grid-survey) with 0.5m probe separation and 20x10m grids, the shortest earth path P1C1 – P2C2 would be 15m and the max usually 50m; but in use case 2 (Wenner x, Schlumberger etc.) and use case 3 (profiling) the P1C1 – P2C2 distance can be down to a metre or less, so results captured from 1 to 50 metres. Stations at 1, 2, 3, 4, 5, 7, 10, 15, 20, 25, 30, 35, 40, 45, 50m.

(c)    ‘Constant’ current – the HP 6826A amplifier, when in constant current mode, was not able to hold constant-current at single-figure mA. Therefore, to constrain the variables, the amplifier was operated in constant-voltage mode with the current manually adjusted to average the target current for each test location; so at each location the current was a nominal metered 10 mA, but, as can be seen from the plots, there was variation during the duration of each pulse due to the ‘inrush’ and polarisation; the derived resistance plots take account of this by using the measured rather than target current. At the 30m point, the ground was stony and the test struggled to inject more than 5 mA at +/- 55v.

(d)   Injection performance – plots in part 2 include a control for each excitation using a fixed 4k7 resistor rather than the earth, to show amplifier performance, and effect of any mains ripple etc.

(e)   Voltage limit – when the HP 6826A maxed-out at +/- 55v when trying to inject 10 mA at 30 metre location (shallow stony patch), a one-off trial attempt was made to continue using another higher-voltage constant-current source (Glassman LP100-12 constant-voltage and constant-current power supply) with external output reversal. 10 mA was eventually injected, but it took +/- 97v. The Glassman power supply (not an amplifier) takes up to 3-4 ms to stabilise after a load removal, so the reversal rate had to be slowed down (32 Hz was used).

 

 

Continued in part 2

DM 21 Aug 2020

Attachments:
imageARMP plots 1 v07.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • davemartin
    davemartin over 6 years ago in reply to davemartin +2 suggested
    ARMP – field plots, part 3 Basic injection voltage ( V1 ) and current ( I ) between C1C2 and resultant differential voltage ( V2 ) between P1P2 were covered in part 1, all using standard archaeological…
  • michaelkellett
    michaelkellett over 6 years ago in reply to davemartin +2 suggested
    Nice to see some more data, I'll be interested to see your final part. It would be nice if you were to include some results with more significant noise in the measured voltage. In your previous post there…
  • davemartin
    davemartin over 6 years ago +1 suggested
    ARMP – field plots, part 2 Basic injection voltage ( V1 ) and current ( I ) between C1C2 and resultant differential voltage ( V2 ) between P1P2 were covered in part 1, all using standard archaeological…
Parents
  • davemartin
    0 davemartin over 6 years ago

    ARMP – field plots, part 2

     

    Basic injection voltage (V1) and current (I) between C1C2 and resultant differential voltage (V2) between P1P2 were covered in part 1, all using standard archaeological geophysics preferred 137Hz square-wave excitation.

     

    Part 2 continues the test results, using exactly the same setup in part 1, and covers control (test load, background measurements), and detected signal range using square-wave excitation. Part 3 will then start to look at various stimuli – varying the square wave frequency, and then using alternative waveforms.

     

    Control

     

    For reference, the test signal generation/injection chain was operated on the bench to check the injection performance.

     

    Waveforms were recorded directly from the Wavetek 275 arbitrary signal generator, and the outputs of the HP 6826A bipolar amplifier - both open-circuit and into a purely-resistive (at these frequencies) 4k7 dummy load (note a). The effect of the survey leads used to connect to the probes was also checked.

     

    image

    Fig 2.1 – Sample injection performance into dummy load with 137Hz square wave excitation
    V1(upper/green), I (lower/purple) – averaged in scope


    Waveforms were recorded as above, but don’t merit inclusion here other than the example above, as they all show the chosen waveforms being reproduced faithfully and no discernible ringing or overshoot effects, whether into the dummy load or with the C1C2 injection path open-circuit.

     

    As well as connecting the dummy load directly to the injection amplifier, the load was connected via various sets of survey leads to check they didn’t introduce any problems. The survey leads used for these tests were a set of existing survey leads, as used for most twin-probe archaeological resistivity work (flexible unscreened twin-core mains cable as used for, say, an electric lawnmower or hedge-trimmer), and (ii) a lead made from Belden 8760.

     

    Analysis of these leads using a Peak Electronics ‘Atlas LCR-40LCR-40’ passive component analyser showed that for 50m lengths of lead, the normal survey lead had resistance 3 ohms and an inductance per core of app 40 μH, and inter-core capacitance app 10nF; the Belden had resistance app 2 ohms and inductance per core of app 15 μH, and inter-core capacitance app 6nF.

     

    No artefacts could be discerned as a result of introducing the survey leads twixt injection amplifier and dummy load when all was connected as it would be in a survey. The only artefact noticed was if the probes C1 and C2 completed an injection path, and hence injection current was passing in the survey lead into the load, but one of P1 or P2 was not in the ground (or making contact) then a small coupled edge was spotted on the P circuit – but that was only if the far end of the P lead was left floating.

     

    External interference

     

    These tests were almost all acquired using a Wavetek signal generator, HP amplifier, and Fluke 4-channel DSO; all these bench instruments used for these outdoor tests were powered from a small 240v inverter, which was a potential noise source – either radiated or conducted. The main noise from the inverter, which was present throughout all the tests in both part 1 and here in part 2 and 3, was of the order of tens of millivolts at several kHz.

     

    It was known that this might cause a problem, as might 50Hz mains in a nearby building, and a mains-powered electric fencing energiser, so the immediately following background noise plots were acquired with a battery-powered rig (two-channel PictoTech 3205 and laptop) as control, the two sensing soil probes P1 and P2 (at their max 50m separation at either end of the test traverse) were connected to ch1 and ch2 of the PicoScope.

     

    In all except the immediately following control plots (figs 2.2 and 2.3) the 50Hz mains supply in the nearby property (whose earthing / ground return point for the mains supply was some 25m from the test traverse at the closest point) was isolated, but was switched on just for these interference-measurement tests. Similarly, the electric fencing energiser for the nearby farm was also powered-off, except during these interference-measurement sweeps. The grounding-point for the electric fencing energiser return was approximately 50m from the P1 location and 95m from P2. The background sweeps (figs 2.2 and 2.3) were chosen to include a capture when an electric fence energiser pulsed.

     

     

    image

    Fig 2.2 – Typical single-ended background P1 and P2 waveforms at X=50m – single sweep – with NO injection
    and nearby 50Hz electricity supply ON, and electric fence energiser ground pulse, and inverter noise

    The individual waveforms for P1 and P2 so closely track each other on this plot as to be indistinguishable except for when the electric fence energiser pulsed.

     

    Differential measurement on a scale which can show the electric fence pulse:

    image

    Fig 2.3 – Typical background differential P1P2 (V2) waveform at X=50m – single sweep – with NO injection
    and nearby 50Hz electricity supply ON, and electric fence energiser ground pulse, and inverter noise

     

    The mains supply nearby was then isolated, and the electric fencing energiser powered-off again, before continuing with the tests below. (There was still some small 50Hz noise though, even with the inverter switched off.)

     

    image

    Fig 2.4 – Typical background differential P1P2 (V2) waveform at X=50m – single sweep – with NO injection
    and nearby 50Hz electricity supply OFF, and inverter noise

     

     

    It should be noted that the effect of the stray/return mains current can cause significant asymmetry in the injection:

    image

    Fig 2.5 – Circa 5mA injection in presence of nearby 50Hz electricity supply,
    as measured across 100R in series with C1 injection lead

     

    But if the resistance calculations are based on instantaneously measured injection current I then reasonable resistance results can still be achieved by suitable windowing (see part 3).

     

     

    Signal Range

     

    With standard square-wave excitation, spikes and ringing in the V2 (P1P2) signal can occur at pulse reversal time, significantly in excess of the proportions exhibited by the injection waveform (V1, I). The V2 peaks can be up to an order of magnitude in excess of signal.

     

    For example at X=15m, in ‘good’ ground, even though the total range between stable +ve and stable –ve on P1P2 was only 9.0v; the range between peak +ve and peak –ve was 32.4v

     

    image

    Fig 2.6 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=15m – single sweep
    Note V2 peaks at reversal

     

     

    At X=30m, when only just over 5mA could be injected (by V1 = +/-60v) on a small stony patch, even though the total V2 range between stable +ve and stable –ve was only 0.7v the range between peak +ve and peak –ve was 60.2v :

    image

    Fig 2.7 – Injected current (I) and differential P1P2 (V2) waveform at X=30m (stony ground) – single sweep
    Note V2 peaks at reversal

     

    Nevertheless, gating so sampling occurs – for 137Hz square wave excitation for window between say 1ms and 3ms from reversal keeps clear of erroneous readings, but the spikes can put stress on the input circuitry.

     

    Analysis and comments on injection waveforms to follow in part 3.

     

    Notes

    (a)    Dummy load - the purely-resistive dummy load totalled 4k7, chosen as representative of the resistance found on the injection path C1C2 on this traverse. The load was made of 2k [tap] 200R [tap] 2k5; the C1C2 injection was applied across the full 4k7, but when needed the P1 and P2 probes were applied across the two taps so they only measured the differential voltage across 200R as typical for the actual resistance measured P1P2 on this traverse.

     

    Continued in part 3

    DM 23 Aug 2020

    Attachments:
    imageARMP plots 2 v06.pdf
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • davemartin
    0 davemartin over 6 years ago in reply to davemartin

    ARMP – field plots, part 3

     

    Basic injection voltage (V1) and current (I) between C1C2 and resultant differential voltage (V2) between P1P2 were covered in part 1, all using standard archaeological geophysics preferred 137Hz square-wave excitation. Part 2 addressed some controls, background interference, and detected signal range using square-wave excitation.

     

    Part 3 now documents various stimuli – varying the square wave frequency, and then using alternative waveforms. Analysis of those, and implications thereof, will follow in part 4.


    Method

     

    Archaeological geophysics commonly uses 137Hz square-wave excitation, with options to reduce the frequency. To inform discussion on excitation strategies, the following stimuli were tested:

    • Square wave 137Hz
    • Square wave 80Hz
    • Square wave 32Hz
    • Sine wave 137Hz
    • Triangle / symmetric sawtooth wave 137Hz
    • Trapezoid wave 137Hz


    In each of the alternative excitation scenarios, a recording was made of the injection results between C1 and C2 (V1and I), the resultant differential potential between P1 and P2 (V2), and the derived resistance (V2), across the full 50m of the test traverse. For each of the above stimuli, a control was also conducted using the full length of the survey leads, but connected to a dummy load of instead of the probes, to check for any artefacts.

     

    Alternative stimuli (1) - different frequency square waves

     

    The main results in part 1 were all collected using square-wave excitation at 137Hz, but to demonstrate settling and the effect of polarisation, comparisons were also run at 80Hz and 32Hz.

     

    At 137 Hz

    image

    Fig 3.1 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 137Hz
    (single sweep)

     

     

    image

    Fig 3.2 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 137Hz
    (averaged in scope)

     

     

    image

    Fig 3.3 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m
    with 137Hz square wave stimulus (based on data averaged in scope)

     

     

    At 80Hz

     

    image

    Fig 3.4 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 80Hz
    (single sweep)

     

     

    image

    Fig 3.5 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 80Hz
    (averaged in scope)

     

     

    image

    Fig 3.6 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m with 80Hz square wave stimulus (based on data averaged in scope)

     

     

    At 32Hz

     

    image

    Fig 3.7 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 32Hz
    (single sweep)

     

     

    image

    Fig 3.8 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 32Hz
    (averaged in scope)

     

     

    image

    Fig 3.9 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m with 32Hz square wave stimulus (based on data averaged in scope)

     

     

    Alternative stimuli (2) – 137Hz sine wave

     

    image

    Fig 3.10 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz sine wave stimulus (single sweep)

     

     

    image

    Fig 3.11 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz sine wave stimulus (averaged in scope)

     

     

    image

    Fig 3.12 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m with 137Hz sine wave stimulus (based on data averaged in scope)

     

     

    Alternative stimuli (3) – 137Hz triangular/sawtooth waveform (equal rise and fall times)

     

    image

    Fig 3.13 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz triangle wave stimulus (single sweep)

     

     

    image

    Fig 3.14 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz triangle wave stimulus (averaged in scope)

     

     

    image

    Fig 3.15 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform
    at X=50m with 137Hz triangle wave stimulus (based on data averaged in scope)

     

     

    Alternative stimuli (4) – trapezoid waveform

     

    Final test in this batch was using trapezoid stimulus, base frequency 137Hz, using Wavetek 275 arbitrary waveform function (signal definition +/- 2,047 points in Y, 2048 points in X, per cycle => 3.56 μs/step).

     

    Proportions chosen for Rise | High | Fall | Low were 1:4:1:4 so rise and fall times both 10% of total cycle time and steady high and low states 40% each. For 137Hz, cycle time 7.3ms, rise and fall times 0.73ms, theoretical stimulus steady states 2.92 ms.

     

     

    image

    Fig 3.16 – Control - Injection waveform (V1 and I) waveform with dummy load (4k7)
    between sets of probes instead of soil (full length of survey leads used), 137Hz trapezoid wave

     

     

    image

    Fig 3.17 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz trapezoid stimulus (single sweep)

     

     

    image

    Fig 3.18 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz trapezoid stimulus (averaged in scope)

     

     

    image

    Fig 3.19 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m with 137Hz trapezoid wave stimulus (based on data averaged in scope)

     

     

    Analysis of these excitation strategies, and implications thereof, will follow in part 4.

     

     

    Continued in part 4

    DM 24 Aug 2020

    Attachments:
    imageARMP plots 3 v02.pdf
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • davemartin
    0 davemartin over 6 years ago in reply to davemartin

    ARMP – field plots, part 3

     

    Basic injection voltage (V1) and current (I) between C1C2 and resultant differential voltage (V2) between P1P2 were covered in part 1, all using standard archaeological geophysics preferred 137Hz square-wave excitation. Part 2 addressed some controls, background interference, and detected signal range using square-wave excitation.

     

    Part 3 now documents various stimuli – varying the square wave frequency, and then using alternative waveforms. Analysis of those, and implications thereof, will follow in part 4.


    Method

     

    Archaeological geophysics commonly uses 137Hz square-wave excitation, with options to reduce the frequency. To inform discussion on excitation strategies, the following stimuli were tested:

    • Square wave 137Hz
    • Square wave 80Hz
    • Square wave 32Hz
    • Sine wave 137Hz
    • Triangle / symmetric sawtooth wave 137Hz
    • Trapezoid wave 137Hz


    In each of the alternative excitation scenarios, a recording was made of the injection results between C1 and C2 (V1and I), the resultant differential potential between P1 and P2 (V2), and the derived resistance (V2), across the full 50m of the test traverse. For each of the above stimuli, a control was also conducted using the full length of the survey leads, but connected to a dummy load of instead of the probes, to check for any artefacts.

     

    Alternative stimuli (1) - different frequency square waves

     

    The main results in part 1 were all collected using square-wave excitation at 137Hz, but to demonstrate settling and the effect of polarisation, comparisons were also run at 80Hz and 32Hz.

     

    At 137 Hz

    image

    Fig 3.1 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 137Hz
    (single sweep)

     

     

    image

    Fig 3.2 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 137Hz
    (averaged in scope)

     

     

    image

    Fig 3.3 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m
    with 137Hz square wave stimulus (based on data averaged in scope)

     

     

    At 80Hz

     

    image

    Fig 3.4 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 80Hz
    (single sweep)

     

     

    image

    Fig 3.5 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 80Hz
    (averaged in scope)

     

     

    image

    Fig 3.6 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m with 80Hz square wave stimulus (based on data averaged in scope)

     

     

    At 32Hz

     

    image

    Fig 3.7 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 32Hz
    (single sweep)

     

     

    image

    Fig 3.8 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m at 32Hz
    (averaged in scope)

     

     

    image

    Fig 3.9 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m with 32Hz square wave stimulus (based on data averaged in scope)

     

     

    Alternative stimuli (2) – 137Hz sine wave

     

    image

    Fig 3.10 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz sine wave stimulus (single sweep)

     

     

    image

    Fig 3.11 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz sine wave stimulus (averaged in scope)

     

     

    image

    Fig 3.12 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m with 137Hz sine wave stimulus (based on data averaged in scope)

     

     

    Alternative stimuli (3) – 137Hz triangular/sawtooth waveform (equal rise and fall times)

     

    image

    Fig 3.13 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz triangle wave stimulus (single sweep)

     

     

    image

    Fig 3.14 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz triangle wave stimulus (averaged in scope)

     

     

    image

    Fig 3.15 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform
    at X=50m with 137Hz triangle wave stimulus (based on data averaged in scope)

     

     

    Alternative stimuli (4) – trapezoid waveform

     

    Final test in this batch was using trapezoid stimulus, base frequency 137Hz, using Wavetek 275 arbitrary waveform function (signal definition +/- 2,047 points in Y, 2048 points in X, per cycle => 3.56 μs/step).

     

    Proportions chosen for Rise | High | Fall | Low were 1:4:1:4 so rise and fall times both 10% of total cycle time and steady high and low states 40% each. For 137Hz, cycle time 7.3ms, rise and fall times 0.73ms, theoretical stimulus steady states 2.92 ms.

     

     

    image

    Fig 3.16 – Control - Injection waveform (V1 and I) waveform with dummy load (4k7)
    between sets of probes instead of soil (full length of survey leads used), 137Hz trapezoid wave

     

     

    image

    Fig 3.17 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz trapezoid stimulus (single sweep)

     

     

    image

    Fig 3.18 – Injected current (I) and voltage (V1) and differential P1P2 (V2) waveform at X=50m
    with 137Hz trapezoid stimulus (averaged in scope)

     

     

    image

    Fig 3.19 – Absolute injected current (I), differential P1P2 (V2), and derived soil resistance (R2) waveform at X=50m with 137Hz trapezoid wave stimulus (based on data averaged in scope)

     

     

    Analysis of these excitation strategies, and implications thereof, will follow in part 4.

     

     

    Continued in part 4

    DM 24 Aug 2020

    Attachments:
    imageARMP plots 3 v02.pdf
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to davemartin

    Nice to see some more data, I'll be interested to see your final part.

     

    It would be nice if you were to include some results with more significant noise in the measured voltage.

     

    In your previous post there was a plot of noise from an earthing system but this was largely removed from the

    measurements because it was effectively common mode current noise.

     

    There will be cases where differential mode noise is present and this will appear on the voltage but not the

    current measurement and so can only be removed by filtering.

     

    Did your measurements preserve numerical data that could be run through a series of different processing methods ?

     

    Thanks.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer