Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum How to publish OSHW schematics
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 326 subscribers
  • Views 956 views
  • Users 0 members are here
  • pcb
  • open_source_hardware
Related

How to publish OSHW schematics

e14 Contributor
e14 Contributor over 14 years ago

I'm in the process of finalizing the designs for an open source hardware project (a pressure sensitive iPad stylus, see http://facebook.com/pressurepen ), and I'm at the point where I want to publish and share the various designs. I have 3D models on Thingiverse and Shapeways, and the app source is on Github. How and where should I publish the circuit diagrams and the files for the circuit board?

 

I imagine a standard format for the PCB files would be Eagle, but I think I'd like to publish the circuit diagram or schematic as well, so someone could design their own PCB based on it. Is there a standard format and repository for such things?

  • Sign in to reply
  • Cancel
  • cookieglitch
    0 cookieglitch over 14 years ago

    Not sure about a standard format for this sort of thing, but PDF, JPG etc are usually reliable enough. Just make sure they are of a high enough resolution in case someone wants to make large copies to work from. Nothing worse than trying to scale something to print it out and finding it is all pixelated!

     

    For storing them, the projects site can work, and so can sites like Github. With things like Eagle v6, all the files are XML based, which makes it much easier to use git with them. Either host them in their own repo, or add them into the app source as a seperate folder. Git hub also supports downloads, meaning you could easily create a zip containing all the relevant files like schematics and publish that. You may also want to have a look at the Wiki pages that your Github repo provides. They should let you create some useful project pages to host your images.

     

    Hope this is a useful start for you! Interested to see what other suggestions people have.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I'd suggest that Eagle is not a standard format. Which cad package does someone use, Eagle, Kicad, gEDA, Altium, Mentor, ZenitPCB, TinyCad, Proteus ?  The common theme is that when you go to get a board manufactured, the fab will want Gerber files.

     

    So what do you do ?  Not all cad packages let you import and edit gerber files, but the format used by an individual package is likely limited to that package alone.  There's no correct answer.

     

    However, my thoughts are that if you're going for the "Open Source Hardware" model then using an Open Source cad package is maybe the best way as that gives you some assurance that your design will remain open and accessible should a commercial package disappear or change it's file format without keeping backward compatibility.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sqkybeaver
    0 sqkybeaver over 14 years ago

    the best way to ensure that your project remains open source, and is recontributed to. us as many methods of distribution as posible. plus a few other tips

     

    1. publish schematics as pdf, jpg and native cad files(regardless of format.)

    2. publish your gerbers, there are many free gerber viewers, and it will allow anyone to have boards made. if your board is simple enough(single or double layer) use a jpeg format too for those interested in etching thier own.

    3. try not to use parts that require a nondisclosure agreement just to view datasheets, it may be easy enough to get a data sheet, however it may turn some away from your project.

    4. support your origonal desighn, and share your problems. many of the people involved in the OHS community are more than willing to help with code, hardware, circuit analisis etc.

    5. give a few away, this is a great way to get feedback and an oppertunity to get skilled people involved in your projects.

    6. HAVE ALL DISTRIBUTABLE MATERIAL AVAILABLE IN ONE LOCATION, the easier it is for anyone to get all related info of your project the more will come. (a zip file on github or sourceforge)