• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Polls Are any SBCs ready to replace desktop computers?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 16 Nov 2014 11:51 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:01 PM
  • Views 5857 views
  • Likes 1 like
  • Comments 27 comments
Related
Recommended

Are any SBCs ready to replace desktop computers?

I would love to replace my power-hungry desktop PC with an inexpensive SBC with no audible fan.  However, so far the SBCs I've tried lately (BeagleBone, Raspberry Pi, BeagleBoard) don't have enough processing power to be a viable desktop PC.

 

So, are any of the higher-performance SBCs that have been released lately up to the task?  I'm looking for a GNU/Linux computer that can do a decent job surfing the Internet (I don't care about video or audio performance) and a decent job compiling C programs.  I would say it needs at least 1 GB RAM and SATA for a disk drive.  100 Mb/s Ethernet is adequate, but I'd prefer not going through a USB hub.  Reasonable number of USB ports and HDMI output.  Wi-Fi is not needed or desired.

 

Here are some of the SBCs I've been watching and might consider.  Feel free to add others!  Most of these are OSHW, which is of course preferred.

 

Banana Pi: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

CubieTruck: Allwinner A20 Dual ARM Cortex-A7, 2 GB DDR3, SATA, GBE.

Intel Next Unit of Computing (NUC): Intel Atom or other, up to 8 GB DDR3, SATA, GBE.

MinnowBoard MAX: Intel Atom, 1 or 2 GB DDR3, SATA, GBE.

Olimex LIME2: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

PCduino3Nano: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

RIoTboard: Freescale i.MX6 ARM Cortex-A9, 1GB DDR3, no SATA, GBE.

Wandboard Quad: Freescale i.MX6 Quad ARM Cortex-A9, 2 GB DDR3, SATA, GBE.

  • sbc
  • oshw
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago +5
    Hi John! I've not used many of these, so I can't comment with much knowledge, but I suspect RIoTboard is getting there, certainly running Android it is speedy (if one is happy running Android to do work…
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild +3
    A nice pic of my XU on the back of one of my monitors.
  • fustini
    fustini over 11 years ago in reply to fustini +3
    johnbeetem - I've been using the MinnowBoard MAX as my 3-D printing workstation and love it! I have a USB 3.0 memory stick for the main disk running Ubuntu. It is really the first time I've used a single…
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    I'm currently trying an ODROID-C1 as a desktop computer. ODroid - Oh Boy!  I've got a few start-up hiccups, but so far it looks pretty promising.  I'm writing this on my C1 using Hardkernel's v1.1 release which came on the SD card I ordered with the board.  Performance is actually pretty good.

     

    I'd really like to use v1.2, because it supports the 1440x900 screen resolution of my monitor.  720p works, but it's a little blurry from pixel interpolation and I don't think I'll be able to use it long without eye strain.  I'm trying to boot v1.2 with a 2GB SD card for Linux and a USB hard drive for the root file system.  I can't seem to get HDMI to come up, nor can I get ssh to come up so I can't talk to it to find out what's happening, and I was too cheap to add an extra US$10 for the serial dongle.  Plus my HDMI connection is a little touchy -- I probably need a new Micro HDMI D to full-size HDMI A cable.

     

    But all-in-all a pretty good start and it looks quite promising as a desktop.  ODROID-C1 is new so the software kinks need to be worked out, just like early days of BeagleBoard and RasPi.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to johnbeetem

    johnbeetem wrote:

     

    I'm currently trying an ODROID-C1 as a desktop computer. ODroid - Oh Boy!  I've got a few start-up hiccups, but so far it looks pretty promising...

    ODROID-C1 is working quite well as my main computer.  I got the USB HDD working and upgraded Ubuntu to ODROID's v1.3.  I had a problem with missing and repeated keystrokes and mouse clicks, but I was able to fix that using a USB 1.1 hub hooked up to ODROID-C1's OTG port.

     

    Having a silent computer with decent performance is pretty nifty image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • johnbeetem
    johnbeetem over 11 years ago in reply to johnbeetem

    johnbeetem wrote:

     

    I'm currently trying an ODROID-C1 as a desktop computer. ODroid - Oh Boy!  I've got a few start-up hiccups, but so far it looks pretty promising...

    ODROID-C1 is working quite well as my main computer.  I got the USB HDD working and upgraded Ubuntu to ODROID's v1.3.  I had a problem with missing and repeated keystrokes and mouse clicks, but I was able to fix that using a USB 1.1 hub hooked up to ODROID-C1's OTG port.

     

    Having a silent computer with decent performance is pretty nifty image