Passive Components
  • Technologies
  • More
Passive Components
Forum Any one know what this is?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 6 answers
  • Subscribers 109 subscribers
  • Views 4082 views
  • Users 0 members are here
Related

Any one know what this is?

jw0752
jw0752 over 9 years ago

Disassembling a nice Siemens Circuit board from an X-Ray machine with a early 1990s manufacturer date. Among the salvaged parts was this little fellow:

 

image

 

The blue case had the numbers J29 P120 and Siemens symbol. It looked like the case could be opened so I inserted a knife blade and opened it. Here is what it looked like inside. I set the insides up on the cover in the second shot to get a better picture.

 

image

 

image

 

The device has 6.4K Ohms of resistance.

 

This is just my curiosity asking. Since the machine has European Design and other components I thought someone from there might recognize it.

 

Thanks

John

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +4 verified
    Hi John, Interesting find! I've never seen such a device, but I did see a similar thing on ebay: PTC MINI MIVAR SIEMENS J29 P190 2PIN PEZZI 5 | eBay Apparently a 'switching thermistor' which as it gets…
  • jw0752
    jw0752 over 9 years ago in reply to shabaz +4 suggested
    Hi Shabaz, That was fast. Tomorrow I will run some temperature vs resistance tests on it to see how it reacts. Nice to see the exact thing listed on ebay. Either there is still some relevant application…
  • jc2048
    jc2048 over 9 years ago +4 suggested
    The passive section of Siemens became EPCOS and that then became a part of TDK. Here's a datasheet from their website https://en.tdk.eu/inf/55/db/PTC/PTC_Switching_Plastic_case_230V.pdf
  • jc2048
    0 jc2048 over 9 years ago in reply to jw0752

    That board's been a useful source of bits for you - you've had practically everything off of there other than the passives. You must be a real expert in desoldering by now.

     

    To my shame, I can't even work out where the device was on the board.

     

    The board is evidently mostly a power supply - the 10A fuses and large choke top-right are where the power came in. Transformer T2, bottom left is the bridge from high voltage to low voltage. You can see the secondary to primary feedback along the bottom edge with a guard track - I assume J1 was an optocoupler. The rest in between is a discrete SMPS. Presumably, C30 and C31 were two very nice high voltage electrolytics off the board. You can see it's high voltage by the careful layout and clearances. It's not very easy to say what the top-left (the low voltage side) was doing, unless you tell us the part numbers of the chips you removed.

     

    It might be that the part was a safety measure, as DAB suggests [a reasonable guess without knowing more about the system], but I don't think it's as simple as shutting down if the temperature exceeds 130C. If you were going to shut the device down on the basis of the temperature, I think you'd choose something a lot lower than 130C. Since the board is a power supply, I would imagine it's more likely that it's being used either as an electronic fuse or a way of getting a delay of a few seconds at startup, perhaps to control in-rush or to delay switching until the electrolytics were fully charged.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to jc2048

    Hi Jon

     

    I really wish you lived a little closer as we would have a good time analyzing some of these boards I take apart. I believe that the PTC was in the position marked R164 and it was in series with R159 which I have no way to put a value on at this point. The traces are very small so it was a low current circuit. The board is, as you say a power supply board. In this case a specialized power supply that is designed to supply controlled current to the filament of an X-Ray tube. This has to be controlled as it determines the mA current of the electron beam striking the tungsten target and subsequently the brightness of the x-ray beam. The board also supplies a controlled AC voltage to a high voltage transformer to produce the potential between the X-Ray tube anode and cathode. The High Voltage transformer in this case was enclosed in the same housing that has the X-Ray Tube. This is commonly called the x-ray tube head. In this case the x-ray machine was a panoramic machine designed to take a picture of all the teeth in the mouth by sweeping the x-ray beam around the back of the head and shooting through the skull from the back past the teeth and producing shadows of the teeth on a screen and film that is synchronized to the rotation and in front of the face. The other function of the board was timing as there has to be a short period of filament voltage to allow it to warm up before the high voltage is applied to the Anode and Cathode. Then the rotation of the head and film have to be timed to match the time the x-rays are emitted. I find that there is so much to learn from these boards beyond the value of their salvaged parts. While I lack your skills I often take the time to study the circuits and look up the data sheets on the ICs prior to demolition. Once in a while I find an interesting circuit arrangement and try to duplicate it on a bread board in order to understand it better. Thanks for your input.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 9 years ago in reply to jc2048

    Hi Jon,

     

    My educated guess was based upon a big issue about these machines overexposing patients when they came out.

    The EU in particular mandated automated circuits to "limit" the exposure automatically.

     

    Using that knowledge I deduced that this simple solution was an easy and inexpensive way for the manufacturer to pass the requirement.

     

    Based upon John's measurements, it seemed like a logical function for a device that normally did not belong in a power supply.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<