Passive Components
  • Technologies
  • More
Passive Components
Forum Capacitor identification
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 110 subscribers
  • Views 1764 views
  • Users 0 members are here
Related

Capacitor identification

koudelad
koudelad over 8 years ago

Hello,

 

I would like to ask you for a help with a capacitor identification.

image

I know that it is an electrolytic capacitor with axial leads, used as a filtering capacitor connected to a bridge rectifier. The whole board is a controller board for a 15-year old Vaillant gas boiler.

 

Both capacitors (marked yellow) should be the same and the visible markings are:

B41283

22/40

10.00

GPF

 

I googled the "B41283" and the first result for me is this datasheet http://www.farnell.com/datasheets/51606.pdf

However, I am not sure about the capacity, voltage and temperature rating. I am probably just missing how to get it from the markings mentioned above.

 

Could you help me identify it and/or recommend a substitute (preferably on EU Farnell site)?

 

Thank you,

David

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +4 verified
    Best Guess is 22 uF at 40 Volts John
  • jw0752
    jw0752 over 8 years ago +3 suggested
    Hi David, I can see from the size chart in the Data Sheet you provided that the 22 uF at 40 Volt units have dimensions of 6.5mm in diameter by 15.5 mm long. You can verify this on your board. Do you have…
  • shabaz
    shabaz over 8 years ago +3 suggested
    Hi David, I believe these are 22uF 40V capacitors, so for a boiler if you get ones with a long life at 105 degrees C, they should be fine. These two should be suitable, provided they are not too large…
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Best Guess is 22 uF at 40 Volts

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago

    Best Guess is 22 uF at 40 Volts

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer