Passive Components
  • Technologies
  • More
Passive Components
Forum I want to make a capacitor discharge tool
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 15 answers
  • Subscribers 113 subscribers
  • Views 12167 views
  • Users 0 members are here
  • passives_featured
  • capacitor_discharge_tool
Related

I want to make a capacitor discharge tool

jw0752
jw0752 over 8 years ago

I want to make a capacitor discharge tool for use in an industrial application where the voltage may be as high as 400 volts and I have no idea what the maximum capacitance may be. I have been weighing the pros and cons of different resistor values. Then I thought, Why not ask some of the best engineers on the planet? If you have some insights for me it would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +8 suggested
    Sounds like it's for a switch mode power supply. Most of them are 470-1000uF, and to prevent damage you'd want to restrict the current to 1A. R= E/I so 400/1 = 400 ohms. Discharge from here https://www…
  • jw0752
    jw0752 over 8 years ago in reply to jc2048 +7 suggested
    Hi Jon, As promised I have run some experiments after returning home. I have taken a 2000 uF 200 Volt capacitor and charged it up. The formula for energy in a capacitor is 1/2 CV^2 which works out to about…
  • jw0752
    jw0752 over 8 years ago +7 suggested
    Last Post: I put the unit together this afternoon using the advice and wisdom from my Forum friends. The series resistor was lowered to 330 ohms and wattage increased to 5 Watts. I discharged the 2000…
Parents
  • three-phase
    0 three-phase over 8 years ago

    When shorting a capacitor you have to remember that the initial energy is quite high and your components will need to be specified to add reliability onto the system, especially if this for an industrial application in use by others.

     

    You will also need to consider the safety implications of the physical design.

     

    When we manually discharge high voltage apparatus, our discharge sticks are built with the discharge element in the actual probe to limit where the high voltage appears in the circuit. Whilst a lower value discharge resistor gives a faster discharge, it will put higher voltage around the rest of the circuit.

     

    The second element of the discharge stick is used to put a complete short across the circuit after we have discharged with the resistive element, then we know for definite that there is no voltage present.

     

    In some respects some of the low voltage detectors that we use can do this as they have a switched load resistor built into them, so the voltage can initially be checked with the probe and then the load resistor switched in to increase the discharge rate.

     

    There are some designs available on stack exchange that may be useful to you;

     

    Capacitor discharge tool

     

    There are also some commercially available items, that you could take a look at, seems this particular one is limited to 350V though.

     

    Ebay capacitor discharge tool

     

    Kind regards

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • three-phase
    0 three-phase over 8 years ago

    When shorting a capacitor you have to remember that the initial energy is quite high and your components will need to be specified to add reliability onto the system, especially if this for an industrial application in use by others.

     

    You will also need to consider the safety implications of the physical design.

     

    When we manually discharge high voltage apparatus, our discharge sticks are built with the discharge element in the actual probe to limit where the high voltage appears in the circuit. Whilst a lower value discharge resistor gives a faster discharge, it will put higher voltage around the rest of the circuit.

     

    The second element of the discharge stick is used to put a complete short across the circuit after we have discharged with the resistive element, then we know for definite that there is no voltage present.

     

    In some respects some of the low voltage detectors that we use can do this as they have a switched load resistor built into them, so the voltage can initially be checked with the probe and then the load resistor switched in to increase the discharge rate.

     

    There are some designs available on stack exchange that may be useful to you;

     

    Capacitor discharge tool

     

    There are also some commercially available items, that you could take a look at, seems this particular one is limited to 350V though.

     

    Ebay capacitor discharge tool

     

    Kind regards

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 8 years ago in reply to three-phase

    Thanks Donald,

    As usual there is nothing new under the Sun. The links you provided will be helpful in deciding how to proceed.

    John

    • Cancel
    • Vote Up +3 Vote Down