Passive Components
  • Technologies
  • More
Passive Components
Forum I want to make a capacitor discharge tool
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 15 answers
  • Subscribers 113 subscribers
  • Views 12143 views
  • Users 0 members are here
  • passives_featured
  • capacitor_discharge_tool
Related

I want to make a capacitor discharge tool

jw0752
jw0752 over 8 years ago

I want to make a capacitor discharge tool for use in an industrial application where the voltage may be as high as 400 volts and I have no idea what the maximum capacitance may be. I have been weighing the pros and cons of different resistor values. Then I thought, Why not ask some of the best engineers on the planet? If you have some insights for me it would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +8 suggested
    Sounds like it's for a switch mode power supply. Most of them are 470-1000uF, and to prevent damage you'd want to restrict the current to 1A. R= E/I so 400/1 = 400 ohms. Discharge from here https://www…
  • jw0752
    jw0752 over 8 years ago in reply to jc2048 +7 suggested
    Hi Jon, As promised I have run some experiments after returning home. I have taken a 2000 uF 200 Volt capacitor and charged it up. The formula for energy in a capacitor is 1/2 CV^2 which works out to about…
  • jw0752
    jw0752 over 8 years ago +7 suggested
    Last Post: I put the unit together this afternoon using the advice and wisdom from my Forum friends. The series resistor was lowered to 330 ohms and wattage increased to 5 Watts. I discharged the 2000…
Parents
  • dougw
    0 dougw over 8 years ago

    I like the simple resistor approach, but if you want to have some fun you could get a sample of a USCi UJN1205K and play around with it. These devices can act as current limiters up to 1200 V - without power supplies. I'd like to see what jc2048 would do with it. Maybe devise some zener circuit to get Vgs to be 4 V.

    By the way - good application for your special probes.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to dougw

    Hi Doug,

    I will take a look at the UJN1205K.  I would like to keep the build simple and I would like to have some sort of indicator of the voltage. Here is an idea that came to mind. Ideally I will be able to find a sensitive LED that will indicate at low current levels. I think this will indicate voltage down to less than 10 volts though I am away from the shop so I can't actually build and test. Voltage above approximately 2 volts will cause current to flow through the shunt diodes D1 - D3. The bridge will make the polarity of the discharge probes irrelevant. R1 will limit discharge current to less than 1 amp at 400 volts. Watching the LED go from lit to off will encourage the operator to leave the discharge shunt in place long enough for voltages to drop to safe levels. I was already thinking of adding the non-slip tips into the build. The larger 1.2 mm size tips would be ideal for ensuring that the probe stay in place and make good contact with the capacitor leads. Thanks for you suggestions.

     

    image

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 8 years ago in reply to jw0752

    Doesn't R1 need to be a higher wattage than 0.5W?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to jc2048

    Hi Jon,

    I have been kicking that question around in my head. If we were dealing with a continuous current I would say certainly but in the case of these discharges over a few seconds at 1 amp I wonder if the heat generated even has time to get to the surface of the resistor before it has tapered off to nothing. When I get time tonight I am going to look at the actual energy in joules that is being dissipated in a high level discharge and see if a higher wattage resistor would be needed. I will also look to see if there are data sheets on resistors that list a tolerance for over wattage for a short time interval. The only downside to putting a higher wattage resistor in place will be size and convenience.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to jc2048

    Hi Jon,

    I put some numbers on paper last night to see if I could make a better guess at the wattage needed for the shunt resistor. I will not get into a lot of detail but there were a couple of interesting things pop up. In most cases as the voltage of the circuit goes up the need for high capacitance goes down. Many common switching supplies use a 400 Volt 100 uF capacitor in the primary section of the supply. A 400 V 100 uF capacitor, fully charged, holds about 8 Joules of energy. If this capacitor is discharged through a 470 Ohm shunt we drop the voltage by 63.2% in the first time constant of 47 milliseconds. What surprised me was to find that the energy in the capacitor drops by 87.5% in this same time period. This puts the energy discharge predominately in the first period of 47 milliseconds. This 7 Joules of energy is manifest as heat in the core of the resistor. Since it occurs very quickly we can't expect there to be much dissipation by conduction. The best remedy to potential heat failure of the resistor is to increase the amount of resistive material that will be heated. This tells me that Jon's suggestion that a 1/2 Watt resistor is probably not adequate for this situation is correct. A real test will have to wait until I get back to the shop where a number of resistors will be treated to some real world tests to see how they react to this type off discharge. Obviously as the capacitance goes up at the higher voltage levels the challenge to discharge also increases accordingly.

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to jc2048

    Hi Jon,

    As promised I have run some experiments after returning home. I have taken a 2000 uF 200 Volt capacitor and charged it up. The formula for energy in a capacitor is 1/2 CV^2 which works out to about 40 Joules for this capacitor. I built the circuit in my schematic above using a 1/2 Watt 470 ohm series discharge resistor.

     

    image

     

    As you can see from the color of the resistor it sustained heat damage after three discharges. Here is a video of the action:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    A second test using a 1 Watt 470 Ohm resistor was able to handle the discharge without any problem. The resistor did heat up but was able to be touched after the experiment. I would estimate it got to about 45 degrees C.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    We were originally discussing a 100 uF 400V capacitor like one we might find in a small switching power supply. The energy storage for 100UF at 400 V is E=1/2CV^2 or 8 Joules. I have no easy way to put 400 volts on a 100 uF capacitor so I decided to simulate this by putting only 8 Joules of charge into the Capacitor in the above experiment. This works out using the formula V = SQRT(2E/C) or about 126 Volts. I will run this experiment using a fresh 1/2 watt resistor. Keep in mind this is an imperfect match as 400 volts from 100 uF would discharge the 8 Joules of energy much more quickly than our 126 volts from the 1000 uf capacitor. Here is a video of the test:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    My conclusion is that the design in the schematic works well and while the 1/2 watt resistor would probably work for the 100 uF 400 V situation it would not be adequate for the 2000 uF 200 Volt capacitor. Jon's suggestion to use a higher wattage resistor is confirmed as the best way to go.

     

    John

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago in reply to jc2048

    Hi Jon,

    As promised I have run some experiments after returning home. I have taken a 2000 uF 200 Volt capacitor and charged it up. The formula for energy in a capacitor is 1/2 CV^2 which works out to about 40 Joules for this capacitor. I built the circuit in my schematic above using a 1/2 Watt 470 ohm series discharge resistor.

     

    image

     

    As you can see from the color of the resistor it sustained heat damage after three discharges. Here is a video of the action:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    A second test using a 1 Watt 470 Ohm resistor was able to handle the discharge without any problem. The resistor did heat up but was able to be touched after the experiment. I would estimate it got to about 45 degrees C.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    We were originally discussing a 100 uF 400V capacitor like one we might find in a small switching power supply. The energy storage for 100UF at 400 V is E=1/2CV^2 or 8 Joules. I have no easy way to put 400 volts on a 100 uF capacitor so I decided to simulate this by putting only 8 Joules of charge into the Capacitor in the above experiment. This works out using the formula V = SQRT(2E/C) or about 126 Volts. I will run this experiment using a fresh 1/2 watt resistor. Keep in mind this is an imperfect match as 400 volts from 100 uF would discharge the 8 Joules of energy much more quickly than our 126 volts from the 1000 uf capacitor. Here is a video of the test:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    My conclusion is that the design in the schematic works well and while the 1/2 watt resistor would probably work for the 100 uF 400 V situation it would not be adequate for the 2000 uF 200 Volt capacitor. Jon's suggestion to use a higher wattage resistor is confirmed as the best way to go.

     

    John

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer