Passive Components
  • Technologies
  • More
Passive Components
Forum I want to make a capacitor discharge tool
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 15 answers
  • Subscribers 113 subscribers
  • Views 12166 views
  • Users 0 members are here
  • passives_featured
  • capacitor_discharge_tool
Related

I want to make a capacitor discharge tool

jw0752
jw0752 over 8 years ago

I want to make a capacitor discharge tool for use in an industrial application where the voltage may be as high as 400 volts and I have no idea what the maximum capacitance may be. I have been weighing the pros and cons of different resistor values. Then I thought, Why not ask some of the best engineers on the planet? If you have some insights for me it would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +8 suggested
    Sounds like it's for a switch mode power supply. Most of them are 470-1000uF, and to prevent damage you'd want to restrict the current to 1A. R= E/I so 400/1 = 400 ohms. Discharge from here https://www…
  • jw0752
    jw0752 over 8 years ago in reply to jc2048 +7 suggested
    Hi Jon, As promised I have run some experiments after returning home. I have taken a 2000 uF 200 Volt capacitor and charged it up. The formula for energy in a capacitor is 1/2 CV^2 which works out to about…
  • jw0752
    jw0752 over 8 years ago +7 suggested
    Last Post: I put the unit together this afternoon using the advice and wisdom from my Forum friends. The series resistor was lowered to 330 ohms and wattage increased to 5 Watts. I discharged the 2000…
Parents
  • dougw
    0 dougw over 8 years ago

    I like the simple resistor approach, but if you want to have some fun you could get a sample of a USCi UJN1205K and play around with it. These devices can act as current limiters up to 1200 V - without power supplies. I'd like to see what jc2048 would do with it. Maybe devise some zener circuit to get Vgs to be 4 V.

    By the way - good application for your special probes.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 8 years ago in reply to dougw

    I'm not too good with FETs - when I started out they were a bit exotic and I've never had to use them for anything.

     

    A constant-current configuration would be like this, wouldn't it?

     

    image

     

    The FET shuts down when the gate gets to below about -6V (below the source), so that would regulate the voltage across the resistor to about 6V and keep the current at around an amp.

     

    It would need a reasonable heatsink - initial dissipation is 400W (on 400V), although it comes down quite rapidly. The 6 ohm resistor would need to be 10W or so.

     

    That SiC part is very expensive though. You could build a whole constant-current load with a MOSFET for that (including a processor to give you constant-wattage rather than constant-current and other nice things).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 8 years ago in reply to dougw

    I'm not too good with FETs - when I started out they were a bit exotic and I've never had to use them for anything.

     

    A constant-current configuration would be like this, wouldn't it?

     

    image

     

    The FET shuts down when the gate gets to below about -6V (below the source), so that would regulate the voltage across the resistor to about 6V and keep the current at around an amp.

     

    It would need a reasonable heatsink - initial dissipation is 400W (on 400V), although it comes down quite rapidly. The 6 ohm resistor would need to be 10W or so.

     

    That SiC part is very expensive though. You could build a whole constant-current load with a MOSFET for that (including a processor to give you constant-wattage rather than constant-current and other nice things).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jc2048
    0 jc2048 over 8 years ago in reply to jc2048

    Just in case someone decides to try this - the device can't manage 400W anyway, so the current would have to be lower.