Passive Components
  • Technologies
  • More
Passive Components
Forum I want to make a capacitor discharge tool
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 15 answers
  • Subscribers 113 subscribers
  • Views 12142 views
  • Users 0 members are here
  • passives_featured
  • capacitor_discharge_tool
Related

I want to make a capacitor discharge tool

jw0752
jw0752 over 8 years ago

I want to make a capacitor discharge tool for use in an industrial application where the voltage may be as high as 400 volts and I have no idea what the maximum capacitance may be. I have been weighing the pros and cons of different resistor values. Then I thought, Why not ask some of the best engineers on the planet? If you have some insights for me it would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +8 suggested
    Sounds like it's for a switch mode power supply. Most of them are 470-1000uF, and to prevent damage you'd want to restrict the current to 1A. R= E/I so 400/1 = 400 ohms. Discharge from here https://www…
  • jw0752
    jw0752 over 8 years ago in reply to jc2048 +7 suggested
    Hi Jon, As promised I have run some experiments after returning home. I have taken a 2000 uF 200 Volt capacitor and charged it up. The formula for energy in a capacitor is 1/2 CV^2 which works out to about…
  • jw0752
    jw0752 over 8 years ago +7 suggested
    Last Post: I put the unit together this afternoon using the advice and wisdom from my Forum friends. The series resistor was lowered to 330 ohms and wattage increased to 5 Watts. I discharged the 2000…
Parents
  • dougw
    0 dougw over 8 years ago

    I like the simple resistor approach, but if you want to have some fun you could get a sample of a USCi UJN1205K and play around with it. These devices can act as current limiters up to 1200 V - without power supplies. I'd like to see what jc2048 would do with it. Maybe devise some zener circuit to get Vgs to be 4 V.

    By the way - good application for your special probes.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to dougw

    Hi Doug,

    I will take a look at the UJN1205K.  I would like to keep the build simple and I would like to have some sort of indicator of the voltage. Here is an idea that came to mind. Ideally I will be able to find a sensitive LED that will indicate at low current levels. I think this will indicate voltage down to less than 10 volts though I am away from the shop so I can't actually build and test. Voltage above approximately 2 volts will cause current to flow through the shunt diodes D1 - D3. The bridge will make the polarity of the discharge probes irrelevant. R1 will limit discharge current to less than 1 amp at 400 volts. Watching the LED go from lit to off will encourage the operator to leave the discharge shunt in place long enough for voltages to drop to safe levels. I was already thinking of adding the non-slip tips into the build. The larger 1.2 mm size tips would be ideal for ensuring that the probe stay in place and make good contact with the capacitor leads. Thanks for you suggestions.

     

    image

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 8 years ago in reply to jw0752

    Doesn't R1 need to be a higher wattage than 0.5W?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to jc2048

    Hi Jon,

    I have been kicking that question around in my head. If we were dealing with a continuous current I would say certainly but in the case of these discharges over a few seconds at 1 amp I wonder if the heat generated even has time to get to the surface of the resistor before it has tapered off to nothing. When I get time tonight I am going to look at the actual energy in joules that is being dissipated in a high level discharge and see if a higher wattage resistor would be needed. I will also look to see if there are data sheets on resistors that list a tolerance for over wattage for a short time interval. The only downside to putting a higher wattage resistor in place will be size and convenience.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago in reply to jc2048

    Hi Jon,

    I have been kicking that question around in my head. If we were dealing with a continuous current I would say certainly but in the case of these discharges over a few seconds at 1 amp I wonder if the heat generated even has time to get to the surface of the resistor before it has tapered off to nothing. When I get time tonight I am going to look at the actual energy in joules that is being dissipated in a high level discharge and see if a higher wattage resistor would be needed. I will also look to see if there are data sheets on resistors that list a tolerance for over wattage for a short time interval. The only downside to putting a higher wattage resistor in place will be size and convenience.

    John