Passive Components
  • Technologies
  • More
Passive Components
Documents Documents
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Document Actions
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Related
Recommended
  • Vishay’s New TPC Series of 1500-W Surface-Mount Automotive TVS in TO-277A Package Features Industry’s Lowest Profile of 1.1 mm

    Source:Vishay High-Power Devices Provide Breakdown Voltages From 6.8 V to 43 V, Clamping Capability From 10.5 V to 61.9 V MALVERN, Pa. — Sept. 30, 2009 — Vishay Intertechnology...
    • Revision #1
    • on 7 Oct 2021 12:53 AM
  • Surface-Mount Resistor from Vishay in Compact 4527 Package

    Vishay has announced that it is expanding its WSR series of Power Metal Strip resistors with the industry's first such device to offer a 5-W power rating in the 4527...
    • Revision #1
    • on 7 Oct 2021 12:48 AM
  • Vishay’s New PLT Series of Precision Low-TCR Thin Film Resistors Offers TCR of ± 5 ppm/°C and Tolerances to ± 0.02 % in Three Case Sizes

    Vishay Intertechnology, Inc. today introduced the new PLT series of precision low-TCR thin film resistors. The devices feature a low standard TCR of ± 5 ppm/°C and tolerances...
    • Revision #1
    • on 7 Oct 2021 12:48 AM
  • Vishay Sfernice Panel Potentiometer Features Long Life of 2 Million Cycles

    Vishay has announced that it has doubled the rotational life of its P30L compact panel potentiometers, which are now specified to deliver 2 million cycles at rated power...
    • Revision #1
    • on 7 Oct 2021 12:46 AM
  • Vishay’s Bulk Metal Foil Ultra-High-Precision Accutrim Trimming Potentiometers

    Vishay has announced two new series of Bulk Metal Foil ultra-high-precision Accutrim trimming potentiometers designed to meet and exceed the requirements of MIL-PRF-39035...
    • Revision #1
    • on 7 Oct 2021 12:46 AM
  • High sensitivity coil for hearing aid applications

    Premo has enlarged its telecoil family with the TC0502 series, a high reliability and sensitivity coil for application in hearing aids developed according to the highest...
    • Revision #1
    • on 7 Oct 2021 12:46 AM
  • DR217 Series Economical Radial Leaded Inductors Deliver Highly Reliable EMI/RFI Protection

    Designed for accuracy and economy, the new Model DR217 Series Radial Leaded Inductors from Datatronic Distribution, Inc., combine superior performance, reliability and...
    • Revision #1
    • on 7 Oct 2021 12:46 AM
  • Vishay’s New Small-Form-Factor, Multilayer Ceramic Chip Antennas for Mobile Devices are Industry’s First to Cover Entire UHF Band From 470 MHz to 860 MHz

    Source:Vishay MALVERN, PENNSYLVANIA — Oct. 14, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the industry’s first high-performance multilayer ceramic...
    • Revision #1
    • on 7 Oct 2021 12:38 AM
  • Upgraded Vishay Sfernice P30L Panel Potentiometer Features Long Life of 2 Million Cycles and Low Temperature Coefficient Down to ± 150 ppm/°C in Compact, Fully Sealed IP67 Package

    Source:Vishay MALVERN, Pa. — Oct. 7, 2009 — Vishay Intertechnology Inc. (NYSE: VSH) today announced that it has doubled the rotational life of its P30L compact panel...
    • Revision #1
    • on 7 Oct 2021 12:37 AM
  • Vishay’s New High-Precision Flat Chip Resistors in Thin Film Technology Feature Tolerances Down to ± 0.05 % and TCR as Low as ± 5 ppm/K in 0603, 0805, and 1206 Case Sizes

    Source: Vishay MALVERN, PENNSYLVANIA — Sept. 23, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of the new TNPU e3 series of high-precision...
    • Revision #1
    • on 7 Oct 2021 12:36 AM
  • Vishay’s New-Generation, Ultra-Precision VHP100 Bulk Metal Foil Resistor is Shortlisted for Elektra 09 European Electronics Industry Awards

    Source:Vishay MALVERN, PENNSYLVANIA — Sept. 28, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the new generation of its VHP100 hermetically sealed...
    • Revision #1
    • on 7 Oct 2021 12:36 AM
  • Can ESR be too low?

    Can ESR be too low? Attachments: community.element14.com/.../2010_2D00_04-CARTS-_2D00_-Can-ESR-Be-Too-Low.pdf 2010-04 CARTS - Can ESR Be Too Low.pdf
    • Revision #1
    • on 6 Oct 2021 9:51 PM
  • New waterploof tact switch from Alps Electric

    We're pleased to introduce our new waterploof tact switch. compact and thin package will especially suitable for mobile, wearable products. SKTADAE010 Features: Improve...
    • Revision #1
    • on 6 Oct 2021 9:45 PM
  • ALPS / Tact Switch new variety released, SKSN series

    We're pleased to introduce new variery of tact switch SKSN series. High operating force type was added. Applications: - Keyless entry - Car audio&navigation - Mobile...
    • Revision #1
    • on 6 Oct 2021 9:45 PM
  • ALPS / high-operating force added to tact switch SKSL series

    We're pleased to introduce new variety of side push tact switch SKSL series. High operating force type (operating force: 3.5N) was newly added. Applications: Keyless...
    • Revision #1
    • on 6 Oct 2021 9:44 PM
  • ALPS / long-life type is added to tactile switch SKRP series

    We're pleased to introduce new variety of sharp feeling tactile switch SKRP series. Operating life of new version is 10 times longer than current products. Futures: ...
    • Revision #1
    • on 6 Oct 2021 9:44 PM
  • ALPS / Surface Mount TACT Switch™︎ with Soft Operating Feel SKPS Series

    High Operating Force and Long Life Suited to Automotive Applications Features ● High operating force (3.0N or 3.6N) suited to automotive equipment requirements ● Long...
    • Revision #1
    • on 6 Oct 2021 9:42 PM
  • ALPS / TACT Switch™︎ Middle Travel Type SKTQ Series

    Features ● High operating force (5N) helps prevent accidental operations ● Quiet operation and definite clicking feel ● Pre-stroke design used to prevent play ● Compact...
    • Revision #1
    • on 6 Oct 2021 9:41 PM
  • ALPS / Surface Mount TACT Switch™︎ with Projection SKTA Series

    Features ● Compact dimensions: 2.6 × 1.6mm ● IP67-equivalent dust and water resistance ● Long operating life of 300,000 cycles ● Has a projection preventing differences...
    • Revision #1
    • on 6 Oct 2021 9:41 PM
  • capacitor help

    need some help with a capacitor there is so much information on this cap but it does not come out and tell you the capacitance so I'm having a hard time figuring out...
    • Revision #1
    • on 6 Oct 2021 8:49 PM
<>