Power & Energy
  • Technologies
  • More
Power & Energy
Alt Energy Solutions & Tech USA's largest solar farms
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
  • Author Author: Eavesdropper
  • Date Created: 30 Mar 2011 3:03 AM Date Created
  • Views 1338 views
  • Likes 1 like
  • Comments 5 comments
  • solar_panel
  • solar_farm
  • kyocera
  • sempra_generation
  • offgrid
  • solar
  • solar_cell
  • innovation
Related
Recommended

USA's largest solar farms

Eavesdropper
Eavesdropper
30 Mar 2011
image
Copper Mountain Solar Installation via Sempra Generation
 
In Nevada, 40 miles southeast of Las Vegas, sits the United State's largest solar installation. Sempra Generation's 775,000 solar panels fill 380 acres generating 48 Mega-watts of electricity. This site is adjacent to an older 10 Mega-watt facility in El Dorado. Together, these sites will power 14,000 homes in California via Pacific Gas & Electric (PG&E) over the next 20 years.
 

image
Mesquite Solar I planned location via Sempra Generation
 
Sempra Generation is not stopping here. Mesquite Solar I, a project in its first phase, is planned to eclipse the Nevada location by a factor of 12.5. 600 Mega-watts will pour from this Arlington Arizona based solar farm, powering up to 56,000 additional homes. This is a commendable effort.
 
 
Perhaps they should bring the panels to power each home directly. I decided to do a little math and figure out how much space and average price this may cost each person.
 
I will use the Kyocera KC175GT, a 175 watt solar panel.
I let it collect sunshine for 6 hours a day. Giving me a total of (175x6) 1050 watt hours. 1.05kwh
The size is 4.2 feet by 3.25 feet. Or 13.65 square feet.
An average home requires about 50kwh. (2 - 3 story home)
So I need approximately 48 panels to power the home. (50/1.05 = 47.62)
Which is a total of 655.2 square feet. And this is 1/66th of an acre.
Each panel costs $770 USD at the moment, on sale. Or $36,960 total for 48 panels.

Although that his a high price to pay to be green, I am sure Sempra Generation could provide each person with panels for far less. I hope they read this and get inspired to go individual generation someday.
 
Eavesdropper
  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    When reading that the 17 power plants have 55 reactors total in Japan - they only supply 24% of the power used...  Seems like an incredible price to pay for green -   How green is green when it is dead or contaminated...  These panels are taking up a great deal of space -  what is the ratio?  Your calculations are relatively close to my own and I think that your remark about going into a different direction is exactly right.  What about places like Washington and Michigan where constant sunshine is not such a regualrity?  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to e14 Contributor

    In non-sunny areas, other energy solutions would have to be taken into consideration. Like geo-thermal differentials, wind/wave motion, etc. But each option has its own drawbacks.

     

    Waste water may be a good option to investigate.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to e14 Contributor

    In non-sunny areas, other energy solutions would have to be taken into consideration. Like geo-thermal differentials, wind/wave motion, etc. But each option has its own drawbacks.

     

    Waste water may be a good option to investigate.

     

    E