Power & Energy
  • Technologies
  • More
Power & Energy
Blog Farmers in Egypt Use Solar Panels to Grow Crops
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
  • Author Author: Catwell
  • Date Created: 17 Sep 2026 8:00 AM Date Created
  • Views 400 views
  • Likes 2 likes
  • Comments 3 comments
  • Agrovoltaics
  • alternative energy
  • farming
  • power
  • energy
  • solar
  • innovation
Related
Recommended

Farmers in Egypt Use Solar Panels to Grow Crops

Catwell
Catwell
17 Sep 2026

image

Agrovoltaics. (Image Credit: ADMC/pixabay)

For thousands of years, Egypt has made agriculture work in its harsh environment. Nowadays, however, farmers are facing more challenges: water scarcity and increasing temperatures that damage crops. Agrovoltaics can help with those issues. Solar panels generate electricity over farmland and shade the plants and soil, keeping them cooler. Initiatives in Egypt supported by funders and partnering organizations have been testing this technique in small farms.

South Sinai is using a 6kWp installation for research and demonstration, while a 100kWp implementation is being deployed in Al Moghra, Marsa Matrouh.

The good part about this is that solar panels don’t compete with crops for sunlight. Sometimes, placing panels in certain areas can lead to more ideal growing conditions for plants. Scientists are testing various configurations. And one of them has checkerboard-style layouts that are being considered in Egypt. This means more sunlight reaches the crops compared to standard solar farms. At the same time, these don’t produce as much electricity since there’s more space between each panel. 

Extra shade is beneficial since water doesn’t evaporate as quickly. In the United States, agrovoltaics’ shading actually reduced the plants’ requirement for water and improved water-use efficiency. It also keeps them safe from the heat and sometimes extreme winds. Researchers are trying out transparent solar panels so light can pass through as it generates power.  

We can’t rely on a single formula for solar power and agriculture. Different crops need different light in addition to temperature and water. Ideally, panels should be set up based on the farm type. Projects like those in Egypt and other places have used different methods to collect data on how well the solar panels and crops are doing. Those results help farmers and scientists determine how they can best adapt agrovoltaics to crops and local conditions.

Evaluating exactly how crops respond to these panels will take time. These projects are also determining whether the generated power benefits the communities. So far, the power is used for running irrigation equipment. It may even support desalination plants to convert the brackish water in the area to water for agriculture.  

New farming opportunities could arise in areas where water and electricity are valuable. Egypt’s agrivoltaics experiments may show others how solar power can be added to agriculture without making local communities choose between food and power production.

“At 3E, we believe in a world powered by renewable energy. Yet too often, the communities that could benefit the most remain beyond the reach of innovation and support. Through the support of the Government of Flanders, Belgium and strong collaboration with research partners, we have been able to bring state-of-the-art solar design and digital solutions to a nomadic community in South Sinai. Our ambition is to see this initiative scale and evolve into a community-driven model that delivers lasting energy access, resilience, and local economic value,” says Gofran Chowdhury, Head of Innovation at 3E.

Have a story tip? Message me here at element14.

  • Sign in to reply
Parents
  • ralphjy
    ralphjy 24 days ago

    It would be nice to see the long term plan for sustainability of these installations.  Witnessing all the issues with replacing aging infrastructure makes me worry about large scale deployments of this type in harsh environments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy 24 days ago

    It would be nice to see the long term plan for sustainability of these installations.  Witnessing all the issues with replacing aging infrastructure makes me worry about large scale deployments of this type in harsh environments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave 24 days ago in reply to ralphjy

    I suspect that if you fast-forward 50+ years, then you'll see lots of twisted and rusted angle iron sticking out of concrete foundations where those solar arrays once stood. Similar to what you see now from installs 50+ years ago.

    I think some of the planning has a condition that it has to be removed after 25 - 30 years, but chances are the original company responsible, will have gone into administration long before then.