• Products and Partners
    Products and Partners
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
Power & Energy
  • Technologies
  • More
Power & Energy
Blog Measure Unknown Inductor Value with Function Generator and Oscilloscope
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
  • Author Author: Jan Cumps
  • Date Created: 26 Sep 2020 9:44 PM Date Created
  • Views 8456 views
  • Likes 12 likes
  • Comments 19 comments
  • inductance
  • smps
  • experimenting_with_magnetic_components
Related
Recommended

Measure Unknown Inductor Value with Function Generator and Oscilloscope

Jan Cumps
Jan Cumps
26 Sep 2020

There are affordable switch mode DC converters available.

One that you see often is this Benq 12 V to 5V converter.

image

I can find info on all components, except the inductor. And I don't have an inductance meter.

There are several other ways to measure inductance. In this exercise I'm using the method with triangle waveform as described on meettechniek.info.

 

Ingredients:

  • the inductor, desoldered
  • a function generator with triangle waveform option
  • an oscilloscope

 

The setup is straightforward.

Set the generator to 50 Ohm and tune it in to a reasonable frequency. I set it at 10 kHz (my inductor is made for the kHz range).

Put the output over the inductor, and the oscilloscope probes.

Then push the voltage of the generator as high as possible, while the waveform doesn't start to show saturation. See the yellow waveform below for an impression.

Then change the frequency so that the voltage drops as low as your oscilloscope can deal with. In my case, I turned it down to 5 kHz.

 

image

 

Then start measuring.

VR: delta of the ramp. I used the delta of horizontal cursors for that: 32 mV

VL: between 0 and halfway the ramp: 95.5 mV.

t: time of the ramp. I used the delta of the vertical cursor for that (and it's half the time of one cycle too): 100 µs.

Ri: impedance of the generator. We had set it to 50 Ohm.

Vg: peak-to-peak output of the generator. Unplug the inductor and measure it with the oscilloscope: 8.16 V.

(I also captured it with the white REF signal but note that it's not at the right horizontal location. The peaks should be at the same spot as the peaks in the yellow trace)

 

... and Calculate the Inductance

(the formula images are from the meettechniek.info site)

image

= 8.16 V / 50 Ohm = 0.16 A

 

image

= 0.095 V * (100 µs / 0.16 A)

= 0.0000594 H = 59 µH

In the common inductor tolerance series, that would most likely be a 68 µH one.

 

 

Validate with the Switch Mode IC specs

Let's check this off with the specs of the LM2576 5V IC that's used in this circuit.

The PCB has an input spec of 12 V. It claims to switch up to 3 A (I found one website that indicated this - most don't claim current).

On the Inductor Select graph, this brings us here:

image

image source: TI LM2576 datasheet

 

That is a match: 68 µH. The expected inductor is used on the PCB.

And the triangle waveform method turned out to be a valid way to get at the inductance of a coil.

 

The whole circuit is exactly the typical application schematic from TI, adjusted for the 12 V input and 3 A output.

image

image source: TI LM2576 datasheet

 

Input and output caps are 220 µF.

The Schottky diode is a On Semiconductor SS34.

 

Link to other magnetics related posts.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz +6
    You are right . I have a known inductor from Velleman, the 50L1, a 50 µH at 1 A, 64 µH at 0 A inductor that has practically the same kernel dimensions, and 41 turns. source: velleman The one one I reviewed…
  • jw0752
    jw0752 over 6 years ago +6
    Hi Jan, I enjoyed your post and it is very timely as I was just playing with a LM2576 T the other day. I have seen the fixed voltage chips and I wanted to see how well the variable voltage variety worked…
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps +5
    Hi Jan, What's the dimensions of the core? From that, and the number of turns, which looks about 30 in your photo, it is maybe possible to guesstimate the core type too : ) From guessing from the photo…
Parents
  • Jan Cumps
    Jan Cumps over 6 years ago

    I'll be able to validate this later this week. I ordered an LRC meter.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps

    Hi Jan,

     

    What's the dimensions of the core? From that, and the number of turns, which looks about 30 in your photo, it is maybe possible to guesstimate the core type too : )

    From guessing from the photo approx dimensions, it may be a 'type 61' ferrite material, which gets into the mid tens of uH ballpark with 30-ish turns at about that size.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz

    shabaz  wrote:

    ....

    From guessing from the photo approx dimensions, it may be a 'type 61' ferrite material, which gets into the mid tens of uH ballpark with 30-ish turns at about that size.

    image

     

    You were spot on! (also showing off my brand new LRC meter that arrived today).

    The triangle wave method was fairly close too. 8 µH off...

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps

    Hi Jan,

     

    That looks like a decent LCR meter, it has separated source and sense connections which is really cool too.

    Does the Cal button request you to open and short the connections? If so, maybe it's possible to build calibration and test fixtures for this LCR meter (or maybe some are supplied), especially for SMD (but would also suit through-hole).

    As a suggestion, if it fits, they could be PCBs with tongues which insert into the device. You could have three (or more). One PCB would allow you to solder on a component (like an 0603 or 0805 location, but with no solder mask over a larger area so that it would be compatible with larger components even through-hole), and another PCB would be identical but kept as a open circuit with nothing ever soldered on it, and another with the same thing, but with a wire or zero-ohm SMD resistor permanently soldered across it. In other words, all the same copper layouts for all three boards, so that inductance and capacitance is about the same for all. Or it could be one board that you rotate around the sides of, to do the different stages. I don't know if that makes sense or if it's even practical.. I'm mentally picturing a PCB that looks like a jigsaw piece from all four sides.

     

    I did a similar thing for my VNA, however that's not got separate source and sense. In this case since it's RF related I had some constraints (and I copied a TI antenna development board and changed the gerber files to suit this different purpose). Here I've accidentally torn off part of the copper at the DUT portion, due to careless heavy use : (  but it's still usable, just not as accurate but 'good enough' for my purposes. I will have to make another, and also add another DUT portion for comparing two components more easily. So that would be another suggestion, to use all four sides, to have more DUT sections : )

    image

    EDIT: It could also be possible to have a breakout board, for converting to 4-wire clips : ) Maybe that's overkill though, it depends on what ranges are supported and if it would benefit from that.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz

    Does the Cal button request you to open and short the connections? If so, maybe it's possible to build calibration and test fixtures for this LCR meter (or maybe some are supplied), especially for SMD (but would also suit through-hole).

     

    Yes yes and yes image

     

    image

     

     

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps

    Ohh that's great! It's awesome that it comes with those ready-made. You're all set for high-quality measurements : )

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 6 years ago in reply to Jan Cumps

    Nice LCR meter, I have the Voltcraft LCR-300, served me pretty well over the years, will be interesting to see how you get on with yours. It does very much look like a clone of an Appa Technology 700 series LCR meter. Appa do make some very good instrumentation in my experience.

     

    Kind regards.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 6 years ago in reply to Jan Cumps

    Nice LCR meter, I have the Voltcraft LCR-300, served me pretty well over the years, will be interesting to see how you get on with yours. It does very much look like a clone of an Appa Technology 700 series LCR meter. Appa do make some very good instrumentation in my experience.

     

    Kind regards.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to three-phase

    ... It does very much look like a clone of an Appa Technology 700 series LCR meter. Appa do make some very good instrumentation in my experience....

    Not only the looks are the same. Also the accessories and the specs. edit: it's the Appa 703.

     

    Appa is an interesting company.

    Some instruments seem to be available from them only.

    Others are out there rebranded by 3, 4, 5 other companies. The RLC meter is an example. Same for their (adorable !) pocket multimeter.

    I read on eevblog that Appa is the OEM, not the rebrander. They seem to be the ones that churn out all those nice instruments.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Jan Cumps

    Jan Cumps  wrote:

     

    ... Appa ...for their (adorable !) pocket multimeter.

    This is the meter I'm referring too. Like a pocket calculator, it fits in your shirt pocket.

    image

    image source: manufacturer website.

     

    kk99 blogged about model 5: Appa iMeter 5.

     

    And this one I got from RS Pro seems to have seen the same designers as the Appa M series:

    imageimage

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to three-phase

    Meanwhile, Appa lineage confirmed on the PCB: