Power & Energy
  • Technologies
  • More
Power & Energy
Forum Best way to determine 18650 capacity, resistance and condition ?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 284 subscribers
  • Views 8170 views
  • Users 0 members are here
Related

Best way to determine 18650 capacity, resistance and condition ?

o.thornwall
o.thornwall over 5 years ago

I'd like to get idea on the best way or process to check the capacity, resistance and usable condition of used 18650 batteries ?

I plan on buying several hundreds of these batteries for an up coming project .

 

Thank you, Oscar.

  • Sign in to reply
  • Cancel

Top Replies

  • pctechnocrat
    pctechnocrat over 5 years ago +4
    I have done this for larger battery packs, but the same general method applies for measuring the internal resistance of the cell. Without buying special battery test hardware, you will need an electronic…
  • cookmesomekai
    cookmesomekai over 5 years ago +3
    Reliably determining the state of health of a lithium ion cell is pretty hard to do unless you have a reference cell. If time is not an issue and you have a source, a sink and a power meter available then…
  • jw0752
    jw0752 over 5 years ago in reply to o.thornwall +2
    The problem is defining exactly the point of total discharge, When I test them I fully charge them and then time how long it takes for them to discharge at a specified current to a lower voltage point…
Parents
  • genebren
    genebren over 5 years ago

    I think that the best way to test a batteries capacity to measure the complete charge and discharge cycle (voltage, current and time) to address the true storage.  I did this on a recent project (Walky the Biped Robot - Power pack  and Walky the Biped Robot - A new hope (actually a new body and battery) ) and I was quite surprised with the data (measured between 220mAh and 290mAh for a rated 1200mAh cell).  There are a lot of junk batteries being sold out there, so it really does pay to test your battery capacity before relying on the stated values.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 5 years ago

    I think that the best way to test a batteries capacity to measure the complete charge and discharge cycle (voltage, current and time) to address the true storage.  I did this on a recent project (Walky the Biped Robot - Power pack  and Walky the Biped Robot - A new hope (actually a new body and battery) ) and I was quite surprised with the data (measured between 220mAh and 290mAh for a rated 1200mAh cell).  There are a lot of junk batteries being sold out there, so it really does pay to test your battery capacity before relying on the stated values.