Power & Energy
  • Technologies
  • More
Power & Energy
Forum Solar Battery Charger
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 4 answers
  • Subscribers 284 subscribers
  • Views 5554 views
  • Users 0 members are here
  • solar-cell
  • automatic battery charger
Related

Solar Battery Charger

tallen121
tallen121 over 8 years ago

I would like to preface this post by saying I have no idea what I'm doing.

So here's what I have going on.

I bought a bunch of solar garden lights at my dollar store. Each light comes with a solar panel and a rechargeable AAA battery.

I've connected all of the batteries up in series, and I've connected up the solar panels in some horrible series/parallel hybrid.

My goal with this is to hook up the batteries to the solar panels, and connect all of that to the interior of a car USB charger to use it to make a solar panel phone charger.

However, I'm not very familiar or comfortable with electricity. So how would I go about connecting the solar panels to the batteries, and eventually to the usb power? Any help is very much appreciated.image

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 8 years ago +1 suggested
    Hi Tallen, Thanks for the heads up on your skill base. Hooking the batteries directly to the solar cells is very bad! Depending upon the battery you use, each is sensitive to the rate at which they charge…
Parents
  • tallen121
    0 tallen121 over 8 years ago

    I suppose I've done it. So for recap:
    1. I've wired the solar panels in series into a car charger circuit.
    2. I've plugged the car charger into a battery bank.

    Now it works and the battery bank should disconnect the battery when it's fully charged.
    The only issues currently are the fact that the solar panels are not providing enough charge to actually power the battery in a reasonable amount of time. I will update my design by doubling the amount of solar panels or at least keep adding them until I can actually charge the battery in less than 3 years.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • tallen121
    0 tallen121 over 8 years ago

    I suppose I've done it. So for recap:
    1. I've wired the solar panels in series into a car charger circuit.
    2. I've plugged the car charger into a battery bank.

    Now it works and the battery bank should disconnect the battery when it's fully charged.
    The only issues currently are the fact that the solar panels are not providing enough charge to actually power the battery in a reasonable amount of time. I will update my design by doubling the amount of solar panels or at least keep adding them until I can actually charge the battery in less than 3 years.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer