Power & Energy
  • Technologies
  • More
Power & Energy
Forum Solar Battery Charger
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 4 answers
  • Subscribers 285 subscribers
  • Views 5511 views
  • Users 0 members are here
  • solar-cell
  • automatic battery charger
Related

Solar Battery Charger

tallen121
tallen121 over 8 years ago

I would like to preface this post by saying I have no idea what I'm doing.

So here's what I have going on.

I bought a bunch of solar garden lights at my dollar store. Each light comes with a solar panel and a rechargeable AAA battery.

I've connected all of the batteries up in series, and I've connected up the solar panels in some horrible series/parallel hybrid.

My goal with this is to hook up the batteries to the solar panels, and connect all of that to the interior of a car USB charger to use it to make a solar panel phone charger.

However, I'm not very familiar or comfortable with electricity. So how would I go about connecting the solar panels to the batteries, and eventually to the usb power? Any help is very much appreciated.image

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 8 years ago +1 suggested
    Hi Tallen, Thanks for the heads up on your skill base. Hooking the batteries directly to the solar cells is very bad! Depending upon the battery you use, each is sensitive to the rate at which they charge…
Parents
  • unlimitedpipes
    0 unlimitedpipes over 8 years ago

    I think you might have trouble with the voltage you have created. I might be wrong of course. Batteries when connected in series add voltages together. A 1.5 volt battery + 1.5 volt battery = 3 volts +1.5 volt battery = 4.5 volts + 1.5 volts = 6 volts ,enough for an Arduino that has a voltage regulator set at 5 volts for USB output which is good for cell phones I believe. The same applies to the solar cells but they are not voltage regulated.

     

    OK now the current supply, if you connect 2 solar panels that you have in series and attach the out put to 2 series batteries they will charge the batteries in ( at regular set period of time maybe 3 hours ) if you connect in series 2 more solar panels and attach them across the 2 series batteries already connected to the 2 solar panels the voltage output will remain the same but there will be 2 times the current available to charge the batteries with which might cut in half the charge time if the batteries will accept the additional charge current.

     

    You have mentioned a car USB charger but I did not see it in the photo. So I left out any explanation of that circuit. Hope this helps.

     

    Cheers Daleimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tallen121
    0 tallen121 over 8 years ago in reply to unlimitedpipes

    I plugged the solar panels that way because I figured the 4 in series would create 6 volts for a phone, and then the 2 in parallel would just up the amps to charge a little faster. But again, I have no idea in reality what I'm doing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tallen121
    0 tallen121 over 8 years ago in reply to unlimitedpipes

    I plugged the solar panels that way because I figured the 4 in series would create 6 volts for a phone, and then the 2 in parallel would just up the amps to charge a little faster. But again, I have no idea in reality what I'm doing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • unlimitedpipes
    0 unlimitedpipes over 8 years ago in reply to tallen121

    The picture you posted show 2 sets of parallel solar cells. I think you would be better to stick with one solar cell connected across one battery those pairs connected in series to the voltage you want. You do know cars use 12 volt batteries?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tallen121
    0 tallen121 over 8 years ago in reply to unlimitedpipes

    So you're saying to just put the solar cells in series? And, yes. But if you're suggesting I buy a car battery for a little cell phone charger experiment...