Power & Energy
  • Technologies
  • More
Power & Energy
Forum converting to 5V power supply
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 3 answers
  • Subscribers 283 subscribers
  • Views 1456 views
  • Users 0 members are here
Related

converting to 5V power supply

houandreas
houandreas over 8 years ago

Hi, I have a base board which offers 2.5V@8A, 3.3V@8A and 12V@1A power supply but my sister board need 5V. So I'm considering to convert 12V to 5V, can I just use two resistors (10k and 24k ohm) to do that? This is under assumption that the sister board's impedance is high so I'm not sure if this simple circuit works. It should work but I'm rly not sure.. first time for me doing this.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +6 suggested
    Hi Bin, The calculation is not right, you can use this web page to do it (the formula is there too): Voltage Divider Calculator However, unless your sister board has very low current requirement (much…
  • jw0752
    jw0752 over 8 years ago +5 verified
    Hi Bin, This little DC / DC converter will work well for your application. I have used them in similar applications. http://www.newark.com/recom-power/r-78e5-0-0-5/dc-dc-converter-2-5w-5v-0-5a-sip/dp/62X9499…
  • genebren
    genebren over 8 years ago +3 suggested
    Hi Bin, Both shabaz and jw0752 have offered some sound advice (as they are known to do around here). Another simple and perhaps lower cost approach might be a simple 5.0V regulator. This is feasible is…
Parents
  • genebren
    0 genebren over 8 years ago

    Hi Bin,

     

    Both shabaz and jw0752 have offered some sound advice (as they are known to do around here).  Another simple and perhaps lower cost approach might be a simple 5.0V regulator.  This is feasible is the supply currents are low enough that the regulator is not called upon to dissipate too much power (not a problem with the DC-to-DC convertors mentioned above).  As an example, if the load current is 100ma, the regulator would dissipate (12v-5v) * 0.1A, or 0.7Watts, which could fall outside of the parts specification.  As a side note, some DC-to-DC convertors can generate a lot of high frequency noise, that might cause other issues (on the main board and the sister board), so be aware, should you see any performance issues in your project.

     

    Good luck and welcome to the Element14 community!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • houandreas
    0 houandreas over 8 years ago in reply to genebren

    thx, i would try a converter first. I also had a look at the base board and found that it uses 3 regulators to offer these 3 kinds of power sources. The power it uses is also 5V and converted to 2.5V,3.3V,12V for user use. And as mentioned in question they support up to 8A,8A,1A, with the calculation you mentioned it can dissipate (5v-2.5v)*8A=20 Watts.Why isn't it a problem? If it's just the regulator's difference, is it ok for me to use one if pay attention to the regulators specification?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to houandreas

    Regulators can be build that will handle several watts.  In addition, heatsinks and good PCB layouts can extend the range by helping to dissipate heat into the air and/or other materials, so that the chip does not over heat.  There are also other techniques, like adding inline diodes to the regulator input to reduce the voltage drop across the regulator (5Vin-0.7Vd- 2.5Vout) * 8A = 14.4Watts (will offering reverse voltage protection).  These are all steps to finding and using regulators without damaging them.

    Good Luck with your project.

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • genebren
    0 genebren over 8 years ago in reply to houandreas

    Regulators can be build that will handle several watts.  In addition, heatsinks and good PCB layouts can extend the range by helping to dissipate heat into the air and/or other materials, so that the chip does not over heat.  There are also other techniques, like adding inline diodes to the regulator input to reduce the voltage drop across the regulator (5Vin-0.7Vd- 2.5Vout) * 8A = 14.4Watts (will offering reverse voltage protection).  These are all steps to finding and using regulators without damaging them.

    Good Luck with your project.

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • houandreas
    0 houandreas over 8 years ago in reply to genebren

    thx for your answerimage that sounds interesting