Power & Energy
  • Technologies
  • More
Power & Energy
Forum converting to 5V power supply
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 3 answers
  • Subscribers 283 subscribers
  • Views 1448 views
  • Users 0 members are here
Related

converting to 5V power supply

houandreas
houandreas over 8 years ago

Hi, I have a base board which offers 2.5V@8A, 3.3V@8A and 12V@1A power supply but my sister board need 5V. So I'm considering to convert 12V to 5V, can I just use two resistors (10k and 24k ohm) to do that? This is under assumption that the sister board's impedance is high so I'm not sure if this simple circuit works. It should work but I'm rly not sure.. first time for me doing this.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +6 suggested
    Hi Bin, The calculation is not right, you can use this web page to do it (the formula is there too): Voltage Divider Calculator However, unless your sister board has very low current requirement (much…
  • jw0752
    jw0752 over 8 years ago +5 verified
    Hi Bin, This little DC / DC converter will work well for your application. I have used them in similar applications. http://www.newark.com/recom-power/r-78e5-0-0-5/dc-dc-converter-2-5w-5v-0-5a-sip/dp/62X9499…
  • genebren
    genebren over 8 years ago +3 suggested
    Hi Bin, Both shabaz and jw0752 have offered some sound advice (as they are known to do around here). Another simple and perhaps lower cost approach might be a simple 5.0V regulator. This is feasible is…
Parents
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    If you wanted to be really crude you could use a high-ish value resistor and a 5v zener to derive 12V.  It's a bit ugly but cheap and easy if you get the current calcs correct!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    If you wanted to be really crude you could use a high-ish value resistor and a 5v zener to derive 12V.  It's a bit ugly but cheap and easy if you get the current calcs correct!