Power & Energy
  • Technologies
  • More
Power & Energy
Forum Where to get LEDs rated for 1 to 1.5v
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 12 answers
  • Subscribers 282 subscribers
  • Views 19472 views
  • Users 0 members are here
Related

Where to get LEDs rated for 1 to 1.5v

hafcanadian
hafcanadian over 8 years ago

I have tried to repair a solar flickering garden pagoda light.  Unlike all the other types of that device I own, this one uses one AA NiMh battery rather than two.  It’s LED needs replacing because one of its wires had broken where it entered the “glass” head.

 

I got some 5mm wide-angle straw hat (stubby length) yellow/amber LEDs from Lighthouse LEDs last year, but illness kept me away from the task until this week.  The replacements from Lighthouse are 2v, but I guess I’d assumed that was a maximum rating.  Unfortunately no, Lighthouse now informs me they need at least 2 volts to light up, which on reflection makes sense.  It explains why the new lamp I soldered in wouldn’t light up... I initially thought I’d ruined the lamp with solder heat, and soldered in another using multiple heat sinks.  It didn’t light either.  Then I touched leads from a fresh AA battery to a lamp fresh out of the shipping bag, and it wouldn’t light.  Ah ha moment... dumb me.  My assumption that 2v was a max, because it was the lowest voltage lamp I could find, was ill advised.  But being an LED neophyte I seem always ignorant of their technics, as numerous faulty Xmas LED strings lying comfoundingly unrepaired in a bag will attest.

 

I think the circuit board controls the flame-like flickering because the original lamp was a straw hat.  But just in case, I also got from Lighthouse some standard 5mm self-flicker lamps at the same time.  What I can’t figure out is how the original LED worked on a single AA battery.  Lighthouse says I shouldn’t need a resistor in the circuit, but there is a coded red-green-red-silver one on the board.  Perhaps that is to control the current coming in during midday from the solar panel?  Regardless, surely the original LED must be a 1 volt lamp?  But where can I purchase such an animal?  Lighthouse claims to not be aware of any such device.

 

I guess I could try adding a second AA NiMh battery to bump the unit to 3v, but the box is only big enough for one and I don’t know but what the diodes and other CB components may not play well with 3 volts, nor if the panel has enough output potential to fully charge two NiMh AAs, even if they were only 600mAh ones.

 

Thanks in advance for any thoughts,

Joel

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +7 verified
    Joel, There are not many (if any) visible spectrum LEDs that will run directly from a single AA battery. But, most of the inexpensive solar/LED devices, using a single AA battery use a device (like cx2601…
  • jw0752
    jw0752 over 8 years ago +7 suggested
    Hi Joel, I was set up to do some experiments this evening and so I decided to take apart a cheap dollar store outside LED light and check the voltages. I knew that they operate on one 1.25 volt NiMH battery…
  • hafcanadian
    hafcanadian over 8 years ago +7 suggested
    Thanks to all who’ve responded. The idea of an inductor that boosts voltage makes a great deal of sense. I can see where the AA battery would not work directly, and my suspicions that the 2v rating for…
Parents
  • 14rhb
    0 14rhb over 8 years ago

    Hi Joel,

     

    An interesting post - I'm sure countless numbers of these, often cheap, solar lights end up in landfill/incineration but luckily not yours...so well done trying to repair them.

     

    Lots of good comments already re: the voltage boosting. A non-technical term for this type of setup is sometimes known as a Joule Thief . The phrase was coined to detail a circuit that extracts all the energy from a single cell battery...and the standard designs work well.

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • 14rhb
    0 14rhb over 8 years ago

    Hi Joel,

     

    An interesting post - I'm sure countless numbers of these, often cheap, solar lights end up in landfill/incineration but luckily not yours...so well done trying to repair them.

     

    Lots of good comments already re: the voltage boosting. A non-technical term for this type of setup is sometimes known as a Joule Thief . The phrase was coined to detail a circuit that extracts all the energy from a single cell battery...and the standard designs work well.

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer