Power & Energy
  • Technologies
  • More
Power & Energy
Forum Where to get LEDs rated for 1 to 1.5v
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 12 answers
  • Subscribers 282 subscribers
  • Views 19472 views
  • Users 0 members are here
Related

Where to get LEDs rated for 1 to 1.5v

hafcanadian
hafcanadian over 8 years ago

I have tried to repair a solar flickering garden pagoda light.  Unlike all the other types of that device I own, this one uses one AA NiMh battery rather than two.  It’s LED needs replacing because one of its wires had broken where it entered the “glass” head.

 

I got some 5mm wide-angle straw hat (stubby length) yellow/amber LEDs from Lighthouse LEDs last year, but illness kept me away from the task until this week.  The replacements from Lighthouse are 2v, but I guess I’d assumed that was a maximum rating.  Unfortunately no, Lighthouse now informs me they need at least 2 volts to light up, which on reflection makes sense.  It explains why the new lamp I soldered in wouldn’t light up... I initially thought I’d ruined the lamp with solder heat, and soldered in another using multiple heat sinks.  It didn’t light either.  Then I touched leads from a fresh AA battery to a lamp fresh out of the shipping bag, and it wouldn’t light.  Ah ha moment... dumb me.  My assumption that 2v was a max, because it was the lowest voltage lamp I could find, was ill advised.  But being an LED neophyte I seem always ignorant of their technics, as numerous faulty Xmas LED strings lying comfoundingly unrepaired in a bag will attest.

 

I think the circuit board controls the flame-like flickering because the original lamp was a straw hat.  But just in case, I also got from Lighthouse some standard 5mm self-flicker lamps at the same time.  What I can’t figure out is how the original LED worked on a single AA battery.  Lighthouse says I shouldn’t need a resistor in the circuit, but there is a coded red-green-red-silver one on the board.  Perhaps that is to control the current coming in during midday from the solar panel?  Regardless, surely the original LED must be a 1 volt lamp?  But where can I purchase such an animal?  Lighthouse claims to not be aware of any such device.

 

I guess I could try adding a second AA NiMh battery to bump the unit to 3v, but the box is only big enough for one and I don’t know but what the diodes and other CB components may not play well with 3 volts, nor if the panel has enough output potential to fully charge two NiMh AAs, even if they were only 600mAh ones.

 

Thanks in advance for any thoughts,

Joel

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +7 verified
    Joel, There are not many (if any) visible spectrum LEDs that will run directly from a single AA battery. But, most of the inexpensive solar/LED devices, using a single AA battery use a device (like cx2601…
  • jw0752
    jw0752 over 8 years ago +7 suggested
    Hi Joel, I was set up to do some experiments this evening and so I decided to take apart a cheap dollar store outside LED light and check the voltages. I knew that they operate on one 1.25 volt NiMH battery…
  • hafcanadian
    hafcanadian over 8 years ago +7 suggested
    Thanks to all who’ve responded. The idea of an inductor that boosts voltage makes a great deal of sense. I can see where the AA battery would not work directly, and my suspicions that the 2v rating for…
  • dougw
    0 dougw over 8 years ago in reply to hafcanadian

    Discoloration of the pins in itself does not mean it has failed, but it is one of the most likely components to fail in this circuit.

    Since it has 4 pins, it is a more complex chip than a simple transistor.

    I would first try re-soldering all the solder joints and closely inspect all wire connections.

    Then try operating the circuit with a known good power source.

    If that fails, you may need to start comparing what is happening on each pin of the chip with a what is happening on corresponding pins of a working circuit.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to hafcanadian

    Hi Joel,

    Here is the likely circuit for the 4 pin IC which I believe is a YX8018;

     

    image

     

    Here is the link to the Google Picture gallery for the YX8018:

     

    https://www.google.com/search?q=YX8018&tbm=isch&tbo=u&source=univ&sa=X&ved=2ahUKEwih78z--IHeAhULiIMKHQzxDmMQsAR6BAgDEAE&biw=1920&bih=934#imgrc=_

     

    If it isn't connections or a bad battery the IC is the likely culprit as Doug mentioned. The stage of rust on the leads pictured is not likely the cause of the failure.

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to hafcanadian

    Joel,

     

    I am not sure that the pattern that John captured on his scope will explain the flicker LED effect.  It is possible that his solar LED has a different chip than yours, but the pattern shown appears to be oscillating at a fixed pattern which is well above the eyes ability to see.  It is oscillation pattern is likely only used to boost the voltage.  Having said that, it would be possible to design a chip that modulated the switching pattern of the boost circuit to create a varying intensity on the LED (I just did not see any evidence of that in the switching rate of John's LED).

     

    Issues that might be effecting your LED lanterns:

     

    1) The batteries might not be able to hold a charge (or charge in the circuit).  Try another battery, or an external power source.  (Note: this simple devices do not follow manufactures specifications for battery charging.  They simply act as a simple trickle charger.  This may not allow the batteries to deliver the full charge available. They do not limit charge or protect against over voltage)

     

    2) Along the line of the batteries, but there may be corrosion on the battery terminals that is causing a poor connection.  Clean the battery connections.

     

    3) The solar panel may not be functional.  Try a fully charged battery.

     

    4) The LED that you have used may have higher forward voltage than the circuit is designed to provide.  In the lower current range of LEDs (<100mA), about 60% of those are rated below 3.5V.  Have you tried to illuminate the LED with a power supply or multiple batteries (with a current limiting resistor) to see what the turn-on voltage is?

     

    There could be other issues that are more difficult to diagnose (or guess) without further information.

     

    Good luck in getting these lamps to light.

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hafcanadian
    0 hafcanadian over 8 years ago in reply to jw0752

    Got distracted by other responsibilities for a few days, and haven’t tried yet to resolder anything, but found a minute to review the thread, and should note what just occurred to me is a missing component in the diagram John provided.

     

    Rather than a light sensor via the panel as some units use, this one has a separate half inch round one imbedded in the lamp body opposite the solar panel.  I haven’t had time to refresh my memory of the wiring, and don’t know exactly where in the diagram one would expect to see that light sensor.  I do know it works though, as I had to cover it with electrical tape so my workbench lighting wouldn’t keep the circuit off while I was testing operation.

     

    Whether faulty or taped over, it shouldn’t be keeping the circuit off should it?   Also I don’t see the on/off switch in the diagram, so I reckon my circuit’s only a tad more complex.

     

    Joel

     

    Also I bent the IC up enough to read “SS550A” on its underside.  Perhaps this diagram I found is closer?

    https://goo.gl/images/KWBptN

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<