Power & Energy
  • Technologies
  • More
Power & Energy
Forum Smps sine wave
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 282 subscribers
  • Views 2901 views
  • Users 0 members are here
Related

Smps sine wave

bigsexy
bigsexy over 6 years ago

As I further learn about the intricacies of electronics and do not have an adequate oscilloscope I have a question regarding SMPS. I know how regular old go to hell transformers work and require a sine wave switching to positive and negative voltages to create the magnetic field induced into the iron core and so forth. But does a sine wave have to go Into negative voltages to work? Let me elaborate a little because I tend to over complicate my thoughts.
Lets say I have a mosfet that I use as a switch to pulse a dc voltage on and off at a significant speed in the kHz range through a wire wrapped in a coil on a transformer core, would that be able to create a half sine wave and therefore be used to induce a voltage in a secondary winding?

I am wondering if in a smps if the electronics recreate the sine wave to go high and low instead of high and off?

If this is confusing speak to you let me know and I will try to draw something up on paper and photo it for the thread.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +3 suggested
    It's too big a subject to explain in an answer here ! I had a quick Google for some tutorial type stuff and found this that isn't too bad: https://www.electronics-tutorials.ws/power/switch-mode-power-supply…
  • jc2048
    jc2048 over 5 years ago in reply to michaelkellett +3 suggested
    This is the best thing I've ever read on the subject, but I'm not sure it qualifies as an 'introduction' [someone reading it would need some familiarity with Faraday and Ampere and be capable of simple…
  • jc2048
    jc2048 over 5 years ago +3 suggested
    The waveform doesn't have to be a sinewave. If you'd like to see the effect of different waveforms, here's a selection from a pattern generator driving an old mains transformer that I found in one of my…
Parents
  • jw0752
    0 jw0752 over 6 years ago

    Hi Kevin,

    The simple answer to your question is that any time a current changes in a wire, whether it changes sinusoidally, linearly, or any other rate of change with respect to time the magnetic field that is generated also changes. A changing magnetic field will induce voltage in conductors that are present within the field. The sine wave is what is produced by a coil that is spinning in a constant magnetic field so we are familiar with this rate of change as that is how our house current is produced. The sine wave is not however necessary to produce induction in a transformer. Waves that are more square or triangular work also. Most SMPS make no attempt to produce a sine wave in the primary of their power supplies. the MOSFETs that turn the power on and off to the transformer are usually much closer to square waves than sine. SMPS usually deal with AC to DC or DC to DC conversion. A special type called an Inverter will convert from DC to AC and since the AC produced is usually for consumer use on appliances the better inverters will make an attempt at producing a sine wave output.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 6 years ago

    Hi Kevin,

    The simple answer to your question is that any time a current changes in a wire, whether it changes sinusoidally, linearly, or any other rate of change with respect to time the magnetic field that is generated also changes. A changing magnetic field will induce voltage in conductors that are present within the field. The sine wave is what is produced by a coil that is spinning in a constant magnetic field so we are familiar with this rate of change as that is how our house current is produced. The sine wave is not however necessary to produce induction in a transformer. Waves that are more square or triangular work also. Most SMPS make no attempt to produce a sine wave in the primary of their power supplies. the MOSFETs that turn the power on and off to the transformer are usually much closer to square waves than sine. SMPS usually deal with AC to DC or DC to DC conversion. A special type called an Inverter will convert from DC to AC and since the AC produced is usually for consumer use on appliances the better inverters will make an attempt at producing a sine wave output.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • fmilburn
    0 fmilburn over 6 years ago in reply to jw0752

    I cannot imagine a more succinct yet information filled paragraph than this :-)