Power & Energy
  • Technologies
  • More
Power & Energy
Forum Smps sine wave
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 282 subscribers
  • Views 2901 views
  • Users 0 members are here
Related

Smps sine wave

bigsexy
bigsexy over 6 years ago

As I further learn about the intricacies of electronics and do not have an adequate oscilloscope I have a question regarding SMPS. I know how regular old go to hell transformers work and require a sine wave switching to positive and negative voltages to create the magnetic field induced into the iron core and so forth. But does a sine wave have to go Into negative voltages to work? Let me elaborate a little because I tend to over complicate my thoughts.
Lets say I have a mosfet that I use as a switch to pulse a dc voltage on and off at a significant speed in the kHz range through a wire wrapped in a coil on a transformer core, would that be able to create a half sine wave and therefore be used to induce a voltage in a secondary winding?

I am wondering if in a smps if the electronics recreate the sine wave to go high and low instead of high and off?

If this is confusing speak to you let me know and I will try to draw something up on paper and photo it for the thread.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +3 suggested
    It's too big a subject to explain in an answer here ! I had a quick Google for some tutorial type stuff and found this that isn't too bad: https://www.electronics-tutorials.ws/power/switch-mode-power-supply…
  • jc2048
    jc2048 over 5 years ago in reply to michaelkellett +3 suggested
    This is the best thing I've ever read on the subject, but I'm not sure it qualifies as an 'introduction' [someone reading it would need some familiarity with Faraday and Ampere and be capable of simple…
  • jc2048
    jc2048 over 5 years ago +3 suggested
    The waveform doesn't have to be a sinewave. If you'd like to see the effect of different waveforms, here's a selection from a pattern generator driving an old mains transformer that I found in one of my…
Parents
  • bigsexy
    0 bigsexy over 6 years ago

    So if I understand correctly, a transformer does not need the voltage to alternate between positive AND negative, and will work just from an electric field being pulsed on and off at a high rate?

     

    Also I want to add clarification to the last sentence of my original post. After re-reading it, it kind of comes off kind of a-hole’ish, what I meant to come across was I have a habit of making things very confusing and can try a different way if my question was confusing.

     

    And a big thank you for the answers! I also have another question I will have to start a new post as it is completely unrelated.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bigsexy
    0 bigsexy over 6 years ago

    So if I understand correctly, a transformer does not need the voltage to alternate between positive AND negative, and will work just from an electric field being pulsed on and off at a high rate?

     

    Also I want to add clarification to the last sentence of my original post. After re-reading it, it kind of comes off kind of a-hole’ish, what I meant to come across was I have a habit of making things very confusing and can try a different way if my question was confusing.

     

    And a big thank you for the answers! I also have another question I will have to start a new post as it is completely unrelated.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 6 years ago in reply to bigsexy

    Hi Kevin,

     

    You are more or less correct. A voltage across a load ( I say across a load as this will produce a current) only needs to change in some way over time to create a changing magnetic field which can induce a current in another circuit. We need to be talking about magnetic fields and currents, not voltages and electric fields. A magnetic filed can only induce a current in another circuit when the field is changing or the other circuit is physically moving so as to cross the field lines of the magnetic field. As you would say the voltage (across a load) does not need to alternate between positive and negative, it only needs to change between one voltage and another voltage. Remember that until we plug a load into the wall outlet nothing happens. There is voltage there but for something to happen there must be a current.

     

    When you talk about plus and minus voltage you are choosing a reference point to be zero volts and measuring from there. Voltage is potential energy. Sometimes it is even called potential instead of voltage. We measure the voltage in our homes as 115 Volts rms but the actual voltage measured from the neutral wire designated as 0 volts to the hot wire goes from about +161V to -161V.  The peak to peak voltage in this case is 322 volts. We use the root mean square (rms) voltage as it tells us how much energy is actually available for a given load. It is kind of the average of the highs and lows. The rms voltage is equivalent to the DC voltage that would produce the same amount of work across a load of equal resistance.

     

    Your question was a good one and as Michael pointed out has a lot of depth which can be explored. If I have made any mistakes in what I have told you my friends on the forum will add corrections or clarifications. This is a great place to ask questions as everyone helps and participates just like a group of collaborative minds.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer