Power & Energy
  • Technologies
  • More
Power & Energy
Forum Issues With MOSFET bridge, DC motor 24V 200W
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 281 subscribers
  • Views 5545 views
  • Users 0 members are here
  • mosfet
  • motor drives
  • mosfet driver
  • h bridge circuit
  • brushed dc motor control
  • h bridge motor control
  • high side driver
Related

Issues With MOSFET bridge, DC motor 24V 200W

shwetankv007
shwetankv007 over 5 years ago

Hello everyone,

I have been working on a project to drive a 200W 24V motor that gets a continuous drive current of about 7-8A. The idea is to run the motor in forward and reverse direction interchangeably much like a car viper. The time for forward and reverse is about 20seconds each.

I want to use 4-N channel MOSFETs for this and use a discrete driver.

Mosfets used - STP55N i.e. 60V 50A

Input supply - 24V

PWM input - In-1 and In-2, a signal on one of the inputs will run the motor in one direction and vice versa.

Bootstrap Capacitor - 10uF 50V

 

Issues -

1. The circuit is working i.e. motor is getting turned on in both the direction but upper MOSFETs are getting heated upto 70degree within few minutes.

2. Is there an issue with the bootstrap circuitry?

image

  • Sign in to reply
  • Cancel

Top Replies

  • kkazem
    kkazem over 4 years ago +3
    It's a bad idea to drive a power mosfet this way. First of all, the Supply Voltage is 24 VDC and the FET's max gate voltage is only 20 V. Therefore, you can expect FET failures via puncturing the gate…
  • dougw
    dougw over 5 years ago +2 suggested
    R1 may be too high of a value. It will take time to charge the gate capacitance, which will turn the FET on slowly, causing heat losses. If R1 is made smaller, it may discharge the capacitor too fast to…
  • dougw
    dougw over 5 years ago in reply to shwetankv007 +1
    Is the capacitor discharging when T1 is on to the point where there is no boost to the gate - which would mean Q1 is only partly turned on? By push-pull I mean put a stage like this on the output of T1…
Parents
  • dougw
    0 dougw over 5 years ago

    R1 may be too high of a value. It will take time to charge the gate capacitance, which will turn the FET on slowly, causing heat losses.

    If R1 is made smaller, it may discharge the capacitor too fast to keep the FET on.

    You may need to drive the gate with a push pull transistor pair so it turns on and off quickly without discharging the capacitor.

    You also need to ensure that Q1 and Q2 are never turned on at the same time. If Q1 is slow to turn off, Q2 will pull current through it, heating it up.

    The same problem happens to Q2 if it is slow to turn off.

    You need a delay between turning each FET off and turning its counterpart on.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 5 years ago

    R1 may be too high of a value. It will take time to charge the gate capacitance, which will turn the FET on slowly, causing heat losses.

    If R1 is made smaller, it may discharge the capacitor too fast to keep the FET on.

    You may need to drive the gate with a push pull transistor pair so it turns on and off quickly without discharging the capacitor.

    You also need to ensure that Q1 and Q2 are never turned on at the same time. If Q1 is slow to turn off, Q2 will pull current through it, heating it up.

    The same problem happens to Q2 if it is slow to turn off.

    You need a delay between turning each FET off and turning its counterpart on.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • shwetankv007
    0 shwetankv007 over 5 years ago in reply to dougw

    When you say to drive the gate with a push pull pair, are you referring to both High side and Low side FETs.

    For experiment, I gave IN_1 a permanent zero volt and IN_2 a permanent 5V. Turning on Q1 and Q4. Do I still need to consider the rise time since the gate is always ON?

     

    Also, the Ciss is around 1.5nF that will give me a rise time of 15us roughly with the 10K resistor. If I use a PWM of 10KHz, then also this rise time may work ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 5 years ago in reply to shwetankv007

    Is the capacitor discharging when T1 is on to the point where there is no boost to the gate - which would mean Q1 is only partly turned on?

    By push-pull I mean put a stage like this on the output of T1, this would allow a large value for R1 that would not discharge the capacitor so fast:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shwetankv007
    0 shwetankv007 over 5 years ago in reply to dougw

    Got that, this will help me reduce the charging slope during the positive and negative triggers. Tried this circuit too for feeding to the gate, still the upper MOSFET is heating.

     

    Some more observations :-

    At Supply voltage 27V, when T1 base is pulled down and T2 pulled up.

    Gate voltage at Q1 is 25V, Drain source voltage at Q1 is 2.5 volts and Drain source voltage at Q4 is zero.

    This suggests that Q1 is not turning on properly.

     

    Is the bootstrap not working correctly? Am I missing something?

    Thanks