Power & Energy
  • Technologies
  • More
Power & Energy
Forum Issues With MOSFET bridge, DC motor 24V 200W
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 281 subscribers
  • Views 5548 views
  • Users 0 members are here
  • mosfet
  • motor drives
  • mosfet driver
  • h bridge circuit
  • brushed dc motor control
  • h bridge motor control
  • high side driver
Related

Issues With MOSFET bridge, DC motor 24V 200W

shwetankv007
shwetankv007 over 5 years ago

Hello everyone,

I have been working on a project to drive a 200W 24V motor that gets a continuous drive current of about 7-8A. The idea is to run the motor in forward and reverse direction interchangeably much like a car viper. The time for forward and reverse is about 20seconds each.

I want to use 4-N channel MOSFETs for this and use a discrete driver.

Mosfets used - STP55N i.e. 60V 50A

Input supply - 24V

PWM input - In-1 and In-2, a signal on one of the inputs will run the motor in one direction and vice versa.

Bootstrap Capacitor - 10uF 50V

 

Issues -

1. The circuit is working i.e. motor is getting turned on in both the direction but upper MOSFETs are getting heated upto 70degree within few minutes.

2. Is there an issue with the bootstrap circuitry?

image

  • Sign in to reply
  • Cancel

Top Replies

  • kkazem
    kkazem over 4 years ago +3
    It's a bad idea to drive a power mosfet this way. First of all, the Supply Voltage is 24 VDC and the FET's max gate voltage is only 20 V. Therefore, you can expect FET failures via puncturing the gate…
  • dougw
    dougw over 5 years ago +2 suggested
    R1 may be too high of a value. It will take time to charge the gate capacitance, which will turn the FET on slowly, causing heat losses. If R1 is made smaller, it may discharge the capacitor too fast to…
  • dougw
    dougw over 5 years ago in reply to shwetankv007 +1
    Is the capacitor discharging when T1 is on to the point where there is no boost to the gate - which would mean Q1 is only partly turned on? By push-pull I mean put a stage like this on the output of T1…
Parents
  • kkazem
    0 kkazem over 4 years ago

    It's a bad idea to drive a power mosfet this way. First of all, the Supply Voltage is 24 VDC and the FET's max gate voltage is only 20 V. Therefore, you can expect FET failures via puncturing the gate, though it probably won't happen right away.  Second, as the turn on path is thru a 10K resistor, the maximum gate charge current is only 2.4 mA peak and reduces as the gate charges up. This would translate into a turn on time of about 37 uS, which is much slower than optimal, causing high FET switching losses. It's not as bad for turn off as the T1 NPN can sink 100-300 mA. A proper FET driver should source and sink at least 1.5 amps for a FET this size for fast switching in the 50-200 nSec range. A cascade (totem-pole) NPN-PNP arrangement (or n-CH-p-CH in MOS) using discrete parts can be used, but the drive supply should be limited to 12 to 15 VDC typically. Even if the FET gate is rated at +/-30V, there's no real advantage to driving the gates that high as they're typically fully enhanced at 10-12 V Vgs. One good, low-cost method for gate drive is to use a CMOS hex inverter or buffer and parallel all of them. Note that you cannot use half the inverters to drive the upper FET and half for the lower FET as the H-Bridge FET Sources are at different grounds. Therefore, you would need two inverter or buffer ICs. The 10uF cap used for the bootstrap supply is a bit high. For this size FET, having Qg (total gate charge) of 90 nanoCoulombs max, a 0.1 uF (100 nF) is more appropriately sized. If the switching frequency is relatively low, as it would be for a motor controller, the 10 uF may work fine, but more than 100 nF isn't needed. In many H-Bridge circuits, it's preferable to have the turn-off speed be faster than the turn on. This is usually done by having a separate resistive circuit for the turn-on & turn off using about a two series resistors with a diode across one of them with the cathode pointing toward the driver. For example, a 5 ohm and a 15 ohm resistor with a 1N4148 across the larger resistor. This effectively gives the turn on circuit 20 ohms series and the turn off just 5 ohm series resistance so that the turn off is substantially faster than turn on. This will help to avoid or minimize Cross-Conduction (aka shoot thru current) in the H-Bridge. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kkazem
    0 kkazem over 4 years ago

    It's a bad idea to drive a power mosfet this way. First of all, the Supply Voltage is 24 VDC and the FET's max gate voltage is only 20 V. Therefore, you can expect FET failures via puncturing the gate, though it probably won't happen right away.  Second, as the turn on path is thru a 10K resistor, the maximum gate charge current is only 2.4 mA peak and reduces as the gate charges up. This would translate into a turn on time of about 37 uS, which is much slower than optimal, causing high FET switching losses. It's not as bad for turn off as the T1 NPN can sink 100-300 mA. A proper FET driver should source and sink at least 1.5 amps for a FET this size for fast switching in the 50-200 nSec range. A cascade (totem-pole) NPN-PNP arrangement (or n-CH-p-CH in MOS) using discrete parts can be used, but the drive supply should be limited to 12 to 15 VDC typically. Even if the FET gate is rated at +/-30V, there's no real advantage to driving the gates that high as they're typically fully enhanced at 10-12 V Vgs. One good, low-cost method for gate drive is to use a CMOS hex inverter or buffer and parallel all of them. Note that you cannot use half the inverters to drive the upper FET and half for the lower FET as the H-Bridge FET Sources are at different grounds. Therefore, you would need two inverter or buffer ICs. The 10uF cap used for the bootstrap supply is a bit high. For this size FET, having Qg (total gate charge) of 90 nanoCoulombs max, a 0.1 uF (100 nF) is more appropriately sized. If the switching frequency is relatively low, as it would be for a motor controller, the 10 uF may work fine, but more than 100 nF isn't needed. In many H-Bridge circuits, it's preferable to have the turn-off speed be faster than the turn on. This is usually done by having a separate resistive circuit for the turn-on & turn off using about a two series resistors with a diode across one of them with the cathode pointing toward the driver. For example, a 5 ohm and a 15 ohm resistor with a 1N4148 across the larger resistor. This effectively gives the turn on circuit 20 ohms series and the turn off just 5 ohm series resistance so that the turn off is substantially faster than turn on. This will help to avoid or minimize Cross-Conduction (aka shoot thru current) in the H-Bridge. 

    • Cancel
    • Vote Up +3 Vote Down