Power & Energy
  • Technologies
  • More
Power & Energy
Forum Issues With MOSFET bridge, DC motor 24V 200W
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 285 subscribers
  • Views 4499 views
  • Users 0 members are here
  • mosfet
  • motor drives
  • mosfet driver
  • h bridge circuit
  • brushed dc motor control
  • h bridge motor control
  • high side driver
Related

Issues With MOSFET bridge, DC motor 24V 200W

shwetankv007
shwetankv007 over 4 years ago

Hello everyone,

I have been working on a project to drive a 200W 24V motor that gets a continuous drive current of about 7-8A. The idea is to run the motor in forward and reverse direction interchangeably much like a car viper. The time for forward and reverse is about 20seconds each.

I want to use 4-N channel MOSFETs for this and use a discrete driver.

Mosfets used - STP55N i.e. 60V 50A

Input supply - 24V

PWM input - In-1 and In-2, a signal on one of the inputs will run the motor in one direction and vice versa.

Bootstrap Capacitor - 10uF 50V

 

Issues -

1. The circuit is working i.e. motor is getting turned on in both the direction but upper MOSFETs are getting heated upto 70degree within few minutes.

2. Is there an issue with the bootstrap circuitry?

image

  • Sign in to reply
  • Cancel

Top Replies

  • kkazem
    kkazem over 3 years ago +3
    It's a bad idea to drive a power mosfet this way. First of all, the Supply Voltage is 24 VDC and the FET's max gate voltage is only 20 V. Therefore, you can expect FET failures via puncturing the gate…
  • dougw
    dougw over 4 years ago +2 suggested
    R1 may be too high of a value. It will take time to charge the gate capacitance, which will turn the FET on slowly, causing heat losses. If R1 is made smaller, it may discharge the capacitor too fast to…
  • dougw
    dougw over 4 years ago in reply to shwetankv007 +1
    Is the capacitor discharging when T1 is on to the point where there is no boost to the gate - which would mean Q1 is only partly turned on? By push-pull I mean put a stage like this on the output of T1…